This module includes functions that control CoAP communication.

Classes

struct otCoapOption
This structure represents a CoAP option.
struct otCoapOptionIterator
This structure acts as an iterator for CoAP options.
struct otCoapResource
This structure represents a CoAP resource.
struct otCoapBlockwiseResource
This structure represents a CoAP resource with block-wise transfer.
struct otCoapTxParameters
This structure represents the CoAP transmission parameters.

Macros

#define OT_DEFAULT_COAP_PORT 5683
Default CoAP port, as specified in RFC 7252.
#define OT_COAP_DEFAULT_TOKEN_LENGTH 2
Default token length.
#define OT_COAP_MAX_TOKEN_LENGTH 8
Max token length as specified (RFC 7252).
#define OT_COAP_MAX_RETRANSMIT 20
Max retransmit supported by OpenThread.
#define OT_COAP_MIN_ACK_TIMEOUT 1000
Minimal ACK timeout in milliseconds supported by OpenThread.
#define OT_COAP_CODE (c, d) ((((c)&0x7) << 5) | ((d)&0x1f))
Helper macro to define CoAP Code values.

Typedefs

typedef enum otCoapType otCoapType
CoAP Type values (2 bit unsigned integer).
typedef enum otCoapCode otCoapCode
CoAP Code values.
typedef enum otCoapOptionType otCoapOptionType
CoAP Option Numbers.
typedef struct otCoapOption otCoapOption
This structure represents a CoAP option.
typedef struct otCoapOptionIterator otCoapOptionIterator
This structure acts as an iterator for CoAP options.
typedef enum otCoapOptionContentFormat otCoapOptionContentFormat
CoAP Content Format codes.
typedef enum otCoapBlockSzx otCoapBlockSzx
CoAP Block Size Exponents.
typedef void(* otCoapResponseHandler ) (void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo, otError aResult)
This function pointer is called when a CoAP response is received or on the request timeout.
typedef void(* otCoapRequestHandler ) (void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo)
This function pointer is called when a CoAP request with a given Uri-Path is received.
typedef otError (* otCoapBlockwiseReceiveHook ) (void *aContext, const uint8_t *aBlock, uint32_t aPosition, uint16_t aBlockLength, bool aMore, uint32_t aTotalLength)
This function pointer is called when a CoAP message with an block-wise transfer option is received.
typedef otError (* otCoapBlockwiseTransmitHook ) (void *aContext, uint8_t *aBlock, uint32_t aPosition, uint16_t *aBlockLength, bool *aMore)
This function pointer is called before the next block in a block-wise transfer is sent.
typedef struct otCoapResource otCoapResource
This structure represents a CoAP resource.
typedef struct otCoapBlockwiseResource otCoapBlockwiseResource
This structure represents a CoAP resource with block-wise transfer.
typedef struct otCoapTxParameters otCoapTxParameters
This structure represents the CoAP transmission parameters.

Enumerations

enum otCoapType {
OT_COAP_TYPE_CONFIRMABLE = 0,
OT_COAP_TYPE_NON_CONFIRMABLE = 1,
OT_COAP_TYPE_ACKNOWLEDGMENT = 2,
OT_COAP_TYPE_RESET = 3
}
CoAP Type values (2 bit unsigned integer).
enum otCoapCode {
OT_COAP_CODE_EMPTY = OT_COAP_CODE(0, 0),
OT_COAP_CODE_GET = OT_COAP_CODE(0, 1),
OT_COAP_CODE_POST = OT_COAP_CODE(0, 2),
OT_COAP_CODE_PUT = OT_COAP_CODE(0, 3),
OT_COAP_CODE_DELETE = OT_COAP_CODE(0, 4),
OT_COAP_CODE_RESPONSE_MIN = OT_COAP_CODE(2, 0),
OT_COAP_CODE_CREATED = OT_COAP_CODE(2, 1),
OT_COAP_CODE_DELETED = OT_COAP_CODE(2, 2),
OT_COAP_CODE_VALID = OT_COAP_CODE(2, 3),
OT_COAP_CODE_CHANGED = OT_COAP_CODE(2, 4),
OT_COAP_CODE_CONTENT = OT_COAP_CODE(2, 5),
OT_COAP_CODE_CONTINUE = OT_COAP_CODE(2, 31),
OT_COAP_CODE_BAD_REQUEST = OT_COAP_CODE(4, 0),
OT_COAP_CODE_UNAUTHORIZED = OT_COAP_CODE(4, 1),
OT_COAP_CODE_BAD_OPTION = OT_COAP_CODE(4, 2),
OT_COAP_CODE_FORBIDDEN = OT_COAP_CODE(4, 3),
OT_COAP_CODE_NOT_FOUND = OT_COAP_CODE(4, 4),
OT_COAP_CODE_METHOD_NOT_ALLOWED = OT_COAP_CODE(4, 5),
OT_COAP_CODE_NOT_ACCEPTABLE = OT_COAP_CODE(4, 6),
OT_COAP_CODE_REQUEST_INCOMPLETE = OT_COAP_CODE(4, 8),
OT_COAP_CODE_PRECONDITION_FAILED = OT_COAP_CODE(4, 12),
OT_COAP_CODE_REQUEST_TOO_LARGE = OT_COAP_CODE(4, 13),
OT_COAP_CODE_UNSUPPORTED_FORMAT = OT_COAP_CODE(4, 15),
OT_COAP_CODE_INTERNAL_ERROR = OT_COAP_CODE(5, 0),
OT_COAP_CODE_NOT_IMPLEMENTED = OT_COAP_CODE(5, 1),
OT_COAP_CODE_BAD_GATEWAY = OT_COAP_CODE(5, 2),
OT_COAP_CODE_SERVICE_UNAVAILABLE = OT_COAP_CODE(5, 3),
OT_COAP_CODE_GATEWAY_TIMEOUT = OT_COAP_CODE(5, 4),
OT_COAP_CODE_PROXY_NOT_SUPPORTED = OT_COAP_CODE(5, 5)
}
CoAP Code values.
enum otCoapOptionType {
OT_COAP_OPTION_IF_MATCH = 1,
OT_COAP_OPTION_URI_HOST = 3,
OT_COAP_OPTION_E_TAG = 4,
OT_COAP_OPTION_IF_NONE_MATCH = 5,
OT_COAP_OPTION_OBSERVE = 6,
OT_COAP_OPTION_URI_PORT = 7,
OT_COAP_OPTION_LOCATION_PATH = 8,
OT_COAP_OPTION_URI_PATH = 11,
OT_COAP_OPTION_CONTENT_FORMAT = 12,
OT_COAP_OPTION_MAX_AGE = 14,
OT_COAP_OPTION_URI_QUERY = 15,
OT_COAP_OPTION_ACCEPT = 17,
OT_COAP_OPTION_LOCATION_QUERY = 20,
OT_COAP_OPTION_BLOCK2 = 23,
OT_COAP_OPTION_BLOCK1 = 27,
OT_COAP_OPTION_SIZE2 = 28,
OT_COAP_OPTION_PROXY_URI = 35,
OT_COAP_OPTION_PROXY_SCHEME = 39,
OT_COAP_OPTION_SIZE1 = 60
}
CoAP Option Numbers.
enum otCoapOptionContentFormat {
OT_COAP_OPTION_CONTENT_FORMAT_TEXT_PLAIN = 0,
OT_COAP_OPTION_CONTENT_FORMAT_COSE_ENCRYPT0 = 16,
OT_COAP_OPTION_CONTENT_FORMAT_COSE_MAC0 = 17,
OT_COAP_OPTION_CONTENT_FORMAT_COSE_SIGN1 = 18,
OT_COAP_OPTION_CONTENT_FORMAT_LINK_FORMAT = 40,
OT_COAP_OPTION_CONTENT_FORMAT_XML = 41,
OT_COAP_OPTION_CONTENT_FORMAT_OCTET_STREAM = 42,
OT_COAP_OPTION_CONTENT_FORMAT_EXI = 47,
OT_COAP_OPTION_CONTENT_FORMAT_JSON = 50,
OT_COAP_OPTION_CONTENT_FORMAT_JSON_PATCH_JSON = 51,
OT_COAP_OPTION_CONTENT_FORMAT_MERGE_PATCH_JSON = 52,
OT_COAP_OPTION_CONTENT_FORMAT_CBOR = 60,
OT_COAP_OPTION_CONTENT_FORMAT_CWT = 61,
OT_COAP_OPTION_CONTENT_FORMAT_COSE_ENCRYPT = 96,
OT_COAP_OPTION_CONTENT_FORMAT_COSE_MAC = 97,
OT_COAP_OPTION_CONTENT_FORMAT_COSE_SIGN = 98,
OT_COAP_OPTION_CONTENT_FORMAT_COSE_KEY = 101,
OT_COAP_OPTION_CONTENT_FORMAT_COSE_KEY_SET = 102,
OT_COAP_OPTION_CONTENT_FORMAT_SENML_JSON = 110,
OT_COAP_OPTION_CONTENT_FORMAT_SENSML_JSON = 111,
OT_COAP_OPTION_CONTENT_FORMAT_SENML_CBOR = 112,
OT_COAP_OPTION_CONTENT_FORMAT_SENSML_CBOR = 113,
OT_COAP_OPTION_CONTENT_FORMAT_SENML_EXI = 114,
OT_COAP_OPTION_CONTENT_FORMAT_SENSML_EXI = 115,
OT_COAP_OPTION_CONTENT_FORMAT_COAP_GROUP_JSON = 256,
OT_COAP_OPTION_CONTENT_FORMAT_SENML_XML = 310,
OT_COAP_OPTION_CONTENT_FORMAT_SENSML_XML = 311
}
CoAP Content Format codes.
enum otCoapBlockSzx {
OT_COAP_OPTION_BLOCK_SZX_16 = 0,
OT_COAP_OPTION_BLOCK_SZX_32 = 1,
OT_COAP_OPTION_BLOCK_SZX_64 = 2,
OT_COAP_OPTION_BLOCK_SZX_128 = 3,
OT_COAP_OPTION_BLOCK_SZX_256 = 4,
OT_COAP_OPTION_BLOCK_SZX_512 = 5,
OT_COAP_OPTION_BLOCK_SZX_1024 = 6
}
CoAP Block Size Exponents.

Functions

void otCoapMessageInit ( otMessage *aMessage, otCoapType aType, otCoapCode aCode)
This function initializes the CoAP header.
otError otCoapMessageInitResponse ( otMessage *aResponse, const otMessage *aRequest, otCoapType aType, otCoapCode aCode)
This function initializes a response message.
otError otCoapMessageSetToken ( otMessage *aMessage, const uint8_t *aToken, uint8_t aTokenLength)
This function sets the Token value and length in a header.
void otCoapMessageGenerateToken ( otMessage *aMessage, uint8_t aTokenLength)
This function sets the Token length and randomizes its value.
otError otCoapMessageAppendContentFormatOption ( otMessage *aMessage, otCoapOptionContentFormat aContentFormat)
This function appends the Content Format CoAP option as specified in https://tools.ietf.org/html/rfc7252#page-92 .
otError otCoapMessageAppendOption ( otMessage *aMessage, uint16_t aNumber, uint16_t aLength, const void *aValue)
This function appends a CoAP option in a header.
otError otCoapMessageAppendUintOption ( otMessage *aMessage, uint16_t aNumber, uint32_t aValue)
This function appends an unsigned integer CoAP option as specified in https://tools.ietf.org/html/rfc7252#section-3.2 .
otError otCoapMessageAppendObserveOption ( otMessage *aMessage, uint32_t aObserve)
This function appends an Observe option.
otError otCoapMessageAppendUriPathOptions ( otMessage *aMessage, const char *aUriPath)
This function appends a Uri-Path option.
uint16_t otCoapBlockSizeFromExponent ( otCoapBlockSzx aSize)
This function converts a CoAP Block option SZX field to the actual block size.
otError otCoapMessageAppendBlock2Option ( otMessage *aMessage, uint32_t aNum, bool aMore, otCoapBlockSzx aSize)
This function appends a Block2 option.
otError otCoapMessageAppendBlock1Option ( otMessage *aMessage, uint32_t aNum, bool aMore, otCoapBlockSzx aSize)
This function appends a Block1 option.
otError otCoapMessageAppendProxyUriOption ( otMessage *aMessage, const char *aUriPath)
This function appends a Proxy-Uri option.
otError otCoapMessageAppendMaxAgeOption ( otMessage *aMessage, uint32_t aMaxAge)
This function appends a Max-Age option.
otError otCoapMessageAppendUriQueryOption ( otMessage *aMessage, const char *aUriQuery)
This function appends a single Uri-Query option.
otError otCoapMessageSetPayloadMarker ( otMessage *aMessage)
This function adds Payload Marker indicating beginning of the payload to the CoAP header.
otCoapType otCoapMessageGetType (const otMessage *aMessage)
This function returns the Type value.
otCoapCode otCoapMessageGetCode (const otMessage *aMessage)
This function returns the Code value.
const char * otCoapMessageCodeToString (const otMessage *aMessage)
This method returns the CoAP Code as human readable string.
uint16_t otCoapMessageGetMessageId (const otMessage *aMessage)
This function returns the Message ID value.
uint8_t otCoapMessageGetTokenLength (const otMessage *aMessage)
This function returns the Token length.
const uint8_t * otCoapMessageGetToken (const otMessage *aMessage)
This function returns a pointer to the Token value.
otError otCoapOptionIteratorInit ( otCoapOptionIterator *aIterator, const otMessage *aMessage)
This function initialises an iterator for the options in the given message.
const otCoapOption * otCoapOptionIteratorGetFirstOptionMatching ( otCoapOptionIterator *aIterator, uint16_t aOption)
This function returns a pointer to the first option matching the specified option number.
const otCoapOption * otCoapOptionIteratorGetFirstOption ( otCoapOptionIterator *aIterator)
This function returns a pointer to the first option.
const otCoapOption * otCoapOptionIteratorGetNextOptionMatching ( otCoapOptionIterator *aIterator, uint16_t aOption)
This function returns a pointer to the next option matching the specified option number.
const otCoapOption * otCoapOptionIteratorGetNextOption ( otCoapOptionIterator *aIterator)
This function returns a pointer to the next option.
otError otCoapOptionIteratorGetOptionUintValue ( otCoapOptionIterator *aIterator, uint64_t *aValue)
This function fills current option value into aValue assuming the current value is an unsigned integer encoded according to https://tools.ietf.org/html/rfc7252#section-3.2 .
otError otCoapOptionIteratorGetOptionValue ( otCoapOptionIterator *aIterator, void *aValue)
This function fills current option value into aValue .
otMessage * otCoapNewMessage ( otInstance *aInstance, const otMessageSettings *aSettings)
This function creates a new CoAP message.
otError otCoapSendRequestWithParameters ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext, const otCoapTxParameters *aTxParameters)
This function sends a CoAP request with custom transmission parameters.
otError otCoapSendRequestBlockWiseWithParameters ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext, const otCoapTxParameters *aTxParameters, otCoapBlockwiseTransmitHook aTransmitHook, otCoapBlockwiseReceiveHook aReceiveHook)
This function sends a CoAP request block-wise with custom transmission parameters.
static otError otCoapSendRequestBlockWise ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext, otCoapBlockwiseTransmitHook aTransmitHook, otCoapBlockwiseReceiveHook aReceiveHook)
This function sends a CoAP request block-wise.
static otError otCoapSendRequest ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, otCoapResponseHandler aHandler, void *aContext)
This function sends a CoAP request.
otError otCoapStart ( otInstance *aInstance, uint16_t aPort)
This function starts the CoAP server.
otError otCoapStop ( otInstance *aInstance)
This function stops the CoAP server.
void otCoapAddResource ( otInstance *aInstance, otCoapResource *aResource)
This function adds a resource to the CoAP server.
void otCoapRemoveResource ( otInstance *aInstance, otCoapResource *aResource)
This function removes a resource from the CoAP server.
void otCoapAddBlockWiseResource ( otInstance *aInstance, otCoapBlockwiseResource *aResource)
This function adds a block-wise resource to the CoAP server.
void otCoapRemoveBlockWiseResource ( otInstance *aInstance, otCoapBlockwiseResource *aResource)
This function removes a block-wise resource from the CoAP server.
void otCoapSetDefaultHandler ( otInstance *aInstance, otCoapRequestHandler aHandler, void *aContext)
This function sets the default handler for unhandled CoAP requests.
otError otCoapSendResponseWithParameters ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, const otCoapTxParameters *aTxParameters)
This function sends a CoAP response from the server with custom transmission parameters.
otError otCoapSendResponseBlockWiseWithParameters ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, const otCoapTxParameters *aTxParameters, void *aContext, otCoapBlockwiseTransmitHook aTransmitHook)
This function sends a CoAP response block-wise from the server with custom transmission parameters.
static otError otCoapSendResponseBlockWise ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext, otCoapBlockwiseTransmitHook aTransmitHook)
This function sends a CoAP response block-wise from the server.
static otError otCoapSendResponse ( otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo)
This function sends a CoAP response from the server.

Detailed Description

This module includes functions that control CoAP communication.

The functions in this module are available when CoAP API feature ( OPENTHREAD_CONFIG_COAP_API_ENABLE ) is enabled.

Typedef Documentation

◆ otCoapBlockwiseReceiveHook

typedef otError (* otCoapBlockwiseReceiveHook) (void *aContext, const uint8_t *aBlock, uint32_t aPosition, uint16_t aBlockLength, bool aMore, uint32_t aTotalLength)

This function pointer is called when a CoAP message with an block-wise transfer option is received.

This function is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

Parameters
[in] aContext A pointer to application-specific context.
[in] aBlock A pointer to the block segment.
[in] aPosition The position of aBlock in a sequence in bytes.
[in] aBlockLength The length of the block segment in bytes.
[in] aMore Flag if more block segments are following.
[in] aTotalLength The total length in bytes of the transferred information (indicated by a Size1 or Size2 option).
Return values
OT_ERROR_NONE Block segment was stored successfully.
OT_ERROR_NO_BUFS No more memory to store blocks.
OT_ERROR_NO_FRAME_RECEIVED Block segment missing.

◆ otCoapBlockwiseTransmitHook

typedef otError (* otCoapBlockwiseTransmitHook) (void *aContext, uint8_t *aBlock, uint32_t aPosition, uint16_t *aBlockLength, bool *aMore)

This function pointer is called before the next block in a block-wise transfer is sent.

This function is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

Parameters
[in] aContext A pointer to application-specific context.
[in,out] aBlock A pointer to where the block segment can be written to.
[in] aPosition The position in a sequence from which to obtain the block segment.
[in,out] aBlockLength On entry, the maximum block segment length in bytes.
[out] aMore A pointer to the flag if more block segments will follow.
Warning
By changing the value of aBlockLength, the block size of the whole exchange is renegotiated. It is recommended to do this after the first block has been received as later changes could cause problems with other CoAP implementations.
Return values
OT_ERROR_NONE No error occurred.
OT_ERROR_INVALID_ARGS Block at aPosition does not exist.

◆ otCoapOptionContentFormat

◆ otCoapOptionIterator

This structure acts as an iterator for CoAP options.

◆ otCoapRequestHandler

typedef void(* otCoapRequestHandler) (void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo)

This function pointer is called when a CoAP request with a given Uri-Path is received.

Parameters
[in] aContext A pointer to arbitrary context information.
[in] aMessage A pointer to the message.
[in] aMessageInfo A pointer to the message info for aMessage .

◆ otCoapResponseHandler

typedef void(* otCoapResponseHandler) (void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo, otError aResult)

This function pointer is called when a CoAP response is received or on the request timeout.

Parameters
[in] aContext A pointer to application-specific context.
[in] aMessage A pointer to the message buffer containing the response. NULL if no response was received.
[in] aMessageInfo A pointer to the message info for aMessage . NULL if no response was received.
[in] aResult A result of the CoAP transaction.
Return values
OT_ERROR_NONE A response was received successfully.
OT_ERROR_ABORT A CoAP transaction was reset by peer.
OT_ERROR_RESPONSE_TIMEOUT No response or acknowledgment received during timeout period.

◆ otCoapTxParameters

This structure represents the CoAP transmission parameters.

Note
mAckTimeout * ((2 ** (mMaxRetransmit + 1)) - 1) * (mAckRandomFactorNumerator / mAckRandomFactorDenominator) must not exceed what can be represented by a uint32_t (0xffffffff). This limitation allows OpenThread to avoid 64-bit arithmetic.

Enumeration Type Documentation

◆ otCoapCode

CoAP Code values.

Enumerator
OT_COAP_CODE_EMPTY

Empty message code.

OT_COAP_CODE_GET

Get.

OT_COAP_CODE_POST

Post.

OT_COAP_CODE_PUT

Put.

OT_COAP_CODE_DELETE

Delete.

OT_COAP_CODE_RESPONSE_MIN

2.00

OT_COAP_CODE_CREATED

Created.

OT_COAP_CODE_DELETED

Deleted.

OT_COAP_CODE_VALID

Valid.

OT_COAP_CODE_CHANGED

Changed.

OT_COAP_CODE_CONTENT

Content.

OT_COAP_CODE_CONTINUE

RFC7959 Continue.

OT_COAP_CODE_BAD_REQUEST

Bad Request.

OT_COAP_CODE_UNAUTHORIZED

Unauthorized.

OT_COAP_CODE_BAD_OPTION

Bad Option.

OT_COAP_CODE_FORBIDDEN

Forbidden.

OT_COAP_CODE_NOT_FOUND

Not Found.

OT_COAP_CODE_METHOD_NOT_ALLOWED

Method Not Allowed.

OT_COAP_CODE_NOT_ACCEPTABLE

Not Acceptable.

OT_COAP_CODE_REQUEST_INCOMPLETE

RFC7959 Request Entity Incomplete.

OT_COAP_CODE_PRECONDITION_FAILED

Precondition Failed.

OT_COAP_CODE_REQUEST_TOO_LARGE

Request Entity Too Large.

OT_COAP_CODE_UNSUPPORTED_FORMAT

Unsupported Content-Format.

OT_COAP_CODE_INTERNAL_ERROR

Internal Server Error.

OT_COAP_CODE_NOT_IMPLEMENTED

Not Implemented.

OT_COAP_CODE_BAD_GATEWAY

Bad Gateway.

OT_COAP_CODE_SERVICE_UNAVAILABLE

Service Unavailable.

OT_COAP_CODE_GATEWAY_TIMEOUT

Gateway Timeout.

OT_COAP_CODE_PROXY_NOT_SUPPORTED

Proxying Not Supported.

◆ otCoapOptionContentFormat

CoAP Content Format codes.

The full list is documented at https://www.iana.org/assignments/core-parameters/core-parameters.xhtml#content-formats

Enumerator
OT_COAP_OPTION_CONTENT_FORMAT_TEXT_PLAIN

text/plain; charset=utf-8: [RFC2046][RFC3676][RFC5147]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_ENCRYPT0

application/cose; cose-type="cose-encrypt0": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_MAC0

application/cose; cose-type="cose-mac0": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_SIGN1

application/cose; cose-type="cose-sign1": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_LINK_FORMAT

application/link-format: [RFC6690]

OT_COAP_OPTION_CONTENT_FORMAT_XML

application/xml: [RFC3023]

OT_COAP_OPTION_CONTENT_FORMAT_OCTET_STREAM

application/octet-stream: [RFC2045][RFC2046]

OT_COAP_OPTION_CONTENT_FORMAT_EXI

application/exi: ["Efficient XML Interchange (EXI) Format 1.0 (Second Edition)", February 2014]

OT_COAP_OPTION_CONTENT_FORMAT_JSON

application/json: [RFC7159]

OT_COAP_OPTION_CONTENT_FORMAT_JSON_PATCH_JSON

application/json-patch+json: [RFC6902]

OT_COAP_OPTION_CONTENT_FORMAT_MERGE_PATCH_JSON

application/merge-patch+json: [RFC7396]

OT_COAP_OPTION_CONTENT_FORMAT_CBOR

application/cbor: [RFC7049]

OT_COAP_OPTION_CONTENT_FORMAT_CWT

application/cwt: [RFC8392]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_ENCRYPT

application/cose; cose-type="cose-encrypt": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_MAC

application/cose; cose-type="cose-mac": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_SIGN

application/cose; cose-type="cose-sign": [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_KEY

application/cose-key: [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_COSE_KEY_SET

application/cose-key-set: [RFC8152]

OT_COAP_OPTION_CONTENT_FORMAT_SENML_JSON

application/senml+json: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENSML_JSON

application/sensml+json: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENML_CBOR

application/senml+cbor: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENSML_CBOR

application/sensml+cbor: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENML_EXI

application/senml-exi: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENSML_EXI

application/sensml-exi: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_COAP_GROUP_JSON

application/coap-group+json: [RFC7390]

OT_COAP_OPTION_CONTENT_FORMAT_SENML_XML

application/senml+xml: [RFC8428]

OT_COAP_OPTION_CONTENT_FORMAT_SENSML_XML

application/sensml+xml: [RFC8428]

◆ otCoapOptionType

CoAP Option Numbers.

Enumerator
OT_COAP_OPTION_IF_MATCH

If-Match.

OT_COAP_OPTION_URI_HOST

Uri-Host.

OT_COAP_OPTION_E_TAG

ETag.

OT_COAP_OPTION_IF_NONE_MATCH

If-None-Match.

OT_COAP_OPTION_OBSERVE

Observe [RFC7641].

OT_COAP_OPTION_URI_PORT

Uri-Port.

OT_COAP_OPTION_LOCATION_PATH

Location-Path.

OT_COAP_OPTION_URI_PATH

Uri-Path.

OT_COAP_OPTION_CONTENT_FORMAT

Content-Format.

OT_COAP_OPTION_MAX_AGE

Max-Age.

OT_COAP_OPTION_URI_QUERY

Uri-Query.

OT_COAP_OPTION_ACCEPT

Accept.

OT_COAP_OPTION_LOCATION_QUERY

Location-Query.

OT_COAP_OPTION_BLOCK2

Block2 (RFC7959)

OT_COAP_OPTION_BLOCK1

Block1 (RFC7959)

OT_COAP_OPTION_SIZE2

Size2 (RFC7959)

OT_COAP_OPTION_PROXY_URI

Proxy-Uri.

OT_COAP_OPTION_PROXY_SCHEME

Proxy-Scheme.

OT_COAP_OPTION_SIZE1

Size1.

◆ otCoapType

CoAP Type values (2 bit unsigned integer).

Enumerator
OT_COAP_TYPE_CONFIRMABLE

Confirmable.

OT_COAP_TYPE_NON_CONFIRMABLE

Non-confirmable.

OT_COAP_TYPE_ACKNOWLEDGMENT

Acknowledgment.

OT_COAP_TYPE_RESET

Reset.

Function Documentation

◆ otCoapAddBlockWiseResource()

void otCoapAddBlockWiseResource ( otInstance * aInstance,
otCoapBlockwiseResource * aResource
)

This function adds a block-wise resource to the CoAP server.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aResource A pointer to the resource.

◆ otCoapAddResource()

void otCoapAddResource ( otInstance * aInstance,
otCoapResource * aResource
)

This function adds a resource to the CoAP server.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aResource A pointer to the resource.

◆ otCoapBlockSizeFromExponent()

uint16_t otCoapBlockSizeFromExponent ( otCoapBlockSzx aSize )

This function converts a CoAP Block option SZX field to the actual block size.

Parameters
[in] aSize Block size exponent.
Returns
The actual size exponent value.

◆ otCoapMessageAppendBlock1Option()

otError otCoapMessageAppendBlock1Option ( otMessage * aMessage,
uint32_t aNum,
bool aMore,
otCoapBlockSzx aSize
)

This function appends a Block1 option.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aNum Current block number.
[in] aMore Boolean to indicate more blocks are to be sent.
[in] aSize Block Size Exponent.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageAppendBlock2Option()

otError otCoapMessageAppendBlock2Option ( otMessage * aMessage,
uint32_t aNum,
bool aMore,
otCoapBlockSzx aSize
)

This function appends a Block2 option.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aNum Current block number.
[in] aMore Boolean to indicate more blocks are to be sent.
[in] aSize Block Size Exponent.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageAppendContentFormatOption()

otError otCoapMessageAppendContentFormatOption ( otMessage * aMessage,
otCoapOptionContentFormat aContentFormat
)

This function appends the Content Format CoAP option as specified in https://tools.ietf.org/html/rfc7252#page-92 .

This must be called before setting otCoapMessageSetPayloadMarker if a payload is to be included in the message.

The function is a convenience wrapper around otCoapMessageAppendUintOption, and if the desired format type code isn't listed in otCoapOptionContentFormat, this base function should be used instead.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aContentFormat One of the content formats listed in otCoapOptionContentFormat above.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageAppendMaxAgeOption()

otError otCoapMessageAppendMaxAgeOption ( otMessage * aMessage,
uint32_t aMaxAge
)

This function appends a Max-Age option.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aMaxAge The Max-Age value.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageAppendObserveOption()

otError otCoapMessageAppendObserveOption ( otMessage * aMessage,
uint32_t aObserve
)

This function appends an Observe option.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aObserve Observe field value.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageAppendOption()

otError otCoapMessageAppendOption ( otMessage * aMessage,
uint16_t aNumber,
uint16_t aLength,
const void * aValue
)

This function appends a CoAP option in a header.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aNumber The CoAP Option number.
[in] aLength The CoAP Option length.
[in] aValue A pointer to the CoAP value.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageAppendProxyUriOption()

otError otCoapMessageAppendProxyUriOption ( otMessage * aMessage,
const char * aUriPath
)

This function appends a Proxy-Uri option.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aUriPath A pointer to a NULL-terminated string.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageAppendUintOption()

otError otCoapMessageAppendUintOption ( otMessage * aMessage,
uint16_t aNumber,
uint32_t aValue
)

This function appends an unsigned integer CoAP option as specified in https://tools.ietf.org/html/rfc7252#section-3.2 .

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aNumber The CoAP Option number.
[in] aValue The CoAP Option unsigned integer value.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.
See also
otCoapMessageGetOptionUintValue

◆ otCoapMessageAppendUriPathOptions()

otError otCoapMessageAppendUriPathOptions ( otMessage * aMessage,
const char * aUriPath
)

This function appends a Uri-Path option.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aUriPath A pointer to a NULL-terminated string.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageAppendUriQueryOption()

otError otCoapMessageAppendUriQueryOption ( otMessage * aMessage,
const char * aUriQuery
)

This function appends a single Uri-Query option.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aUriQuery A pointer to NULL-terminated string, which should contain a single key=value pair.
Return values
OT_ERROR_NONE Successfully appended the option.
OT_ERROR_INVALID_ARGS The option type is not equal or greater than the last option type.
OT_ERROR_NO_BUFS The option length exceeds the buffer size.

◆ otCoapMessageCodeToString()

const char* otCoapMessageCodeToString ( const otMessage * aMessage )

This method returns the CoAP Code as human readable string.

Parameters
[in] aMessage A pointer to the CoAP message.

@ returns The CoAP Code as string.

◆ otCoapMessageGenerateToken()

void otCoapMessageGenerateToken ( otMessage * aMessage,
uint8_t aTokenLength
)

This function sets the Token length and randomizes its value.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aTokenLength The Length of a Token to set.

◆ otCoapMessageGetCode()

otCoapCode otCoapMessageGetCode ( const otMessage * aMessage )

This function returns the Code value.

Parameters
[in] aMessage A pointer to the CoAP message.
Returns
The Code value.

◆ otCoapMessageGetMessageId()

uint16_t otCoapMessageGetMessageId ( const otMessage * aMessage )

This function returns the Message ID value.

Parameters
[in] aMessage A pointer to the CoAP message.
Returns
The Message ID value.

◆ otCoapMessageGetToken()

const uint8_t* otCoapMessageGetToken ( const otMessage * aMessage )

This function returns a pointer to the Token value.

Parameters
[in] aMessage A pointer to the CoAP message.
Returns
A pointer to the Token value.

◆ otCoapMessageGetTokenLength()

uint8_t otCoapMessageGetTokenLength ( const otMessage * aMessage )

This function returns the Token length.

Parameters
[in] aMessage A pointer to the CoAP message.
Returns
The Token length.

◆ otCoapMessageGetType()

otCoapType otCoapMessageGetType ( const otMessage * aMessage )

This function returns the Type value.

Parameters
[in] aMessage A pointer to the CoAP message.
Returns
The Type value.

◆ otCoapMessageInit()

void otCoapMessageInit ( otMessage * aMessage,
otCoapType aType,
otCoapCode aCode
)

This function initializes the CoAP header.

Parameters
[in,out] aMessage A pointer to the CoAP message to initialize.
[in] aType CoAP message type.
[in] aCode CoAP message code.

◆ otCoapMessageInitResponse()

otError otCoapMessageInitResponse ( otMessage * aResponse,
const otMessage * aRequest,
otCoapType aType,
otCoapCode aCode
)

This function initializes a response message.

Note
Both message ID and token are set according to aRequest .
Parameters
[in,out] aResponse A pointer to the CoAP response message.
[in] aRequest A pointer to the CoAP request message.
[in] aType CoAP message type.
[in] aCode CoAP message code.
Return values
OT_ERROR_NONE Successfully initialized the response message.
OT_ERROR_NO_BUFS Insufficient message buffers available to initialize the response message.

◆ otCoapMessageSetPayloadMarker()

otError otCoapMessageSetPayloadMarker ( otMessage * aMessage )

This function adds Payload Marker indicating beginning of the payload to the CoAP header.

Parameters
[in,out] aMessage A pointer to the CoAP message.
Return values
OT_ERROR_NONE Payload Marker successfully added.
OT_ERROR_NO_BUFS Header Payload Marker exceeds the buffer size.

◆ otCoapMessageSetToken()

otError otCoapMessageSetToken ( otMessage * aMessage,
const uint8_t * aToken,
uint8_t aTokenLength
)

This function sets the Token value and length in a header.

Parameters
[in,out] aMessage A pointer to the CoAP message.
[in] aToken A pointer to the Token value.
[in] aTokenLength The Length of aToken .
Return values
OT_ERROR_NONE Successfully set the Token value.
OT_ERROR_NO_BUFS Insufficient buffers to set the Token value.

◆ otCoapNewMessage()

otMessage * otCoapNewMessage ( otInstance * aInstance,
const otMessageSettings * aSettings
)

This function creates a new CoAP message.

Note
If aSettings is 'NULL', the link layer security is enabled and the message priority is set to OT_MESSAGE_PRIORITY_NORMAL by default.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aSettings A pointer to the message settings or NULL to set default settings.
Returns
A pointer to the message buffer or NULL if no message buffers are available or parameters are invalid.

◆ otCoapOptionIteratorGetFirstOption()

const otCoapOption * otCoapOptionIteratorGetFirstOption ( otCoapOptionIterator * aIterator )

This function returns a pointer to the first option.

Parameters
[in,out] aIterator A pointer to the CoAP message option iterator.
Returns
A pointer to the first option. If no option is present NULL pointer is returned.

◆ otCoapOptionIteratorGetFirstOptionMatching()

const otCoapOption * otCoapOptionIteratorGetFirstOptionMatching ( otCoapOptionIterator * aIterator,
uint16_t aOption
)

This function returns a pointer to the first option matching the specified option number.

Parameters
[in] aIterator A pointer to the CoAP message option iterator.
[in] aOption The option number sought.
Returns
A pointer to the first matching option. If no matching option is present NULL pointer is returned.

◆ otCoapOptionIteratorGetNextOption()

const otCoapOption * otCoapOptionIteratorGetNextOption ( otCoapOptionIterator * aIterator )

This function returns a pointer to the next option.

Parameters
[in,out] aIterator A pointer to the CoAP message option iterator.
Returns
A pointer to the next option. If no more options are present NULL pointer is returned.

◆ otCoapOptionIteratorGetNextOptionMatching()

const otCoapOption * otCoapOptionIteratorGetNextOptionMatching ( otCoapOptionIterator * aIterator,
uint16_t aOption
)

This function returns a pointer to the next option matching the specified option number.

Parameters
[in] aIterator A pointer to the CoAP message option iterator.
[in] aOption The option number sought.
Returns
A pointer to the next matching option. If no further matching option is present NULL pointer is returned.

◆ otCoapOptionIteratorGetOptionUintValue()

otError otCoapOptionIteratorGetOptionUintValue ( otCoapOptionIterator * aIterator,
uint64_t * aValue
)

This function fills current option value into aValue assuming the current value is an unsigned integer encoded according to https://tools.ietf.org/html/rfc7252#section-3.2 .

Parameters
[in,out] aIterator A pointer to the CoAP message option iterator.
[out] aValue A pointer to an unsigned integer to receive the option value.
Return values
OT_ERROR_NONE Successfully filled value.
OT_ERROR_NOT_FOUND No current option.
OT_ERROR_NO_BUFS Value is too long to fit in a uint64_t.
See also
otCoapMessageAppendUintOption

◆ otCoapOptionIteratorGetOptionValue()

otError otCoapOptionIteratorGetOptionValue ( otCoapOptionIterator * aIterator,
void * aValue
)

This function fills current option value into aValue .

Parameters
[in,out] aIterator A pointer to the CoAP message option iterator.
[out] aValue A pointer to a buffer to receive the option value.
Return values
OT_ERROR_NONE Successfully filled value.
OT_ERROR_NOT_FOUND No current option.

◆ otCoapOptionIteratorInit()

otError otCoapOptionIteratorInit ( otCoapOptionIterator * aIterator,
const otMessage * aMessage
)

This function initialises an iterator for the options in the given message.

Parameters
[in,out] aIterator A pointer to the CoAP message option iterator.
[in] aMessage A pointer to the CoAP message.
Return values
OT_ERROR_NONE Successfully initialised.
OT_ERROR_PARSE Message state is inconsistent.

◆ otCoapRemoveBlockWiseResource()

void otCoapRemoveBlockWiseResource ( otInstance * aInstance,
otCoapBlockwiseResource * aResource
)

This function removes a block-wise resource from the CoAP server.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aResource A pointer to the resource.

◆ otCoapRemoveResource()

void otCoapRemoveResource ( otInstance * aInstance,
otCoapResource * aResource
)

This function removes a resource from the CoAP server.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aResource A pointer to the resource.

◆ otCoapSendRequest()

static otError otCoapSendRequest ( otInstance * aInstance,
otMessage * aMessage,
const otMessageInfo * aMessageInfo,
otCoapResponseHandler aHandler,
void * aContext
)
inline static

This function sends a CoAP request.

If a response for a request is expected, respective function and context information should be provided. If no response is expected, these arguments should be NULL pointers.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to the message to send.
[in] aMessageInfo A pointer to the message info associated with aMessage .
[in] aHandler A function pointer that shall be called on response reception or timeout.
[in] aContext A pointer to arbitrary context information. May be NULL if not used.
Return values
OT_ERROR_NONE Successfully sent CoAP message.
OT_ERROR_NO_BUFS Failed to allocate retransmission data.

◆ otCoapSendRequestBlockWise()

static otError otCoapSendRequestBlockWise ( otInstance * aInstance,
otMessage * aMessage,
const otMessageInfo * aMessageInfo,
otCoapResponseHandler aHandler,
void * aContext,
otCoapBlockwiseTransmitHook aTransmitHook,
otCoapBlockwiseReceiveHook aReceiveHook
)
inline static

This function sends a CoAP request block-wise.

This function is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

If a response for a request is expected, respective function and context information should be provided. If the response is expected to be block-wise, a respective hook function should be provided. If no response is expected, these arguments should be NULL pointers.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to the message to send.
[in] aMessageInfo A pointer to the message info associated with aMessage .
[in] aHandler A function pointer that shall be called on response reception or timeout.
[in] aContext A pointer to arbitrary context information. May be NULL if not used.
[in] aTransmitHook A pointer to a hook function for outgoing block-wise transfer.
[in] aReceiveHook A pointer to a hook function for incoming block-wise transfer.
Return values
OT_ERROR_NONE Successfully sent CoAP message.
OT_ERROR_NO_BUFS Failed to allocate retransmission data.

◆ otCoapSendRequestBlockWiseWithParameters()

otError otCoapSendRequestBlockWiseWithParameters ( otInstance * aInstance,
otMessage * aMessage,
const otMessageInfo * aMessageInfo,
otCoapResponseHandler aHandler,
void * aContext,
const otCoapTxParameters * aTxParameters,
otCoapBlockwiseTransmitHook aTransmitHook,
otCoapBlockwiseReceiveHook aReceiveHook
)

This function sends a CoAP request block-wise with custom transmission parameters.

This function is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

If a response for a request is expected, respective function and context information should be provided. If the response is expected to be block-wise, a respective hook function should be provided. If no response is expected, these arguments should be NULL pointers.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to the message to send.
[in] aMessageInfo A pointer to the message info associated with aMessage .
[in] aHandler A function pointer that shall be called on response reception or timeout.
[in] aContext A pointer to arbitrary context information. May be NULL if not used.
[in] aTxParameters A pointer to transmission parameters for this request. Use NULL for defaults.
[in] aTransmitHook A pointer to a hook function for outgoing block-wise transfer.
[in] aReceiveHook A pointer to a hook function for incoming block-wise transfer.
Return values
OT_ERROR_NONE Successfully sent CoAP message.
OT_ERROR_NO_BUFS Failed to allocate retransmission data.

◆ otCoapSendRequestWithParameters()

otError otCoapSendRequestWithParameters ( otInstance * aInstance,
otMessage * aMessage,
const otMessageInfo * aMessageInfo,
otCoapResponseHandler aHandler,
void * aContext,
const otCoapTxParameters * aTxParameters
)

This function sends a CoAP request with custom transmission parameters.

If a response for a request is expected, respective function and context information should be provided. If no response is expected, these arguments should be NULL pointers.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to the message to send.
[in] aMessageInfo A pointer to the message info associated with aMessage .
[in] aHandler A function pointer that shall be called on response reception or timeout.
[in] aContext A pointer to arbitrary context information. May be NULL if not used.
[in] aTxParameters A pointer to transmission parameters for this request. Use NULL for defaults. Otherwise, parameters given must meet the following conditions:
  1. mMaxRetransmit is no more than OT_COAP_MAX_RETRANSMIT.
  2. mAckRandomFactorNumerator / mAckRandomFactorDenominator must not be below 1.0.
  3. The calculated exchange life time must not overflow uint32_t.
Return values
OT_ERROR_INVALID_ARGS aTxParameters is invalid.
OT_ERROR_NONE Successfully sent CoAP message.
OT_ERROR_NO_BUFS Failed to allocate retransmission data.

◆ otCoapSendResponse()

static otError otCoapSendResponse ( otInstance * aInstance,
otMessage * aMessage,
const otMessageInfo * aMessageInfo
)
inline static

This function sends a CoAP response from the server.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to the CoAP response to send.
[in] aMessageInfo A pointer to the message info associated with aMessage .
Return values
OT_ERROR_NONE Successfully enqueued the CoAP response message.
OT_ERROR_NO_BUFS Insufficient buffers available to send the CoAP response.

◆ otCoapSendResponseBlockWise()

static otError otCoapSendResponseBlockWise ( otInstance * aInstance,
otMessage * aMessage,
const otMessageInfo * aMessageInfo,
void * aContext,
otCoapBlockwiseTransmitHook aTransmitHook
)
inline static

This function sends a CoAP response block-wise from the server.

This function is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to the CoAP response to send.
[in] aMessageInfo A pointer to the message info associated with aMessage .
[in] aContext A pointer to arbitrary context information. May be NULL if not used.
[in] aTransmitHook A pointer to a hook function for outgoing block-wise transfer.
Return values
OT_ERROR_NONE Successfully enqueued the CoAP response message.
OT_ERROR_NO_BUFS Insufficient buffers available to send the CoAP response.

◆ otCoapSendResponseBlockWiseWithParameters()

otError otCoapSendResponseBlockWiseWithParameters ( otInstance * aInstance,
otMessage * aMessage,
const otMessageInfo * aMessageInfo,
const otCoapTxParameters * aTxParameters,
void * aContext,
otCoapBlockwiseTransmitHook aTransmitHook
)

This function sends a CoAP response block-wise from the server with custom transmission parameters.

This function is available when OPENTHREAD_CONFIG_COAP_BLOCKWISE_TRANSFER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to the CoAP response to send.
[in] aMessageInfo A pointer to the message info associated with aMessage .
[in] aTxParameters A pointer to transmission parameters for this response. Use NULL for defaults.
[in] aContext A pointer to arbitrary context information. May be NULL if not used.
[in] aTransmitHook A pointer to a hook function for outgoing block-wise transfer.
Return values
OT_ERROR_NONE Successfully enqueued the CoAP response message.
OT_ERROR_NO_BUFS Insufficient buffers available to send the CoAP response.

◆ otCoapSendResponseWithParameters()

otError otCoapSendResponseWithParameters ( otInstance * aInstance,
otMessage * aMessage,
const otMessageInfo * aMessageInfo,
const otCoapTxParameters * aTxParameters
)

This function sends a CoAP response from the server with custom transmission parameters.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMessage A pointer to the CoAP response to send.
[in] aMessageInfo A pointer to the message info associated with aMessage .
[in] aTxParameters A pointer to transmission parameters for this response. Use NULL for defaults.
Return values
OT_ERROR_NONE Successfully enqueued the CoAP response message.
OT_ERROR_NO_BUFS Insufficient buffers available to send the CoAP response.

◆ otCoapSetDefaultHandler()

void otCoapSetDefaultHandler ( otInstance * aInstance,
otCoapRequestHandler aHandler,
void * aContext
)

This function sets the default handler for unhandled CoAP requests.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aHandler A function pointer that shall be called when an unhandled request arrives.
[in] aContext A pointer to arbitrary context information. May be NULL if not used.

◆ otCoapStart()

otError otCoapStart ( otInstance * aInstance,
uint16_t aPort
)

This function starts the CoAP server.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPort The local UDP port to bind to.
Return values
OT_ERROR_NONE Successfully started the CoAP server.
OT_ERROR_FAILED Failed to start the CoAP server.

◆ otCoapStop()

otError otCoapStop ( otInstance * aInstance )

This function stops the CoAP server.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NONE Successfully stopped the CoAP server.