This module includes functions that control link-layer configuration.

Classes

struct otThreadLinkInfo
This structure represents link-specific information for messages received from the Thread radio.
struct otMacFilterEntry
This structure represents a Mac Filter entry.
struct otMacCounters
This structure represents the MAC layer counters.
struct otActiveScanResult
This structure represents a received IEEE 802.15.4 Beacon.
struct otEnergyScanResult
This structure represents an energy scan result.

Macros

#define OT_US_PER_TEN_SYMBOLS 160
The microseconds per 10 symbols.
#define OT_MAC_FILTER_FIXED_RSS_DISABLED 127
Used to indicate no fixed received signal strength was set.
#define OT_MAC_FILTER_ITERATOR_INIT 0
Initializer for otMacFilterIterator.

Typedefs

typedef struct otThreadLinkInfo otThreadLinkInfo
This structure represents link-specific information for messages received from the Thread radio.
typedef uint8_t otMacFilterIterator
Used to iterate through mac filter entries.
typedef enum otMacFilterAddressMode otMacFilterAddressMode
Defines address mode of the mac filter.
typedef struct otMacFilterEntry otMacFilterEntry
This structure represents a Mac Filter entry.
typedef struct otMacCounters otMacCounters
This structure represents the MAC layer counters.
typedef struct otActiveScanResult otActiveScanResult
This structure represents a received IEEE 802.15.4 Beacon.
typedef struct otEnergyScanResult otEnergyScanResult
This structure represents an energy scan result.
typedef void(* otHandleActiveScanResult ) ( otActiveScanResult *aResult, void *aContext)
This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.
typedef void(* otHandleEnergyScanResult ) ( otEnergyScanResult *aResult, void *aContext)
This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.
typedef void(* otLinkPcapCallback ) (const otRadioFrame *aFrame, bool aIsTx, void *aContext)
This function pointer is called when an IEEE 802.15.4 frame is received.

Enumerations

enum otMacFilterAddressMode {
OT_MAC_FILTER_ADDRESS_MODE_DISABLED ,
OT_MAC_FILTER_ADDRESS_MODE_ALLOWLIST ,
OT_MAC_FILTER_ADDRESS_MODE_DENYLIST
}
Defines address mode of the mac filter.

Functions

otError otLinkActiveScan ( otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleActiveScanResult aCallback, void *aCallbackContext)
This function starts an IEEE 802.15.4 Active Scan.
bool otLinkIsActiveScanInProgress ( otInstance *aInstance)
This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.
otError otLinkEnergyScan ( otInstance *aInstance, uint32_t aScanChannels, uint16_t aScanDuration, otHandleEnergyScanResult aCallback, void *aCallbackContext)
This function starts an IEEE 802.15.4 Energy Scan.
bool otLinkIsEnergyScanInProgress ( otInstance *aInstance)
This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.
otError otLinkSendDataRequest ( otInstance *aInstance)
This function enqueues an IEEE 802.15.4 Data Request message for transmission.
bool otLinkIsInTransmitState ( otInstance *aInstance)
This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.
uint8_t otLinkGetChannel ( otInstance *aInstance)
Get the IEEE 802.15.4 channel.
otError otLinkSetChannel ( otInstance *aInstance, uint8_t aChannel)
Set the IEEE 802.15.4 channel.
uint32_t otLinkGetSupportedChannelMask ( otInstance *aInstance)
Get the supported channel mask of MAC layer.
otError otLinkSetSupportedChannelMask ( otInstance *aInstance, uint32_t aChannelMask)
Set the supported channel mask of MAC layer.
const otExtAddress * otLinkGetExtendedAddress ( otInstance *aInstance)
Get the IEEE 802.15.4 Extended Address.
otError otLinkSetExtendedAddress ( otInstance *aInstance, const otExtAddress *aExtAddress)
This function sets the IEEE 802.15.4 Extended Address.
void otLinkGetFactoryAssignedIeeeEui64 ( otInstance *aInstance, otExtAddress *aEui64)
Get the factory-assigned IEEE EUI-64.
otPanId otLinkGetPanId ( otInstance *aInstance)
Get the IEEE 802.15.4 PAN ID.
otError otLinkSetPanId ( otInstance *aInstance, otPanId aPanId)
Set the IEEE 802.15.4 PAN ID.
uint32_t otLinkGetPollPeriod ( otInstance *aInstance)
Get the data poll period of sleepy end device.
otError otLinkSetPollPeriod ( otInstance *aInstance, uint32_t aPollPeriod)
Set/clear user-specified/external data poll period for sleepy end device.
otShortAddress otLinkGetShortAddress ( otInstance *aInstance)
Get the IEEE 802.15.4 Short Address.
uint8_t otLinkGetMaxFrameRetriesDirect ( otInstance *aInstance)
This method returns the maximum number of frame retries during direct transmission.
void otLinkSetMaxFrameRetriesDirect ( otInstance *aInstance, uint8_t aMaxFrameRetriesDirect)
This method sets the maximum number of frame retries during direct transmission.
uint8_t otLinkGetMaxFrameRetriesIndirect ( otInstance *aInstance)
This method returns the maximum number of frame retries during indirect transmission.
void otLinkSetMaxFrameRetriesIndirect ( otInstance *aInstance, uint8_t aMaxFrameRetriesIndirect)
This method sets the maximum number of frame retries during indirect transmission.
otMacFilterAddressMode otLinkFilterGetAddressMode ( otInstance *aInstance)
This function gets the address mode of MAC filter.
void otLinkFilterSetAddressMode ( otInstance *aInstance, otMacFilterAddressMode aMode)
This function sets the address mode of MAC filter.
otError otLinkFilterAddAddress ( otInstance *aInstance, const otExtAddress *aExtAddress)
This method adds an Extended Address to MAC filter.
void otLinkFilterRemoveAddress ( otInstance *aInstance, const otExtAddress *aExtAddress)
This method removes an Extended Address from MAC filter.
void otLinkFilterClearAddresses ( otInstance *aInstance)
This method clears all the Extended Addresses from MAC filter.
otError otLinkFilterGetNextAddress ( otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry)
This method gets an in-use address filter entry.
otError otLinkFilterAddRssIn ( otInstance *aInstance, const otExtAddress *aExtAddress, int8_t aRss)
This method adds a fixed received signal strength (in dBm) entry for the messages from a given Extended Address in MAC Filter.
void otLinkFilterRemoveRssIn ( otInstance *aInstance, const otExtAddress *aExtAddress)
This method removes a MAC Filter entry for fixed received signal strength setting for a given Extended Address.
void otLinkFilterSetDefaultRssIn ( otInstance *aInstance, int8_t aRss)
This method sets the default received signal strength (in dBm) on MAC Filter.
void otLinkFilterClearDefaultRssIn ( otInstance *aInstance)
This method clears any previously set default received signal strength (in dBm) on MAC Filter.
void otLinkFilterClearAllRssIn ( otInstance *aInstance)
This method clears all the received signal strength entries (including default RSS-in) on MAC Filter.
otError otLinkFilterGetNextRssIn ( otInstance *aInstance, otMacFilterIterator *aIterator, otMacFilterEntry *aEntry)
This method gets an in-use RssIn filter entry.
uint8_t otLinkConvertRssToLinkQuality ( otInstance *aInstance, int8_t aRss)
This method converts received signal strength to link quality.
int8_t otLinkConvertLinkQualityToRss ( otInstance *aInstance, uint8_t aLinkQuality)
This method converts link quality to typical received signal strength.
const uint32_t * otLinkGetTxDirectRetrySuccessHistogram ( otInstance *aInstance, uint8_t *aNumberOfEntries)
This method gets histogram of retries for a single direct packet until success.
const uint32_t * otLinkGetTxIndirectRetrySuccessHistogram ( otInstance *aInstance, uint8_t *aNumberOfEntries)
This method gets histogram of retries for a single indirect packet until success.
void otLinkResetTxRetrySuccessHistogram ( otInstance *aInstance)
This method clears histogram statistics for direct and indirect transmissions.
const otMacCounters * otLinkGetCounters ( otInstance *aInstance)
Get the MAC layer counters.
void otLinkResetCounters ( otInstance *aInstance)
Reset the MAC layer counters.
void otLinkSetPcapCallback ( otInstance *aInstance, otLinkPcapCallback aPcapCallback, void *aCallbackContext)
This function registers a callback to provide received raw IEEE 802.15.4 frames.
bool otLinkIsPromiscuous ( otInstance *aInstance)
This function indicates whether or not promiscuous mode is enabled at the link layer.
otError otLinkSetPromiscuous ( otInstance *aInstance, bool aPromiscuous)
This function enables or disables the link layer promiscuous mode.
uint8_t otLinkCslGetChannel ( otInstance *aInstance)
This function gets the CSL channel.
otError otLinkCslSetChannel ( otInstance *aInstance, uint8_t aChannel)
This function sets the CSL channel.
uint16_t otLinkCslGetPeriod ( otInstance *aInstance)
This function gets the CSL period.
otError otLinkCslSetPeriod ( otInstance *aInstance, uint16_t aPeriod)
This function sets the CSL period.
uint32_t otLinkCslGetTimeout ( otInstance *aInstance)
This function gets the CSL timeout.
otError otLinkCslSetTimeout ( otInstance *aInstance, uint32_t aTimeout)
This function sets the CSL timeout.
uint16_t otLinkGetCcaFailureRate ( otInstance *aInstance)
This function returns the current CCA (Clear Channel Assessment) failure rate.
otError otLinkSetEnabled ( otInstance *aInstance, bool aEnable)
This function enables or disables the link layer.
bool otLinkIsEnabled ( otInstance *aInstance)
This function indicates whether or not the link layer is enabled.
otError otLinkSendEmptyData ( otInstance *aInstance)
This function instructs the device to send an empty IEEE 802.15.4 data frame.

Detailed Description

This module includes functions that control link-layer configuration.

Macro Definition Documentation

◆ OT_MAC_FILTER_FIXED_RSS_DISABLED

#define OT_MAC_FILTER_FIXED_RSS_DISABLED 127

Used to indicate no fixed received signal strength was set.

Typedef Documentation

◆ otHandleActiveScanResult

typedef void(* otHandleActiveScanResult) ( otActiveScanResult *aResult, void *aContext)

This function pointer is called during an IEEE 802.15.4 Active Scan when an IEEE 802.15.4 Beacon is received or the scan completes.

Parameters
[in] aResult A valid pointer to the beacon information or NULL when the active scan completes.
[in] aContext A pointer to application-specific context.

◆ otHandleEnergyScanResult

typedef void(* otHandleEnergyScanResult) ( otEnergyScanResult *aResult, void *aContext)

This function pointer is called during an IEEE 802.15.4 Energy Scan when the result for a channel is ready or the scan completes.

Parameters
[in] aResult A valid pointer to the energy scan result information or NULL when the energy scan completes.
[in] aContext A pointer to application-specific context.

◆ otLinkPcapCallback

typedef void(* otLinkPcapCallback) (const otRadioFrame *aFrame, bool aIsTx, void *aContext)

This function pointer is called when an IEEE 802.15.4 frame is received.

Note
This callback is called after FCS processing and aFrame may not contain the actual FCS that was received.
This callback is called before IEEE 802.15.4 security processing.
Parameters
[in] aFrame A pointer to the received IEEE 802.15.4 frame.
[in] aIsTx Whether this frame is transmitted, not received.
[in] aContext A pointer to application-specific context.

Enumeration Type Documentation

◆ otMacFilterAddressMode

Defines address mode of the mac filter.

Enumerator
OT_MAC_FILTER_ADDRESS_MODE_DISABLED

Address filter is disabled.

OT_MAC_FILTER_ADDRESS_MODE_ALLOWLIST

Allowlist address filter mode is enabled.

OT_MAC_FILTER_ADDRESS_MODE_DENYLIST

Denylist address filter mode is enabled.

Function Documentation

◆ otLinkActiveScan()

otError otLinkActiveScan ( otInstance * aInstance,
uint32_t aScanChannels,
uint16_t aScanDuration,
otHandleActiveScanResult aCallback,
void * aCallbackContext
)

This function starts an IEEE 802.15.4 Active Scan.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aScanChannels A bit vector indicating which channels to scan (e.g. OT_CHANNEL_11_MASK).
[in] aScanDuration The time in milliseconds to spend scanning each channel.
[in] aCallback A pointer to a function called on receiving a beacon or scan completes.
[in] aCallbackContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Accepted the Active Scan request.
OT_ERROR_BUSY Already performing an Active Scan.

◆ otLinkConvertLinkQualityToRss()

int8_t otLinkConvertLinkQualityToRss ( otInstance * aInstance,
uint8_t aLinkQuality
)

This method converts link quality to typical received signal strength.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aLinkQuality LinkQuality value, should be in range [0,3].
Returns
Typical platform received signal strength mapping to aLinkQuality .

◆ otLinkConvertRssToLinkQuality()

uint8_t otLinkConvertRssToLinkQuality ( otInstance * aInstance,
int8_t aRss
)

This method converts received signal strength to link quality.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aRss The received signal strength value to be converted.
Returns
Link quality value mapping to aRss .

◆ otLinkCslGetChannel()

uint8_t otLinkCslGetChannel ( otInstance * aInstance )

This function gets the CSL channel.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The CSL channel.

◆ otLinkCslGetPeriod()

uint16_t otLinkCslGetPeriod ( otInstance * aInstance )

This function gets the CSL period.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The CSL period in units of 10 symbols.

◆ otLinkCslGetTimeout()

uint32_t otLinkCslGetTimeout ( otInstance * aInstance )

This function gets the CSL timeout.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The CSL timeout in seconds.

◆ otLinkCslSetChannel()

otError otLinkCslSetChannel ( otInstance * aInstance,
uint8_t aChannel
)

This function sets the CSL channel.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aChannel The CSL sample channel. Channel value should be 0 (Set CSL Channel unspecified) or within the range [1, 10] (if 915-MHz supported) and 11, 26 .
Return values
OT_ERROR_NONE Successfully set the CSL parameters.
OT_ERROR_INVALID_ARGS Invalid aChannel .

◆ otLinkCslSetPeriod()

otError otLinkCslSetPeriod ( otInstance * aInstance,
uint16_t aPeriod
)

This function sets the CSL period.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPeriod The CSL period in units of 10 symbols.
Return values
OT_ERROR_NONE Successfully set the CSL period.
OT_ERROR_INVALID_ARGS Invalid CSL period.

◆ otLinkCslSetTimeout()

otError otLinkCslSetTimeout ( otInstance * aInstance,
uint32_t aTimeout
)

This function sets the CSL timeout.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aTimeout The CSL timeout in seconds.
Return values
OT_ERROR_NONE Successfully set the CSL timeout.
OT_ERROR_INVALID_ARGS Invalid CSL timeout.

◆ otLinkEnergyScan()

otError otLinkEnergyScan ( otInstance * aInstance,
uint32_t aScanChannels,
uint16_t aScanDuration,
otHandleEnergyScanResult aCallback,
void * aCallbackContext
)

This function starts an IEEE 802.15.4 Energy Scan.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aScanChannels A bit vector indicating on which channels to perform energy scan.
[in] aScanDuration The time in milliseconds to spend scanning each channel.
[in] aCallback A pointer to a function called to pass on scan result on indicate scan completion.
[in] aCallbackContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Accepted the Energy Scan request.
OT_ERROR_BUSY Could not start the energy scan.

◆ otLinkFilterAddAddress()

otError otLinkFilterAddAddress ( otInstance * aInstance,
const otExtAddress * aExtAddress
)

This method adds an Extended Address to MAC filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A pointer to the Extended Address (MUST NOT be NULL).
Return values
OT_ERROR_NONE Successfully added aExtAddress to MAC filter.
OT_ERROR_NO_BUFS No available entry exists.

◆ otLinkFilterAddRssIn()

otError otLinkFilterAddRssIn ( otInstance * aInstance,
const otExtAddress * aExtAddress,
int8_t aRss
)

This method adds a fixed received signal strength (in dBm) entry for the messages from a given Extended Address in MAC Filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A pointer to the IEEE 802.15.4 Extended Address. MUST NOT be NULL.
[in] aRss A received signal strength (in dBm).
Return values
OT_ERROR_NONE Successfully added an entry for aExtAddress and aRss .
OT_ERROR_NO_BUFS No available entry exists.

◆ otLinkFilterClearAddresses()

void otLinkFilterClearAddresses ( otInstance * aInstance )

This method clears all the Extended Addresses from MAC filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otLinkFilterClearAllRssIn()

void otLinkFilterClearAllRssIn ( otInstance * aInstance )

This method clears all the received signal strength entries (including default RSS-in) on MAC Filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otLinkFilterClearDefaultRssIn()

void otLinkFilterClearDefaultRssIn ( otInstance * aInstance )

This method clears any previously set default received signal strength (in dBm) on MAC Filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otLinkFilterGetAddressMode()

otMacFilterAddressMode otLinkFilterGetAddressMode ( otInstance * aInstance )

This function gets the address mode of MAC filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
the address mode.

◆ otLinkFilterGetNextAddress()

otError otLinkFilterGetNextAddress ( otInstance * aInstance,
otMacFilterIterator * aIterator,
otMacFilterEntry * aEntry
)

This method gets an in-use address filter entry.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in,out] aIterator A pointer to the MAC filter iterator context. To get the first in-use address filter entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT. MUST NOT be NULL.
[out] aEntry A pointer to where the information is placed. MUST NOT be NULL.
Return values
OT_ERROR_NONE Successfully retrieved an in-use address filter entry.
OT_ERROR_NOT_FOUND No subsequent entry exists.

◆ otLinkFilterGetNextRssIn()

otError otLinkFilterGetNextRssIn ( otInstance * aInstance,
otMacFilterIterator * aIterator,
otMacFilterEntry * aEntry
)

This method gets an in-use RssIn filter entry.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in,out] aIterator A pointer to the MAC filter iterator context. MUST NOT be NULL. To get the first entry, it should be set to OT_MAC_FILTER_ITERATOR_INIT.
[out] aEntry A pointer to where the information is placed. The last entry would have the extended address as all 0xff to indicate the default received signal strength if it was set. aEntry MUST NOT be NULL.
Return values
OT_ERROR_NONE Successfully retrieved the next entry.
OT_ERROR_NOT_FOUND No subsequent entry exists.

◆ otLinkFilterRemoveAddress()

void otLinkFilterRemoveAddress ( otInstance * aInstance,
const otExtAddress * aExtAddress
)

This method removes an Extended Address from MAC filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

No action is performed if there is no existing entry in Filter matching the given Extended Address.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A pointer to the Extended Address (MUST NOT be NULL).

◆ otLinkFilterRemoveRssIn()

void otLinkFilterRemoveRssIn ( otInstance * aInstance,
const otExtAddress * aExtAddress
)

This method removes a MAC Filter entry for fixed received signal strength setting for a given Extended Address.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

No action is performed if there is no existing entry in Filter matching the given Extended Address.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A pointer to the IEEE 802.15.4 Extended Address. MUST NOT be NULL.

◆ otLinkFilterSetAddressMode()

void otLinkFilterSetAddressMode ( otInstance * aInstance,
otMacFilterAddressMode aMode
)

This function sets the address mode of MAC filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMode The address mode to set.

◆ otLinkFilterSetDefaultRssIn()

void otLinkFilterSetDefaultRssIn ( otInstance * aInstance,
int8_t aRss
)

This method sets the default received signal strength (in dBm) on MAC Filter.

This function is available when OPENTHREAD_CONFIG_MAC_FILTER_ENABLE configuration is enabled.

The default RSS value is used for all received frames from addresses for which there is no explicit RSS-IN entry in the Filter list (added using otLinkFilterAddRssIn() ).

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aRss The default received signal strength (in dBm) to set.

◆ otLinkGetCcaFailureRate()

uint16_t otLinkGetCcaFailureRate ( otInstance * aInstance )

This function returns the current CCA (Clear Channel Assessment) failure rate.

The rate is maintained over a window of (roughly) last OPENTHREAD_CONFIG_CCA_FAILURE_RATE_AVERAGING_WINDOW frame transmissions.

Returns
The CCA failure rate with maximum value 0xffff corresponding to 100% failure rate.

◆ otLinkGetChannel()

uint8_t otLinkGetChannel ( otInstance * aInstance )

Get the IEEE 802.15.4 channel.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The IEEE 802.15.4 channel.
See also
otLinkSetChannel

◆ otLinkGetCounters()

const otMacCounters * otLinkGetCounters ( otInstance * aInstance )

Get the MAC layer counters.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the MAC layer counters.

◆ otLinkGetExtendedAddress()

const otExtAddress * otLinkGetExtendedAddress ( otInstance * aInstance )

Get the IEEE 802.15.4 Extended Address.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the IEEE 802.15.4 Extended Address.

◆ otLinkGetFactoryAssignedIeeeEui64()

void otLinkGetFactoryAssignedIeeeEui64 ( otInstance * aInstance,
otExtAddress * aEui64
)

Get the factory-assigned IEEE EUI-64.

Parameters
[in] aInstance A pointer to the OpenThread instance.
[out] aEui64 A pointer to where the factory-assigned IEEE EUI-64 is placed.

◆ otLinkGetMaxFrameRetriesDirect()

uint8_t otLinkGetMaxFrameRetriesDirect ( otInstance * aInstance )

This method returns the maximum number of frame retries during direct transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The maximum number of retries during direct transmission.

◆ otLinkGetMaxFrameRetriesIndirect()

uint8_t otLinkGetMaxFrameRetriesIndirect ( otInstance * aInstance )

This method returns the maximum number of frame retries during indirect transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The maximum number of retries during indirect transmission.

◆ otLinkGetPanId()

otPanId otLinkGetPanId ( otInstance * aInstance )

Get the IEEE 802.15.4 PAN ID.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The IEEE 802.15.4 PAN ID.
See also
otLinkSetPanId

◆ otLinkGetPollPeriod()

uint32_t otLinkGetPollPeriod ( otInstance * aInstance )

Get the data poll period of sleepy end device.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The data poll period of sleepy end device in milliseconds.
See also
otLinkSetPollPeriod

◆ otLinkGetShortAddress()

otShortAddress otLinkGetShortAddress ( otInstance * aInstance )

Get the IEEE 802.15.4 Short Address.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the IEEE 802.15.4 Short Address.

◆ otLinkGetSupportedChannelMask()

uint32_t otLinkGetSupportedChannelMask ( otInstance * aInstance )

Get the supported channel mask of MAC layer.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The supported channel mask as uint32_t with bit 0 (lsb) mapping to channel 0, bit 1 to channel 1, so on.

◆ otLinkGetTxDirectRetrySuccessHistogram()

const uint32_t* otLinkGetTxDirectRetrySuccessHistogram ( otInstance * aInstance,
uint8_t * aNumberOfEntries
)

This method gets histogram of retries for a single direct packet until success.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aNumberOfEntries A pointer to where the size of returned histogram array is placed.
Returns
A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.

◆ otLinkGetTxIndirectRetrySuccessHistogram()

const uint32_t* otLinkGetTxIndirectRetrySuccessHistogram ( otInstance * aInstance,
uint8_t * aNumberOfEntries
)

This method gets histogram of retries for a single indirect packet until success.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aNumberOfEntries A pointer to where the size of returned histogram array is placed.
Returns
A pointer to the histogram of retries (in a form of an array). The n-th element indicates that the packet has been sent with n-th retry.

◆ otLinkIsActiveScanInProgress()

bool otLinkIsActiveScanInProgress ( otInstance * aInstance )

This function indicates whether or not an IEEE 802.15.4 Active Scan is currently in progress.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
true if an IEEE 802.15.4 Active Scan is in progress, false otherwise.

◆ otLinkIsEnabled()

bool otLinkIsEnabled ( otInstance * aInstance )

This function indicates whether or not the link layer is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
true Link layer is enabled.
false Link layer is not enabled.

◆ otLinkIsEnergyScanInProgress()

bool otLinkIsEnergyScanInProgress ( otInstance * aInstance )

This function indicates whether or not an IEEE 802.15.4 Energy Scan is currently in progress.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
true if an IEEE 802.15.4 Energy Scan is in progress, false otherwise.

◆ otLinkIsInTransmitState()

bool otLinkIsInTransmitState ( otInstance * aInstance )

This function indicates whether or not an IEEE 802.15.4 MAC is in the transmit state.

MAC module is in the transmit state during CSMA/CA procedure, CCA, Data, Beacon or Data Request frame transmission and receiving an ACK of a transmitted frame. MAC module is not in the transmit state during transmission of an ACK frame or a Beacon Request frame.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
true if an IEEE 802.15.4 MAC is in the transmit state, false otherwise.

◆ otLinkIsPromiscuous()

bool otLinkIsPromiscuous ( otInstance * aInstance )

This function indicates whether or not promiscuous mode is enabled at the link layer.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
true Promiscuous mode is enabled.
false Promiscuous mode is not enabled.

◆ otLinkResetCounters()

void otLinkResetCounters ( otInstance * aInstance )

Reset the MAC layer counters.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otLinkResetTxRetrySuccessHistogram()

void otLinkResetTxRetrySuccessHistogram ( otInstance * aInstance )

This method clears histogram statistics for direct and indirect transmissions.

This function is valid when OPENTHREAD_CONFIG_MAC_RETRY_SUCCESS_HISTOGRAM_ENABLE configuration is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otLinkSendDataRequest()

otError otLinkSendDataRequest ( otInstance * aInstance )

This function enqueues an IEEE 802.15.4 Data Request message for transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NONE Successfully enqueued an IEEE 802.15.4 Data Request message.
OT_ERROR_ALREADY An IEEE 802.15.4 Data Request message is already enqueued.
OT_ERROR_INVALID_STATE Device is not in rx-off-when-idle mode.
OT_ERROR_NO_BUFS Insufficient message buffers available.

◆ otLinkSendEmptyData()

otError otLinkSendEmptyData ( otInstance * aInstance )

This function instructs the device to send an empty IEEE 802.15.4 data frame.

This function is only supported on an Rx-Off-When-Idle device to send an empty data frame to its parent. Note: available only when OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NONE Successfully enqueued an empty message.
OT_ERROR_INVALID_STATE Device is not in Rx-Off-When-Idle mode.
OT_ERROR_NO_BUFS Insufficient message buffers available.

◆ otLinkSetChannel()

otError otLinkSetChannel ( otInstance * aInstance,
uint8_t aChannel
)

Set the IEEE 802.15.4 channel.

This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aChannel The IEEE 802.15.4 channel.
Return values
OT_ERROR_NONE Successfully set the channel.
OT_ERROR_INVALID_ARGS If aChannel is not in the range [11, 26] or is not in the supported channel mask.
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otLinkGetChannel

◆ otLinkSetEnabled()

otError otLinkSetEnabled ( otInstance * aInstance,
bool aEnable
)

This function enables or disables the link layer.

Note
The link layer may only be enabled / disabled when the Thread Interface is disabled.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aEnable true to enable the link layer, or false otherwise.
Return values
OT_ERROR_NONE Successfully enabled / disabled the link layer.
OT_ERROR_INVALID_STATE Could not disable the link layer because the Thread interface is enabled.

◆ otLinkSetExtendedAddress()

otError otLinkSetExtendedAddress ( otInstance * aInstance,
const otExtAddress * aExtAddress
)

This function sets the IEEE 802.15.4 Extended Address.

This function succeeds only when Thread protocols are disabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtAddress A pointer to the IEEE 802.15.4 Extended Address.
Return values
OT_ERROR_NONE Successfully set the IEEE 802.15.4 Extended Address.
OT_ERROR_INVALID_ARGS aExtAddress was NULL.
OT_ERROR_INVALID_STATE Thread protocols are enabled.

◆ otLinkSetMaxFrameRetriesDirect()

void otLinkSetMaxFrameRetriesDirect ( otInstance * aInstance,
uint8_t aMaxFrameRetriesDirect
)

This method sets the maximum number of frame retries during direct transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMaxFrameRetriesDirect The maximum number of retries during direct transmission.

◆ otLinkSetMaxFrameRetriesIndirect()

void otLinkSetMaxFrameRetriesIndirect ( otInstance * aInstance,
uint8_t aMaxFrameRetriesIndirect
)

This method sets the maximum number of frame retries during indirect transmission.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMaxFrameRetriesIndirect The maximum number of retries during indirect transmission.

◆ otLinkSetPanId()

otError otLinkSetPanId ( otInstance * aInstance,
otPanId aPanId
)

Set the IEEE 802.15.4 PAN ID.

This function succeeds only when Thread protocols are disabled. A successful call to this function also invalidates the Active and Pending Operational Datasets in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPanId The IEEE 802.15.4 PAN ID.
Return values
OT_ERROR_NONE Successfully set the PAN ID.
OT_ERROR_INVALID_ARGS If aPanId is not in the range [0, 65534].
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otLinkGetPanId

◆ otLinkSetPcapCallback()

void otLinkSetPcapCallback ( otInstance * aInstance,
otLinkPcapCallback aPcapCallback,
void * aCallbackContext
)

This function registers a callback to provide received raw IEEE 802.15.4 frames.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPcapCallback A pointer to a function that is called when receiving an IEEE 802.15.4 link frame or NULL to disable the callback.
[in] aCallbackContext A pointer to application-specific context.

◆ otLinkSetPollPeriod()

otError otLinkSetPollPeriod ( otInstance * aInstance,
uint32_t aPollPeriod
)

Set/clear user-specified/external data poll period for sleepy end device.

Note
This function updates only poll period of sleepy end device. To update child timeout the function otThreadSetChildTimeout() shall be called.
Minimal non-zero value should be OPENTHREAD_CONFIG_MAC_MINIMUM_POLL_PERIOD (10ms). Or zero to clear user-specified poll period.
User-specified value should be no more than the maximal value 0x3FFFFFF ((1 << 26) - 1) allowed, otherwise it would be clipped by the maximal value.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPollPeriod data poll period in milliseconds.
Return values
OT_ERROR_NONE Successfully set/cleared user-specified poll period.
OT_ERROR_INVALID_ARGS If aPollPeriod is invalid.
See also
otLinkGetPollPeriod

◆ otLinkSetPromiscuous()

otError otLinkSetPromiscuous ( otInstance * aInstance,
bool aPromiscuous
)

This function enables or disables the link layer promiscuous mode.

Note
Promiscuous mode may only be enabled when the Thread interface is disabled.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPromiscuous true to enable promiscuous mode, or false otherwise.
Return values
OT_ERROR_NONE Successfully enabled promiscuous mode.
OT_ERROR_INVALID_STATE Could not enable promiscuous mode because the Thread interface is enabled.

◆ otLinkSetSupportedChannelMask()

otError otLinkSetSupportedChannelMask ( otInstance * aInstance,
uint32_t aChannelMask
)

Set the supported channel mask of MAC layer.

This function succeeds only when Thread protocols are disabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aChannelMask The supported channel mask (bit 0 or lsb mapping to channel 0, and so on).
Return values
OT_ERROR_NONE Successfully set the supported channel mask.
OT_ERROR_INVALID_STATE Thread protocols are enabled.