Plat-crypto

This module includes the platform abstraction for Crypto.

Classes

struct otCryptoKey
This structure represents the Key Material required for Crypto operations.
struct otCryptoContext
This structure stores the context object for platform APIs.

Typedefs

typedef uint32_t otCryptoKeyRef
This datatype represents the key reference.
typedef struct otCryptoKey otCryptoKey
typedef struct otCryptoContext otCryptoContext

Enumerations

enum otCryptoKeyType {
OT_CRYPTO_KEY_TYPE_RAW ,
OT_CRYPTO_KEY_TYPE_AES ,
OT_CRYPTO_KEY_TYPE_HMAC
}
This enumeration defines the key types.
enum otCryptoKeyAlgorithm {
OT_CRYPTO_KEY_ALG_VENDOR ,
OT_CRYPTO_KEY_ALG_AES_ECB ,
OT_CRYPTO_KEY_ALG_HMAC_SHA_256
}
This enumeration defines the key algorithms.
enum {
OT_CRYPTO_KEY_USAGE_NONE = 0,
OT_CRYPTO_KEY_USAGE_EXPORT = 1 << 0,
OT_CRYPTO_KEY_USAGE_ENCRYPT = 1 << 1,
OT_CRYPTO_KEY_USAGE_DECRYPT = 1 << 2,
OT_CRYPTO_KEY_USAGE_SIGN_HASH = 1 << 3
}
This enumeration defines the key usage flags.
enum otCryptoKeyStorage {
OT_CRYPTO_KEY_STORAGE_VOLATILE ,
OT_CRYPTO_KEY_STORAGE_PERSISTENT
}
This enumeration defines the key storage types.

Functions

otError otPlatCryptoInit (void)
Initialize the Crypto module.
otError otPlatCryptoImportKey ( otCryptoKeyRef *aKeyRef, otCryptoKeyType aKeyType, otCryptoKeyAlgorithm aKeyAlgorithm, int aKeyUsage, otCryptoKeyStorage aKeyPersistence, const uint8_t *aKey, size_t aKeyLen)
Import a key into PSA ITS.
otError otPlatCryptoExportKey ( otCryptoKeyRef aKeyRef, uint8_t *aBuffer, size_t aBufferLen, size_t *aKeyLen)
Export a key stored in PSA ITS.
otError otPlatCryptoDestroyKey ( otCryptoKeyRef aKeyRef)
Destroy a key stored in PSA ITS.
bool otPlatCryptoHasKey ( otCryptoKeyRef aKeyRef)
Check if the key ref passed has an associated key in PSA ITS.
otError otPlatCryptoHmacSha256Init ( otCryptoContext *aContext)
Initialize the HMAC operation.
otError otPlatCryptoHmacSha256Deinit ( otCryptoContext *aContext)
Uninitialize the HMAC operation.
otError otPlatCryptoHmacSha256Start ( otCryptoContext *aContext, const otCryptoKey *aKey)
Start HMAC operation.
otError otPlatCryptoHmacSha256Update ( otCryptoContext *aContext, const void *aBuf, uint16_t aBufLength)
Update the HMAC operation with new input.
otError otPlatCryptoHmacSha256Finish ( otCryptoContext *aContext, uint8_t *aBuf, size_t aBufLength)
Complete the HMAC operation.
otError otPlatCryptoAesInit ( otCryptoContext *aContext)
Initialise the AES operation.
otError otPlatCryptoAesSetKey ( otCryptoContext *aContext, const otCryptoKey *aKey)
Set the key for AES operation.
otError otPlatCryptoAesEncrypt ( otCryptoContext *aContext, const uint8_t *aInput, uint8_t *aOutput)
Encrypt the given data.
otError otPlatCryptoAesFree ( otCryptoContext *aContext)
Free the AES context.
otError otPlatCryptoHkdfInit ( otCryptoContext *aContext)
Initialise the HKDF context.
otError otPlatCryptoHkdfExpand ( otCryptoContext *aContext, const uint8_t *aInfo, uint16_t aInfoLength, uint8_t *aOutputKey, uint16_t aOutputKeyLength)
Perform HKDF Expand step.
otError otPlatCryptoHkdfExtract ( otCryptoContext *aContext, const uint8_t *aSalt, uint16_t aSaltLength, const otCryptoKey *aInputKey)
Perform HKDF Extract step.
otError otPlatCryptoHkdfDeinit ( otCryptoContext *aContext)
Uninitialize the HKDF context.
otError otPlatCryptoSha256Init ( otCryptoContext *aContext)
Initialise the SHA-256 operation.
otError otPlatCryptoSha256Deinit ( otCryptoContext *aContext)
Uninitialize the SHA-256 operation.
otError otPlatCryptoSha256Start ( otCryptoContext *aContext)
Start SHA-256 operation.
otError otPlatCryptoSha256Update ( otCryptoContext *aContext, const void *aBuf, uint16_t aBufLength)
Update SHA-256 operation with new input.
otError otPlatCryptoSha256Finish ( otCryptoContext *aContext, uint8_t *aHash, uint16_t aHashSize)
Finish SHA-256 operation.

Detailed Description

This module includes the platform abstraction for Crypto.

Enumeration Type Documentation

◆ anonymous enum

anonymous enum

This enumeration defines the key usage flags.

Enumerator
OT_CRYPTO_KEY_USAGE_NONE

Key Usage: Key Usage is empty.

OT_CRYPTO_KEY_USAGE_EXPORT

Key Usage: Key can be exported.

OT_CRYPTO_KEY_USAGE_ENCRYPT

Key Usage: Encryption (vendor defined).

OT_CRYPTO_KEY_USAGE_DECRYPT

Key Usage: AES ECB.

OT_CRYPTO_KEY_USAGE_SIGN_HASH

Key Usage: HMAC SHA-256.

◆ otCryptoKeyAlgorithm

This enumeration defines the key algorithms.

Enumerator
OT_CRYPTO_KEY_ALG_VENDOR

Key Algorithm: Vendor Defined.

OT_CRYPTO_KEY_ALG_AES_ECB

Key Algorithm: AES ECB.

OT_CRYPTO_KEY_ALG_HMAC_SHA_256

Key Algorithm: HMAC SHA-256.

◆ otCryptoKeyStorage

This enumeration defines the key storage types.

Enumerator
OT_CRYPTO_KEY_STORAGE_VOLATILE

Key Persistence: Key is volatile.

OT_CRYPTO_KEY_STORAGE_PERSISTENT

Key Persistence: Key is persistent.

◆ otCryptoKeyType

This enumeration defines the key types.

Enumerator
OT_CRYPTO_KEY_TYPE_RAW

Key Type: Raw Data.

OT_CRYPTO_KEY_TYPE_AES

Key Type: AES.

OT_CRYPTO_KEY_TYPE_HMAC

Key Type: HMAC.

Function Documentation

◆ otPlatCryptoAesEncrypt()

otError otPlatCryptoAesEncrypt ( otCryptoContext * aContext,
const uint8_t * aInput,
uint8_t * aOutput
)

Encrypt the given data.

Parameters
[in] aContext Context for AES operation.
[in] aInput Pointer to the input buffer.
[in] aOutput Pointer to the output buffer.
Return values
OT_ERROR_NONE Successfully encrypted aInput .
OT_ERROR_FAILED Failed to encrypt aInput .
OT_ERROR_INVALID_ARGS aContext or aKey or aOutput were NULL

◆ otPlatCryptoAesFree()

otError otPlatCryptoAesFree ( otCryptoContext * aContext )

Free the AES context.

Parameters
[in] aContext Context for AES operation.
Return values
OT_ERROR_NONE Successfully freed AES context.
OT_ERROR_FAILED Failed to free AES context.
OT_ERROR_INVALID_ARGS aContext was NULL

◆ otPlatCryptoAesInit()

otError otPlatCryptoAesInit ( otCryptoContext * aContext )

Initialise the AES operation.

Parameters
[in] aContext Context for AES operation.
Return values
OT_ERROR_NONE Successfully Initialised AES operation.
OT_ERROR_FAILED Failed to Initialise AES operation.
OT_ERROR_INVALID_ARGS aContext was NULL
OT_ERROR_NO_BUFS Cannot allocate the context.
Note
The platform driver shall point the context to the correct object such as psa_key_id or mbedtls_aes_context_t.

◆ otPlatCryptoAesSetKey()

otError otPlatCryptoAesSetKey ( otCryptoContext * aContext,
const otCryptoKey * aKey
)

Set the key for AES operation.

Parameters
[in] aContext Context for AES operation.
[out] aKey Key to use for AES operation.
Return values
OT_ERROR_NONE Successfully set the key for AES operation.
OT_ERROR_FAILED Failed to set the key for AES operation.
OT_ERROR_INVALID_ARGS aContext or aKey was NULL

◆ otPlatCryptoDestroyKey()

otError otPlatCryptoDestroyKey ( otCryptoKeyRef aKeyRef )

Destroy a key stored in PSA ITS.

Parameters
[in] aKeyRef The key ref to be destroyed
Return values
OT_ERROR_NONE Successfully destroyed the key.
OT_ERROR_FAILED Failed to destroy the key.
Note
This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.

◆ otPlatCryptoExportKey()

otError otPlatCryptoExportKey ( otCryptoKeyRef aKeyRef,
uint8_t * aBuffer,
size_t aBufferLen,
size_t * aKeyLen
)

Export a key stored in PSA ITS.

Parameters
[in] aKeyRef The key ref to be used for crypto operations.
[out] aBuffer Pointer to the buffer where key needs to be exported.
[in] aBufferLen Length of the buffer passed to store the exported key.
[out] aKeyLen Pointer to return the length of the exported key.
Return values
OT_ERROR_NONE Successfully exported aKeyRef .
OT_ERROR_FAILED Failed to export aKeyRef .
OT_ERROR_INVALID_ARGS aBuffer was NULL
Note
This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.

◆ otPlatCryptoHasKey()

bool otPlatCryptoHasKey ( otCryptoKeyRef aKeyRef )

Check if the key ref passed has an associated key in PSA ITS.

Parameters
[in] aKeyRef The Key Ref to check.
Return values
TRUE There is an associated key with aKeyRef .
FALSE There is no associated key with aKeyRef .
Note
This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.

◆ otPlatCryptoHkdfDeinit()

otError otPlatCryptoHkdfDeinit ( otCryptoContext * aContext )

Uninitialize the HKDF context.

Parameters
[in] aContext Context for HKDF operation.
Return values
OT_ERROR_NONE Successfully un-initialised HKDF operation.
OT_ERROR_FAILED Failed to un-initialised HKDF operation.
OT_ERROR_INVALID_ARGS aContext was NULL

◆ otPlatCryptoHkdfExpand()

otError otPlatCryptoHkdfExpand ( otCryptoContext * aContext,
const uint8_t * aInfo,
uint16_t aInfoLength,
uint8_t * aOutputKey,
uint16_t aOutputKeyLength
)

Perform HKDF Expand step.

Parameters
[in] aContext Operation context for HKDF operation.
[in] aInfo Pointer to the Info sequence.
[in] aInfoLength Length of the Info sequence.
[out] aOutputKey Pointer to the output Key.
[in] aOutputKeyLength Size of the output key buffer.
Return values
OT_ERROR_NONE HKDF Expand was successful.
OT_ERROR_FAILED HKDF Expand failed.
OT_ERROR_INVALID_ARGS aContext was NULL

◆ otPlatCryptoHkdfExtract()

otError otPlatCryptoHkdfExtract ( otCryptoContext * aContext,
const uint8_t * aSalt,
uint16_t aSaltLength,
const otCryptoKey * aInputKey
)

Perform HKDF Extract step.

Parameters
[in] aContext Operation context for HKDF operation.
[in] aSalt Pointer to the Salt for HKDF.
[in] aInfoLength length of Salt.
[in] aInputKey Pointer to the input key.
Return values
OT_ERROR_NONE HKDF Extract was successful.
OT_ERROR_FAILED HKDF Extract failed.

◆ otPlatCryptoHkdfInit()

otError otPlatCryptoHkdfInit ( otCryptoContext * aContext )

Initialise the HKDF context.

Parameters
[in] aContext Context for HKDF operation.
Return values
OT_ERROR_NONE Successfully Initialised AES operation.
OT_ERROR_FAILED Failed to Initialise AES operation.
OT_ERROR_INVALID_ARGS aContext was NULL
Note
The platform driver shall point the context to the correct object such as psa_key_derivation_operation_t or HmacSha256::Hash

◆ otPlatCryptoHmacSha256Deinit()

otError otPlatCryptoHmacSha256Deinit ( otCryptoContext * aContext )

Uninitialize the HMAC operation.

Parameters
[in] aContext Context for HMAC operation.
Return values
OT_ERROR_NONE Successfully uninitialized HMAC operation.
OT_ERROR_FAILED Failed to uninitialized HMAC operation.
OT_ERROR_INVALID_ARGS aContext was NULL

◆ otPlatCryptoHmacSha256Finish()

otError otPlatCryptoHmacSha256Finish ( otCryptoContext * aContext,
uint8_t * aBuf,
size_t aBufLength
)

Complete the HMAC operation.

Parameters
[in] aContext Context for HMAC operation.
[out] aBuf A pointer to the output buffer.
[in] aBufLength The length of aBuf in bytes.
Return values
OT_ERROR_NONE Successfully completed HMAC operation.
OT_ERROR_FAILED Failed to complete HMAC operation.
OT_ERROR_INVALID_ARGS aContext or aBuf was NULL

◆ otPlatCryptoHmacSha256Init()

otError otPlatCryptoHmacSha256Init ( otCryptoContext * aContext )

Initialize the HMAC operation.

Parameters
[in] aContext Context for HMAC operation.
Return values
OT_ERROR_NONE Successfully initialized HMAC operation.
OT_ERROR_FAILED Failed to initialize HMAC operation.
OT_ERROR_INVALID_ARGS aContext was NULL
Note
The platform driver shall point the context to the correct object such as psa_mac_operation_t or mbedtls_md_context_t.

◆ otPlatCryptoHmacSha256Start()

otError otPlatCryptoHmacSha256Start ( otCryptoContext * aContext,
const otCryptoKey * aKey
)

Start HMAC operation.

Parameters
[in] aContext Context for HMAC operation.
[in] aKey Key material to be used for for HMAC operation.
Return values
OT_ERROR_NONE Successfully started HMAC operation.
OT_ERROR_FAILED Failed to start HMAC operation.
OT_ERROR_INVALID_ARGS aContext or aKey was NULL

◆ otPlatCryptoHmacSha256Update()

otError otPlatCryptoHmacSha256Update ( otCryptoContext * aContext,
const void * aBuf,
uint16_t aBufLength
)

Update the HMAC operation with new input.

Parameters
[in] aContext Context for HMAC operation.
[in] aBuf A pointer to the input buffer.
[in] aBufLength The length of aBuf in bytes.
Return values
OT_ERROR_NONE Successfully updated HMAC with new input operation.
OT_ERROR_FAILED Failed to update HMAC operation.
OT_ERROR_INVALID_ARGS aContext or aBuf was NULL

◆ otPlatCryptoImportKey()

otError otPlatCryptoImportKey ( otCryptoKeyRef * aKeyRef,
otCryptoKeyType aKeyType,
otCryptoKeyAlgorithm aKeyAlgorithm,
int aKeyUsage,
otCryptoKeyStorage aKeyPersistence,
const uint8_t * aKey,
size_t aKeyLen
)

Import a key into PSA ITS.

Parameters
[in,out] aKeyRef Pointer to the key ref to be used for crypto operations.
[in] aKeyType Key Type encoding for the key.
[in] aKeyAlgorithm Key algorithm encoding for the key.
[in] aKeyUsage Key Usage encoding for the key (combinations of OT_CRYPTO_KEY_USAGE_* ).
[in] aKeyPersistence Key Persistence for this key
[in] aKey Actual key to be imported.
[in] aKeyLen Length of the key to be imported.
Return values
OT_ERROR_NONE Successfully imported the key.
OT_ERROR_FAILED Failed to import the key.
OT_ERROR_INVALID_ARGS aKey was set to NULL.
Note
If OT_CRYPTO_KEY_STORAGE_PERSISTENT is passed for aKeyPersistence then aKeyRef is input and platform should use the given aKeyRef and MUST not change it.

If OT_CRYPTO_KEY_STORAGE_VOLATILE is passed for aKeyPersistence then aKeyRef is output, the initial value does not matter and platform API MUST update it to return the new key ref.

This API is only used by OT core when OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE is enabled.

◆ otPlatCryptoInit()

otError otPlatCryptoInit ( void )

Initialize the Crypto module.

Return values
OT_ERROR_NONE Successfully initialized Crypto module.
OT_ERROR_FAILED Failed to initialize Crypto module.

◆ otPlatCryptoSha256Deinit()

otError otPlatCryptoSha256Deinit ( otCryptoContext * aContext )

Uninitialize the SHA-256 operation.

Parameters
[in] aContext Context for SHA-256 operation.
Return values
OT_ERROR_NONE Successfully un-initialised SHA-256 operation.
OT_ERROR_FAILED Failed to un-initialised SHA-256 operation.
OT_ERROR_INVALID_ARGS aContext was NULL

◆ otPlatCryptoSha256Finish()

otError otPlatCryptoSha256Finish ( otCryptoContext * aContext,
uint8_t * aHash,
uint16_t aHashSize
)

Finish SHA-256 operation.

Parameters
[in] aContext Context for SHA-256 operation.
[in] aContextSize Context size SHA-256 operation.
[in] aHash A pointer to the output buffer, where hash needs to be stored.
[in] aHashSize The length of aHash in bytes.
Return values
OT_ERROR_NONE Successfully completed the SHA-256 operation.
OT_ERROR_FAILED Failed to complete SHA-256 operation.
OT_ERROR_INVALID_ARGS aContext or aHash was NULL

◆ otPlatCryptoSha256Init()

otError otPlatCryptoSha256Init ( otCryptoContext * aContext )

Initialise the SHA-256 operation.

Parameters
[in] aContext Context for SHA-256 operation.
Return values
OT_ERROR_NONE Successfully initialised SHA-256 operation.
OT_ERROR_FAILED Failed to initialise SHA-256 operation.
OT_ERROR_INVALID_ARGS aContext was NULL
Note
The platform driver shall point the context to the correct object such as psa_hash_operation_t or mbedtls_sha256_context.

◆ otPlatCryptoSha256Start()

otError otPlatCryptoSha256Start ( otCryptoContext * aContext )

Start SHA-256 operation.

Parameters
[in] aContext Context for SHA-256 operation.
Return values
OT_ERROR_NONE Successfully started SHA-256 operation.
OT_ERROR_FAILED Failed to start SHA-256 operation.
OT_ERROR_INVALID_ARGS aContext was NULL

◆ otPlatCryptoSha256Update()

otError otPlatCryptoSha256Update ( otCryptoContext * aContext,
const void * aBuf,
uint16_t aBufLength
)

Update SHA-256 operation with new input.

Parameters
[in] aContext Context for SHA-256 operation.
[in] aBuf A pointer to the input buffer.
[in] aBufLength The length of aBuf in bytes.
Return values
OT_ERROR_NONE Successfully updated SHA-256 with new input operation.
OT_ERROR_FAILED Failed to update SHA-256 operation.
OT_ERROR_INVALID_ARGS aContext or aBuf was NULL