Factory Diagnostics

This module includes functions that control the Thread stack's execution.

Functions

otError otDiagProcessCmd ( otInstance *aInstance, uint8_t aArgsLength, char *aArgs[], char *aOutput, size_t aOutputMaxLen)
This function processes a factory diagnostics command line.
void otDiagProcessCmdLine ( otInstance *aInstance, const char *aString, char *aOutput, size_t aOutputMaxLen)
This function processes a factory diagnostics command line.
bool otDiagIsEnabled ( otInstance *aInstance)
This function indicates whether or not the factory diagnostics mode is enabled.

Detailed Description

This module includes functions that control the Thread stack's execution.

Function Documentation

◆ otDiagIsEnabled()

bool otDiagIsEnabled ( otInstance * aInstance )

This function indicates whether or not the factory diagnostics mode is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
TRUE if factory diagnostics mode is enabled
FALSE if factory diagnostics mode is disabled.

◆ otDiagProcessCmd()

otError otDiagProcessCmd ( otInstance * aInstance,
uint8_t aArgsLength,
char * aArgs[],
char * aOutput,
size_t aOutputMaxLen
)

This function processes a factory diagnostics command line.

The output of this function (the content written to aOutput ) MUST terminate with \0 and the \0 is within the output buffer.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aArgsLength The number of elements in aArgs .
[in] aArgs An array of arguments.
[out] aOutput The diagnostics execution result.
[in] aOutputMaxLen The output buffer size.
Return values
OT_ERROR_INVALID_ARGS The command is supported but invalid arguments provided.
OT_ERROR_NONE The command is successfully process.
OT_ERROR_NOT_IMPLEMENTED The command is not supported.

◆ otDiagProcessCmdLine()

void otDiagProcessCmdLine ( otInstance * aInstance,
const char * aString,
char * aOutput,
size_t aOutputMaxLen
)

This function processes a factory diagnostics command line.

The output of this function (the content written to aOutput ) MUST terminate with \0 and the \0 is within the output buffer.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aString A NULL-terminated input string.
[out] aOutput The diagnostics execution result.
[in] aOutputMaxLen The output buffer size.