otNetifMulticastAddress Struct Reference

This structure represents an IPv6 network interface multicast address.

#include < include/openthread/ip6.h >

Public Attributes

otIp6Address mAddress
The IPv6 multicast address.
const struct otNetifMulticastAddress * mNext
A pointer to the next network interface multicast address.

This structure represents an IPv6 network interface multicast address.


The documentation for this struct was generated from the following file:
  • include/openthread/ ip6.h