otNetworkDiagRoute Struct Reference

This structure represents a Network Diagnostic Route TLV value.

#include <include/openthread/netdiag.h>

Public Attributes

uint8_t mIdSequence
 The sequence number associated with the set of Router ID assignments in mRouteData.
 
uint8_t mRouteCount
 Number of elements in mRouteData.
 
otNetworkDiagRouteData mRouteData [OT_NETWORK_MAX_ROUTER_ID+1]
 Link Quality and Routing Cost data.

This structure represents a Network Diagnostic Route TLV value.


The documentation for this struct was generated from the following file:
  • include/openthread/netdiag.h