otSrpServerLeaseConfig Struct Reference

This structure includes SRP server LEASE and KEY-LEASE configurations.

#include < include/openthread/srp_server.h >

Public Attributes

uint32_t mMinLease
The minimum LEASE interval in seconds.
uint32_t mMaxLease
The maximum LEASE interval in seconds.
uint32_t mMinKeyLease
The minimum KEY-LEASE interval in seconds.
uint32_t mMaxKeyLease
The maximum KEY-LEASE interval in seconds.

This structure includes SRP server LEASE and KEY-LEASE configurations.


The documentation for this struct was generated from the following file:
  • include/openthread/ srp_server.h