otOperationalDatasetComponents Struct Reference

This structure represents presence of different components in Active or Pending Operational Dataset.

#include <include/openthread/dataset.h>

Public Attributes

bool mIsActiveTimestampPresent: 1
 TRUE if Active Timestamp is present, FALSE otherwise.
 
bool mIsPendingTimestampPresent: 1
 TRUE if Pending Timestamp is present, FALSE otherwise.
 
bool mIsNetworkKeyPresent: 1
 TRUE if Network Key is present, FALSE otherwise.
 
bool mIsNetworkNamePresent: 1
 TRUE if Network Name is present, FALSE otherwise.
 
bool mIsExtendedPanIdPresent: 1
 TRUE if Extended PAN ID is present, FALSE otherwise.
 
bool mIsMeshLocalPrefixPresent: 1
 TRUE if Mesh Local Prefix is present, FALSE otherwise.
 
bool mIsDelayPresent: 1
 TRUE if Delay Timer is present, FALSE otherwise.
 
bool mIsPanIdPresent: 1
 TRUE if PAN ID is present, FALSE otherwise.
 
bool mIsChannelPresent: 1
 TRUE if Channel is present, FALSE otherwise.
 
bool mIsPskcPresent: 1
 TRUE if PSKc is present, FALSE otherwise.
 
bool mIsSecurityPolicyPresent: 1
 TRUE if Security Policy is present, FALSE otherwise.
 
bool mIsChannelMaskPresent: 1
 TRUE if Channel Mask is present, FALSE otherwise.

This structure represents presence of different components in Active or Pending Operational Dataset.


The documentation for this struct was generated from the following file:
  • include/openthread/dataset.h