otHistoryTrackerUnicastAddressInfo Struct Reference
This structure represent a unicast IPv6 address info.
#include <
include/openthread/history_tracker.h
>
Public Attributes | |
otIp6Address | mAddress |
The unicast IPv6 address. | |
uint8_t | mPrefixLength |
The Prefix length (in bits). | |
uint8_t | mAddressOrigin |
The address origin (OT_ADDRESS_ORIGIN_* constants). | |
otHistoryTrackerAddressEvent | mEvent |
Indicates the event (address is added/removed). | |
uint8_t | mScope: 4 |
The IPv6 scope. | |
bool | mPreferred: 1 |
If the address is preferred. | |
bool | mValid: 1 |
If the address is valid. | |
bool | mRloc: 1 |
If the address is an RLOC. |
This structure represent a unicast IPv6 address info.
The documentation for this struct was generated from the following file:
- include/openthread/
history_tracker.h