otDnssdServiceInstanceInfo Struct Reference
This structure represents information of a discovered service instance for a DNS-SD query.
#include <
include/openthread/dnssd_server.h
>
Public Attributes | |
const char * | mFullName |
Full instance name (e.g. "OpenThread._ipps._tcp.default.service.arpa."). | |
const char * | mHostName |
Host name (e.g. "ot-host.default.service.arpa."). | |
uint8_t | mAddressNum |
Number of host IPv6 addresses. | |
const otIp6Address * | mAddresses |
Host IPv6 addresses. | |
uint16_t | mPort |
Service port. | |
uint16_t | mPriority |
Service priority. | |
uint16_t | mWeight |
Service weight. | |
uint16_t | mTxtLength |
Service TXT RDATA length. | |
const uint8_t * | mTxtData |
Service TXT RDATA. | |
uint32_t | mTtl |
Service TTL (in seconds). |
This structure represents information of a discovered service instance for a DNS-SD query.
The documentation for this struct was generated from the following file:
- include/openthread/
dnssd_server.h