This module includes functions for the Thread Joiner role.
Classes |
|
| struct | otJoinerDiscerner |
|
This structure represents a Joiner Discerner.
|
|
Macros |
|
| #define | OT_JOINER_MAX_DISCERNER_LENGTH 64 |
|
Maximum length of a Joiner Discerner in bits.
|
|
Typedefs |
|
| typedef enum otJoinerState | otJoinerState |
|
This enumeration defines the Joiner State.
|
|
| typedef struct otJoinerDiscerner | otJoinerDiscerner |
|
This structure represents a Joiner Discerner.
|
|
| typedef void(* | otJoinerCallback ) ( otError aError, void *aContext) |
|
This function pointer is called to notify the completion of a join operation.
|
|
Enumerations |
|
| enum |
otJoinerState
{
OT_JOINER_STATE_IDLE = 0, OT_JOINER_STATE_DISCOVER = 1, OT_JOINER_STATE_CONNECT = 2, OT_JOINER_STATE_CONNECTED = 3, OT_JOINER_STATE_ENTRUST = 4, OT_JOINER_STATE_JOINED = 5 } |
|
This enumeration defines the Joiner State.
|
|
Functions |
|
| otError | otJoinerStart ( otInstance *aInstance, const char *aPskd, const char *aProvisioningUrl, const char *aVendorName, const char *aVendorModel, const char *aVendorSwVersion, const char *aVendorData, otJoinerCallback aCallback, void *aContext) |
|
This function enables the Thread Joiner role.
|
|
| void | otJoinerStop ( otInstance *aInstance) |
|
This function disables the Thread Joiner role.
|
|
| otJoinerState | otJoinerGetState ( otInstance *aInstance) |
|
This function returns the Joiner State.
|
|
| const otExtAddress * | otJoinerGetId ( otInstance *aInstance) |
|
This method gets the Joiner ID.
|
|
| otError | otJoinerSetDiscerner ( otInstance *aInstance, otJoinerDiscerner *aDiscerner) |
|
This method sets the Joiner Discerner.
|
|
| const otJoinerDiscerner * | otJoinerGetDiscerner ( otInstance *aInstance) |
|
This method gets the Joiner Discerner.
|
|
Detailed Description
This module includes functions for the Thread Joiner role.
- Note
-
The functions in this module require
OPENTHREAD_CONFIG_JOINER_ENABLE=1.
Typedef Documentation
◆ otJoinerCallback
| typedef void(* otJoinerCallback) ( otError aError, void *aContext) |
This function pointer is called to notify the completion of a join operation.
- Parameters
-
[in] aErrorOT_ERROR_NONE if the join process succeeded. OT_ERROR_SECURITY if the join process failed due to security credentials. OT_ERROR_NOT_FOUND if no joinable network was discovered. OT_ERROR_RESPONSE_TIMEOUT if a response timed out. [in] aContextA pointer to application-specific context.
Function Documentation
◆ otJoinerGetDiscerner()
| const otJoinerDiscerner * otJoinerGetDiscerner | ( | otInstance * |
aInstance
|
) |
This method gets the Joiner Discerner.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- A pointer to Joiner Discerner or NULL if none is set.
◆ otJoinerGetId()
| const otExtAddress * otJoinerGetId | ( | otInstance * |
aInstance
|
) |
This method gets the Joiner ID.
If a Joiner Discerner is not set, Joiner ID is the first 64 bits of the result of computing SHA-256 over factory-assigned IEEE EUI-64. Otherwise the Joiner ID is calculated from the Joiner Discerner value.
The Joiner ID is also used as the device's IEEE 802.15.4 Extended Address during commissioning process.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- A pointer to the Joiner ID.
◆ otJoinerGetState()
| otJoinerState otJoinerGetState | ( | otInstance * |
aInstance
|
) |
This function returns the Joiner State.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Return values
-
OT_JOINER_STATE_IDLEOT_JOINER_STATE_DISCOVEROT_JOINER_STATE_CONNECTOT_JOINER_STATE_CONNECTEDOT_JOINER_STATE_ENTRUSTOT_JOINER_STATE_JOINED
◆ otJoinerSetDiscerner()
| otError otJoinerSetDiscerner | ( | otInstance * |
aInstance,
|
| otJoinerDiscerner * |
aDiscerner
|
||
| ) |
This method sets the Joiner Discerner.
The Joiner Discerner is used to calculate the Joiner ID used during commissioning/joining process.
By default (when a discerner is not provided or set to NULL), Joiner ID is derived as first 64 bits of the result of computing SHA-256 over factory-assigned IEEE EUI-64. Note that this is the main behavior expected by Thread specification.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aDiscernerA pointer to a Joiner Discerner. If NULL clears any previously set discerner.
- Return values
-
OT_ERROR_NONEThe Joiner Discerner updated successfully. OT_ERROR_INVALID_ARGSaDiscerneris not valid (specified length is not within valid range).OT_ERROR_INVALID_STATEThere is an ongoing Joining process so Joiner Discerner could not be changed.
◆ otJoinerStart()
| otError otJoinerStart | ( | otInstance * |
aInstance,
|
| const char * |
aPskd,
|
||
| const char * |
aProvisioningUrl,
|
||
| const char * |
aVendorName,
|
||
| const char * |
aVendorModel,
|
||
| const char * |
aVendorSwVersion,
|
||
| const char * |
aVendorData,
|
||
| otJoinerCallback |
aCallback,
|
||
| void * |
aContext
|
||
| ) |
This function enables the Thread Joiner role.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aPskdA pointer to the PSKd. [in] aProvisioningUrlA pointer to the Provisioning URL (may be NULL). [in] aVendorNameA pointer to the Vendor Name (may be NULL). [in] aVendorModelA pointer to the Vendor Model (may be NULL). [in] aVendorSwVersionA pointer to the Vendor SW Version (may be NULL). [in] aVendorDataA pointer to the Vendor Data (may be NULL). [in] aCallbackA pointer to a function that is called when the join operation completes. [in] aContextA pointer to application-specific context.
- Return values
-
OT_ERROR_NONESuccessfully started the Joiner role. OT_ERROR_BUSYThe previous attempt is still on-going. OT_ERROR_INVALID_ARGSaPskdoraProvisioningUrlis invalid.OT_ERROR_INVALID_STATEThe IPv6 stack is not enabled or Thread stack is fully enabled.
◆ otJoinerStop()
| void otJoinerStop | ( | otInstance * |
aInstance
|
) |
This function disables the Thread Joiner role.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.