Factory Diagnostics

This module includes the platform abstraction for diagnostics features.

Functions

otError otPlatDiagProcess ( otInstance *aInstance, uint8_t aArgsLength, char *aArgs[], char *aOutput, size_t aOutputMaxLen)
This function processes a factory diagnostics command line.
void otPlatDiagModeSet (bool aMode)
This function enables/disables the factory diagnostics mode.
bool otPlatDiagModeGet (void)
This function indicates whether or not factory diagnostics mode is enabled.
void otPlatDiagChannelSet (uint8_t aChannel)
This function sets the channel to use for factory diagnostics.
void otPlatDiagTxPowerSet (int8_t aTxPower)
This function sets the transmit power to use for factory diagnostics.
void otPlatDiagRadioReceived ( otInstance *aInstance, otRadioFrame *aFrame, otError aError)
This function processes the received radio frame.
void otPlatDiagAlarmCallback ( otInstance *aInstance)
This function processes the alarm event.

Detailed Description

This module includes the platform abstraction for diagnostics features.

Function Documentation

◆ otPlatDiagAlarmCallback()

void otPlatDiagAlarmCallback ( otInstance * aInstance )

This function processes the alarm event.

Parameters
[in] aInstance The OpenThread instance for current request.

◆ otPlatDiagChannelSet()

void otPlatDiagChannelSet ( uint8_t aChannel )

This function sets the channel to use for factory diagnostics.

Parameters
[in] aChannel The channel value.

◆ otPlatDiagModeGet()

bool otPlatDiagModeGet ( void )

This function indicates whether or not factory diagnostics mode is enabled.

Returns
TRUE if factory diagnostics mode is enabled, FALSE otherwise.

◆ otPlatDiagModeSet()

void otPlatDiagModeSet ( bool aMode )

This function enables/disables the factory diagnostics mode.

Parameters
[in] aMode TRUE to enable diagnostics mode, FALSE otherwise.

◆ otPlatDiagProcess()

otError otPlatDiagProcess ( otInstance * aInstance,
uint8_t aArgsLength,
char * aArgs[],
char * aOutput,
size_t aOutputMaxLen
)

This function processes a factory diagnostics command line.

The output of this function (the content written to aOutput ) MUST terminate with \0 and the \0 is within the output buffer.

Parameters
[in] aInstance The OpenThread instance for current request.
[in] aArgsLength The number of arguments in aArgs .
[in] aArgs The arguments of diagnostics command line.
[out] aOutput The diagnostics execution result.
[in] aOutputMaxLen The output buffer size.
Return values
OT_ERROR_INVALID_ARGS The command is supported but invalid arguments provided.
OT_ERROR_NONE The command is successfully process.
OT_ERROR_INVALID_COMMAND The command is not valid or not supported.

◆ otPlatDiagRadioReceived()

void otPlatDiagRadioReceived ( otInstance * aInstance,
otRadioFrame * aFrame,
otError aError
)

This function processes the received radio frame.

Parameters
[in] aInstance The OpenThread instance for current request.
[in] aFrame The received radio frame.
[in] aError The received radio frame status.

◆ otPlatDiagTxPowerSet()

void otPlatDiagTxPowerSet ( int8_t aTxPower )

This function sets the transmit power to use for factory diagnostics.

Parameters
[in] aTxPower The transmit power value.