otServerConfig Struct Reference

This structure represents a Server configuration.

#include <include/openthread/netdata.h>

Public Attributes

bool mStable: 1
 Whether this config is considered Stable Network Data.
 
uint8_t mServerDataLength
 Length of server data.
 
uint8_t mServerData [OT_SERVER_DATA_MAX_SIZE]
 Server data bytes.
 
uint16_t mRloc16
 The Server RLOC16.

This structure represents a Server configuration.


The documentation for this struct was generated from the following file:
  • include/openthread/netdata.h