This structure represents an MLE Link Mode configuration.
#include <
include/openthread/thread.h
>
Public Attributes | |
bool | mRxOnWhenIdle: 1 |
1, if the sender has its receiver on when not transmitting. 0, otherwise. | |
bool | mDeviceType: 1 |
1, if the sender is an FTD. 0, otherwise. | |
bool | mNetworkData: 1 |
1, if the sender requires the full Network Data. 0, otherwise. |
This structure represents an MLE Link Mode configuration.
The documentation for this struct was generated from the following file:
- include/openthread/
thread.h