General

This module includes functions for all Thread roles.

Classes

struct otBorderRouterConfig
This structure represents a Border Router configuration.
struct otExternalRouteConfig
This structure represents an External Route configuration.
struct otServerConfig
This structure represents a Server configuration.
struct otServiceConfig
This structure represents a Service configuration.
struct otNetworkDiagConnectivity
This structure represents a Network Diagnostic Connectivity value.
struct otNetworkDiagRouteData
This structure represents a Network Diagnostic Route data.
struct otNetworkDiagRoute
This structure represents a Network Diagnostic Route TLV value.
struct otNetworkDiagMacCounters
This structure represents a Network Diagnostic Mac Counters value.
struct otNetworkDiagChildEntry
This structure represents a Network Diagnostic Child Table Entry.
struct otNetworkDiagTlv
This structure represents a Network Diagnostic TLV.
struct otLinkModeConfig
This structure represents an MLE Link Mode configuration.
struct otNeighborInfo
This structure holds diagnostic information for a neighboring Thread node.
struct otLeaderData
This structure represents the Thread Leader Data.
struct otRouterInfo
This structure holds diagnostic information for a Thread Router.
struct otIpCounters
This structure represents the IP level counters.
struct otMleCounters
This structure represents the Thread MLE counters.
struct otThreadParentResponseInfo
This structure represents the MLE Parent Response data.
struct otThreadDiscoveryRequestInfo
This structure represents the Thread Discovery Request data.

Macros

#define OT_NETWORK_DATA_ITERATOR_INIT 0
Value to initialize otNetworkDataIterator .
#define OT_SERVICE_DATA_MAX_SIZE 252
Max size of Service Data in bytes.
#define OT_SERVER_DATA_MAX_SIZE 248
Max size of Server Data in bytes. Theoretical limit, practically much lower.
#define OT_NETWORK_DIAGNOSTIC_TYPELIST_MAX_ENTRIES 19
Maximum Number of Network Diagnostic TLV Types to Request or Reset.
#define OT_NETWORK_DIAGNOSTIC_CHILD_TABLE_ENTRY_SIZE 3
Size of Network Diagnostic Child Table entry.
#define OT_NETWORK_DIAGNOSTIC_ITERATOR_INIT 0
Initializer for otNetworkDiagIterator.
#define OT_NETWORK_BASE_TLV_MAX_LENGTH 254
Maximum value length of Thread Base TLV.
#define OT_NETWORK_MAX_ROUTER_ID 62
Maximum Router ID.
#define OT_NEIGHBOR_INFO_ITERATOR_INIT 0
Initializer for otNeighborInfoIterator.
#define OT_JOINER_ADVDATA_MAX_LENGTH 64
Maximum AdvData Length of Joiner Advertisement.

Typedefs

typedef uint32_t otNetworkDataIterator
Used to iterate through Network Data information.
typedef struct otBorderRouterConfig otBorderRouterConfig
This structure represents a Border Router configuration.
typedef struct otExternalRouteConfig otExternalRouteConfig
This structure represents an External Route configuration.
typedef enum otRoutePreference otRoutePreference
Defines valid values for mPreference in otExternalRouteConfig and otBorderRouterConfig .
typedef struct otServerConfig otServerConfig
This structure represents a Server configuration.
typedef struct otServiceConfig otServiceConfig
This structure represents a Service configuration.
typedef enum otNetDataPublisherEvent otNetDataPublisherEvent
This enumeration represents the events reported from the Publisher callbacks.
typedef void(* otNetDataDnsSrpServicePublisherCallback ) ( otNetDataPublisherEvent aEvent, void *aContext)
This function pointer type defines the callback used to notify when a "DNS/SRP Service" entry is added to or removed from the Thread Network Data.
typedef void(* otNetDataPrefixPublisherCallback ) ( otNetDataPublisherEvent aEvent, const otIp6Prefix *aPrefix, void *aContext)
This function pointer type defines the callback used to notify when a prefix (on-mesh or external route) entry is added to or removed from the Thread Network Data.
typedef uint16_t otNetworkDiagIterator
Used to iterate through Network Diagnostic TLV.
typedef struct otNetworkDiagConnectivity otNetworkDiagConnectivity
This structure represents a Network Diagnostic Connectivity value.
typedef struct otNetworkDiagRouteData otNetworkDiagRouteData
This structure represents a Network Diagnostic Route data.
typedef struct otNetworkDiagRoute otNetworkDiagRoute
This structure represents a Network Diagnostic Route TLV value.
typedef struct otNetworkDiagMacCounters otNetworkDiagMacCounters
This structure represents a Network Diagnostic Mac Counters value.
typedef struct otNetworkDiagChildEntry otNetworkDiagChildEntry
This structure represents a Network Diagnostic Child Table Entry.
typedef struct otNetworkDiagTlv otNetworkDiagTlv
This structure represents a Network Diagnostic TLV.
typedef void(* otReceiveDiagnosticGetCallback ) ( otError aError, otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext)
This function pointer is called when Network Diagnostic Get response is received.
typedef struct otLinkModeConfig otLinkModeConfig
This structure represents an MLE Link Mode configuration.
typedef int16_t otNeighborInfoIterator
Used to iterate through neighbor table.
typedef struct otLeaderData otLeaderData
This structure represents the Thread Leader Data.
typedef struct otIpCounters otIpCounters
This structure represents the IP level counters.
typedef struct otMleCounters otMleCounters
This structure represents the Thread MLE counters.
typedef struct otThreadParentResponseInfo otThreadParentResponseInfo
This structure represents the MLE Parent Response data.
typedef void(* otThreadParentResponseCallback ) ( otThreadParentResponseInfo *aInfo, void *aContext)
This function pointer is called every time an MLE Parent Response message is received.
typedef struct otThreadDiscoveryRequestInfo otThreadDiscoveryRequestInfo
This structure represents the Thread Discovery Request data.
typedef void(* otThreadDiscoveryRequestCallback ) (const otThreadDiscoveryRequestInfo *aInfo, void *aContext)
This function pointer is called every time an MLE Discovery Request message is received.
typedef void(* otThreadAnycastLocatorCallback ) (void *aContext, otError aError, const otIp6Address *aMeshLocalAddress, uint16_t aRloc16)
This function pointer type defines the callback to notify the outcome of a otThreadLocateAnycastDestination() request.

Enumerations

enum otRoutePreference {
OT_ROUTE_PREFERENCE_LOW = -1,
OT_ROUTE_PREFERENCE_MED = 0,
OT_ROUTE_PREFERENCE_HIGH = 1
}
Defines valid values for mPreference in otExternalRouteConfig and otBorderRouterConfig .
enum otNetDataPublisherEvent {
OT_NETDATA_PUBLISHER_EVENT_ENTRY_ADDED = 0,
OT_NETDATA_PUBLISHER_EVENT_ENTRY_REMOVED = 1
}
This enumeration represents the events reported from the Publisher callbacks.
enum {
OT_NETWORK_DIAGNOSTIC_TLV_EXT_ADDRESS = 0,
OT_NETWORK_DIAGNOSTIC_TLV_SHORT_ADDRESS = 1,
OT_NETWORK_DIAGNOSTIC_TLV_MODE = 2,
OT_NETWORK_DIAGNOSTIC_TLV_TIMEOUT = 3,
OT_NETWORK_DIAGNOSTIC_TLV_CONNECTIVITY = 4,
OT_NETWORK_DIAGNOSTIC_TLV_ROUTE = 5,
OT_NETWORK_DIAGNOSTIC_TLV_LEADER_DATA = 6,
OT_NETWORK_DIAGNOSTIC_TLV_NETWORK_DATA = 7,
OT_NETWORK_DIAGNOSTIC_TLV_IP6_ADDR_LIST = 8,
OT_NETWORK_DIAGNOSTIC_TLV_MAC_COUNTERS = 9,
OT_NETWORK_DIAGNOSTIC_TLV_BATTERY_LEVEL = 14,
OT_NETWORK_DIAGNOSTIC_TLV_SUPPLY_VOLTAGE = 15,
OT_NETWORK_DIAGNOSTIC_TLV_CHILD_TABLE = 16,
OT_NETWORK_DIAGNOSTIC_TLV_CHANNEL_PAGES = 17,
OT_NETWORK_DIAGNOSTIC_TLV_TYPE_LIST = 18,
OT_NETWORK_DIAGNOSTIC_TLV_MAX_CHILD_TIMEOUT = 19
}
enum otDeviceRole {
OT_DEVICE_ROLE_DISABLED = 0,
OT_DEVICE_ROLE_DETACHED = 1,
OT_DEVICE_ROLE_CHILD = 2,
OT_DEVICE_ROLE_ROUTER = 3,
OT_DEVICE_ROLE_LEADER = 4
}
Represents a Thread device role.

Functions

otError otNetDataGet ( otInstance *aInstance, bool aStable, uint8_t *aData, uint8_t *aDataLength)
This method provides a full or stable copy of the Partition's Thread Network Data.
otError otNetDataGetNextOnMeshPrefix ( otInstance *aInstance, otNetworkDataIterator *aIterator, otBorderRouterConfig *aConfig)
This function gets the next On Mesh Prefix in the partition's Network Data.
otError otNetDataGetNextRoute ( otInstance *aInstance, otNetworkDataIterator *aIterator, otExternalRouteConfig *aConfig)
This function gets the next external route in the partition's Network Data.
otError otNetDataGetNextService ( otInstance *aInstance, otNetworkDataIterator *aIterator, otServiceConfig *aConfig)
This function gets the next service in the partition's Network Data.
uint8_t otNetDataGetVersion ( otInstance *aInstance)
Get the Network Data Version.
uint8_t otNetDataGetStableVersion ( otInstance *aInstance)
Get the Stable Network Data Version.
otError otNetDataSteeringDataCheckJoiner ( otInstance *aInstance, const otExtAddress *aEui64)
Check if the steering data includes a Joiner.
otError otNetDataSteeringDataCheckJoinerWithDiscerner ( otInstance *aInstance, const struct otJoinerDiscerner *aDiscerner)
Check if the steering data includes a Joiner with a given discerner value.
void otNetDataPublishDnsSrpServiceAnycast ( otInstance *aInstance, uint8_t aSequenceNUmber)
This function requests "DNS/SRP Service Anycast Address" to be published in the Thread Network Data.
void otNetDataPublishDnsSrpServiceUnicast ( otInstance *aInstance, const otIp6Address *aAddress, uint16_t aPort)
This function requests "DNS/SRP Service Unicast Address" to be published in the Thread Network Data.
void otNetDataPublishDnsSrpServiceUnicastMeshLocalEid ( otInstance *aInstance, uint16_t aPort)
This function requests "DNS/SRP Service Unicast Address" to be published in the Thread Network Data.
bool otNetDataIsDnsSrpServiceAdded ( otInstance *aInstance)
This function indicates whether or not currently the "DNS/SRP Service" entry is added to the Thread Network Data.
void otNetDataSetDnsSrpServicePublisherCallback ( otInstance *aInstance, otNetDataDnsSrpServicePublisherCallback aCallback, void *aContext)
This function sets a callback for notifying when a published "DNS/SRP Service" is actually added to or removed from the Thread Network Data.
void otNetDataUnpublishDnsSrpService ( otInstance *aInstance)
This function unpublishes any previously added "DNS/SRP (Anycast or Unicast) Service" entry from the Thread Network Data.
otError otNetDataPublishOnMeshPrefix ( otInstance *aInstance, const otBorderRouterConfig *aConfig)
This function requests an on-mesh prefix to be published in the Thread Network Data.
otError otNetDataPublishExternalRoute ( otInstance *aInstance, const otExternalRouteConfig *aConfig)
This function requests an external route prefix to be published in the Thread Network Data.
bool otNetDataIsPrefixAdded ( otInstance *aInstance, const otIp6Prefix *aPrefix)
This function indicates whether or not currently a published prefix entry (on-mesh or external route) is added to the Thread Network Data.
void otNetDataSetPrefixPublisherCallback ( otInstance *aInstance, otNetDataPrefixPublisherCallback aCallback, void *aContext)
This function sets a callback for notifying when a published prefix entry is actually added to or removed from the Thread Network Data.
otError otNetDataUnpublishPrefix ( otInstance *aInstance, const otIp6Prefix *aPrefix)
This function unpublishes a previously published prefix (on-mesh or external route).
otError otThreadGetNextDiagnosticTlv (const otMessage *aMessage, otNetworkDiagIterator *aIterator, otNetworkDiagTlv *aNetworkDiagTlv)
This function gets the next Network Diagnostic TLV in the message.
otError otThreadSendDiagnosticGet ( otInstance *aInstance, const otIp6Address *aDestination, const uint8_t aTlvTypes[], uint8_t aCount, otReceiveDiagnosticGetCallback aCallback, void *aCallbackContext)
Send a Network Diagnostic Get request.
otError otThreadSendDiagnosticReset ( otInstance *aInstance, const otIp6Address *aDestination, const uint8_t aTlvTypes[], uint8_t aCount)
Send a Network Diagnostic Reset request.
otError otThreadSetEnabled ( otInstance *aInstance, bool aEnabled)
This function starts Thread protocol operation.
uint16_t otThreadGetVersion (void)
This function gets the Thread protocol version.
bool otThreadIsSingleton ( otInstance *aInstance)
This function indicates whether a node is the only router on the network.
otError otThreadDiscover ( otInstance *aInstance, uint32_t aScanChannels, uint16_t aPanId, bool aJoiner, bool aEnableEui64Filtering, otHandleActiveScanResult aCallback, void *aCallbackContext)
This function starts a Thread Discovery scan.
bool otThreadIsDiscoverInProgress ( otInstance *aInstance)
This function determines if an MLE Thread Discovery is currently in progress.
otError otThreadSetJoinerAdvertisement ( otInstance *aInstance, uint32_t aOui, const uint8_t *aAdvData, uint8_t aAdvDataLength)
This method sets the Thread Joiner Advertisement when discovering Thread network.
uint32_t otThreadGetChildTimeout ( otInstance *aInstance)
Get the Thread Child Timeout used when operating in the Child role.
void otThreadSetChildTimeout ( otInstance *aInstance, uint32_t aTimeout)
Set the Thread Child Timeout used when operating in the Child role.
const otExtendedPanId * otThreadGetExtendedPanId ( otInstance *aInstance)
Get the IEEE 802.15.4 Extended PAN ID.
otError otThreadSetExtendedPanId ( otInstance *aInstance, const otExtendedPanId *aExtendedPanId)
Set the IEEE 802.15.4 Extended PAN ID.
otError otThreadGetLeaderRloc ( otInstance *aInstance, otIp6Address *aLeaderRloc)
This function returns a pointer to the Leader's RLOC.
otLinkModeConfig otThreadGetLinkMode ( otInstance *aInstance)
Get the MLE Link Mode configuration.
otError otThreadSetLinkMode ( otInstance *aInstance, otLinkModeConfig aConfig)
Set the MLE Link Mode configuration.
void otThreadGetNetworkKey ( otInstance *aInstance, otNetworkKey *aNetworkKey)
Get the Thread Network Key.
otNetworkKeyRef otThreadGetNetworkKeyRef ( otInstance *aInstance)
Get the otNetworkKeyRef for Thread Network Key.
otError otThreadSetNetworkKey ( otInstance *aInstance, const otNetworkKey *aKey)
Set the Thread Network Key.
otError otThreadSetNetworkKeyRef ( otInstance *aInstance, otNetworkKeyRef aKeyRef)
Set the Thread Network Key as a otNetworkKeyRef .
const otIp6Address * otThreadGetRloc ( otInstance *aInstance)
This function returns a pointer to the Thread Routing Locator (RLOC) address.
const otIp6Address * otThreadGetMeshLocalEid ( otInstance *aInstance)
This function returns a pointer to the Mesh Local EID address.
const otMeshLocalPrefix * otThreadGetMeshLocalPrefix ( otInstance *aInstance)
This function returns a pointer to the Mesh Local Prefix.
otError otThreadSetMeshLocalPrefix ( otInstance *aInstance, const otMeshLocalPrefix *aMeshLocalPrefix)
This function sets the Mesh Local Prefix.
const otIp6Address * otThreadGetLinkLocalIp6Address ( otInstance *aInstance)
This function returns the Thread link-local IPv6 address.
const otIp6Address * otThreadGetLinkLocalAllThreadNodesMulticastAddress ( otInstance *aInstance)
This function returns the Thread Link-Local All Thread Nodes multicast address.
const otIp6Address * otThreadGetRealmLocalAllThreadNodesMulticastAddress ( otInstance *aInstance)
This function returns the Thread Realm-Local All Thread Nodes multicast address.
otError otThreadGetServiceAloc ( otInstance *aInstance, uint8_t aServiceId, otIp6Address *aServiceAloc)
This function retrieves the Service ALOC for given Service ID.
const char * otThreadGetNetworkName ( otInstance *aInstance)
Get the Thread Network Name.
otError otThreadSetNetworkName ( otInstance *aInstance, const char *aNetworkName)
Set the Thread Network Name.
const char * otThreadGetDomainName ( otInstance *aInstance)
Get the Thread Domain Name.
otError otThreadSetDomainName ( otInstance *aInstance, const char *aDomainName)
Set the Thread Domain Name.
otError otThreadSetFixedDuaInterfaceIdentifier ( otInstance *aInstance, const otIp6InterfaceIdentifier *aIid)
Set/Clear the Interface Identifier manually specified for the Thread Domain Unicast Address.
const otIp6InterfaceIdentifier * otThreadGetFixedDuaInterfaceIdentifier ( otInstance *aInstance)
Get the Interface Identifier manually specified for the Thread Domain Unicast Address.
uint32_t otThreadGetKeySequenceCounter ( otInstance *aInstance)
Get the thrKeySequenceCounter.
void otThreadSetKeySequenceCounter ( otInstance *aInstance, uint32_t aKeySequenceCounter)
Set the thrKeySequenceCounter.
uint32_t otThreadGetKeySwitchGuardTime ( otInstance *aInstance)
Get the thrKeySwitchGuardTime.
void otThreadSetKeySwitchGuardTime ( otInstance *aInstance, uint32_t aKeySwitchGuardTime)
Set the thrKeySwitchGuardTime.
otError otThreadBecomeDetached ( otInstance *aInstance)
Detach from the Thread network.
otError otThreadBecomeChild ( otInstance *aInstance)
Attempt to reattach as a child.
otError otThreadGetNextNeighborInfo ( otInstance *aInstance, otNeighborInfoIterator *aIterator, otNeighborInfo *aInfo)
This function gets the next neighbor information.
otDeviceRole otThreadGetDeviceRole ( otInstance *aInstance)
Get the device role.
const char * otThreadDeviceRoleToString ( otDeviceRole aRole)
Convert the device role to human-readable string.
otError otThreadGetLeaderData ( otInstance *aInstance, otLeaderData *aLeaderData)
This function get the Thread Leader Data.
uint8_t otThreadGetLeaderRouterId ( otInstance *aInstance)
Get the Leader's Router ID.
uint8_t otThreadGetLeaderWeight ( otInstance *aInstance)
Get the Leader's Weight.
uint32_t otThreadGetPartitionId ( otInstance *aInstance)
Get the Partition ID.
uint16_t otThreadGetRloc16 ( otInstance *aInstance)
Get the RLOC16.
otError otThreadGetParentInfo ( otInstance *aInstance, otRouterInfo *aParentInfo)
The function retrieves diagnostic information for a Thread Router as parent.
otError otThreadGetParentAverageRssi ( otInstance *aInstance, int8_t *aParentRssi)
The function retrieves the average RSSI for the Thread Parent.
otError otThreadGetParentLastRssi ( otInstance *aInstance, int8_t *aLastRssi)
The function retrieves the RSSI of the last packet from the Thread Parent.
const otIpCounters * otThreadGetIp6Counters ( otInstance *aInstance)
Get the IPv6 counters.
void otThreadResetIp6Counters ( otInstance *aInstance)
Reset the IPv6 counters.
const otMleCounters * otThreadGetMleCounters ( otInstance *aInstance)
Get the Thread MLE counters.
void otThreadResetMleCounters ( otInstance *aInstance)
Reset the Thread MLE counters.
void otThreadRegisterParentResponseCallback ( otInstance *aInstance, otThreadParentResponseCallback aCallback, void *aContext)
This function registers a callback to receive MLE Parent Response data.
void otThreadSetDiscoveryRequestCallback ( otInstance *aInstance, otThreadDiscoveryRequestCallback aCallback, void *aContext)
This function sets a callback to receive MLE Discovery Request data.
otError otThreadLocateAnycastDestination ( otInstance *aInstance, const otIp6Address *aAnycastAddress, otThreadAnycastLocatorCallback aCallback, void *aContext)
This function requests the closest destination of a given anycast address to be located.
bool otThreadIsAnycastLocateInProgress ( otInstance *aInstance)
This function indicates whether an anycast locate request is currently in progress.
void otThreadSendAddressNotification ( otInstance *aInstance, otIp6Address *aDestination, otIp6Address *aTarget, otIp6InterfaceIdentifier *aMlIid)
This function sends a Proactive Address Notification (ADDR_NTF.ntf) message.
otError otThreadSendProactiveBackboneNotification ( otInstance *aInstance, otIp6Address *aTarget, otIp6InterfaceIdentifier *aMlIid, uint32_t aTimeSinceLastTransaction)
This function sends a Proactive Backbone Notification (PRO_BB.ntf) message on the Backbone link.

Detailed Description

This module includes functions for all Thread roles.

The Network Data Publisher provides mechanisms to limit the number of similar Service and/or Prefix (on-mesh prefix or external route) entries in the Thread Network Data by monitoring the Network Data and managing if or when to add or remove entries.

All the functions in this module require OPENTHREAD_CONFIG_NETDATA_PUBLISHER_ENABLE to be enabled.

Note
The functions in this module require OPENTHREAD_FTD=1 or OPENTHREAD_MTD=1 .

Typedef Documentation

◆ otNetDataDnsSrpServicePublisherCallback

typedef void(* otNetDataDnsSrpServicePublisherCallback) ( otNetDataPublisherEvent aEvent, void *aContext)

This function pointer type defines the callback used to notify when a "DNS/SRP Service" entry is added to or removed from the Thread Network Data.

On remove the callback is invoked independent of whether the entry is removed by Publisher (e.g., when there are too many similar entries already present in the Network Data) or through an explicit call to unpublish the entry (i.e., a call to otNetDataUnpublishDnsSrpService() ).

Parameters
[in] aEvent Indicates the event (whether the entry was added or removed).
[in] aContext A pointer to application-specific context.

◆ otNetDataPrefixPublisherCallback

typedef void(* otNetDataPrefixPublisherCallback) ( otNetDataPublisherEvent aEvent, const otIp6Prefix *aPrefix, void *aContext)

This function pointer type defines the callback used to notify when a prefix (on-mesh or external route) entry is added to or removed from the Thread Network Data.

On remove the callback is invoked independent of whether the entry is removed by Publisher (e.g., when there are too many similar entries already present in the Network Data) or through an explicit call to unpublish the entry.

Parameters
[in] aEvent Indicates the event (whether the entry was added or removed).
[in] aPrefix A pointer to the prefix entry.
[in] aContext A pointer to application-specific context.

◆ otNetworkDiagMacCounters

This structure represents a Network Diagnostic Mac Counters value.

See RFC 2863 for definitions of member fields.

◆ otReceiveDiagnosticGetCallback

typedef void(* otReceiveDiagnosticGetCallback) ( otError aError, otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext)

This function pointer is called when Network Diagnostic Get response is received.

Parameters
[in] aError The error when failed to get the response.
[in] aMessage A pointer to the message buffer containing the received Network Diagnostic Get response payload. Available only when aError is OT_ERROR_NONE .
[in] aMessageInfo A pointer to the message info for aMessage . Available only when aError is OT_ERROR_NONE .
[in] aContext A pointer to application-specific context.

◆ otThreadAnycastLocatorCallback

typedef void(* otThreadAnycastLocatorCallback) (void *aContext, otError aError, const otIp6Address *aMeshLocalAddress, uint16_t aRloc16)

This function pointer type defines the callback to notify the outcome of a otThreadLocateAnycastDestination() request.

Parameters
[in] aContext A pointer to an arbitrary context (provided when callback is registered).
[in] aError The error when handling the request. OT_ERROR_NONE indicates success. OT_ERROR_RESPONSE_TIMEOUT indicates a destination could not be found. OT_ERROR_ABORT indicates the request was aborted.
[in] aMeshLocalAddress A pointer to the mesh-local EID of the closest destination of the anycast address when aError is OT_ERROR_NONE, NULL otherwise.
[in] aRloc16 The RLOC16 of the destination if found, otherwise invalid RLOC16 (0xfffe).

◆ otThreadDiscoveryRequestCallback

typedef void(* otThreadDiscoveryRequestCallback) (const otThreadDiscoveryRequestInfo *aInfo, void *aContext)

This function pointer is called every time an MLE Discovery Request message is received.

Parameters
[in] aInfo A pointer to the Discovery Request info data.
[in] aContext A pointer to callback application-specific context.

◆ otThreadParentResponseCallback

typedef void(* otThreadParentResponseCallback) ( otThreadParentResponseInfo *aInfo, void *aContext)

This function pointer is called every time an MLE Parent Response message is received.

Parameters
[in] aStats pointer to a location on stack holding the stats data.
[in] aContext A pointer to callback client-specific context.

Enumeration Type Documentation

◆ anonymous enum

anonymous enum
Enumerator
OT_NETWORK_DIAGNOSTIC_TLV_EXT_ADDRESS

MAC Extended Address TLV.

OT_NETWORK_DIAGNOSTIC_TLV_SHORT_ADDRESS

Address16 TLV.

OT_NETWORK_DIAGNOSTIC_TLV_MODE

Mode TLV.

OT_NETWORK_DIAGNOSTIC_TLV_TIMEOUT

Timeout TLV (the maximum polling time period for SEDs)

OT_NETWORK_DIAGNOSTIC_TLV_CONNECTIVITY

Connectivity TLV.

OT_NETWORK_DIAGNOSTIC_TLV_ROUTE

Route64 TLV.

OT_NETWORK_DIAGNOSTIC_TLV_LEADER_DATA

Leader Data TLV.

OT_NETWORK_DIAGNOSTIC_TLV_NETWORK_DATA

Network Data TLV.

OT_NETWORK_DIAGNOSTIC_TLV_IP6_ADDR_LIST

IPv6 Address List TLV.

OT_NETWORK_DIAGNOSTIC_TLV_MAC_COUNTERS

MAC Counters TLV.

OT_NETWORK_DIAGNOSTIC_TLV_BATTERY_LEVEL

Battery Level TLV.

OT_NETWORK_DIAGNOSTIC_TLV_SUPPLY_VOLTAGE

Supply Voltage TLV.

OT_NETWORK_DIAGNOSTIC_TLV_CHILD_TABLE

Child Table TLV.

OT_NETWORK_DIAGNOSTIC_TLV_CHANNEL_PAGES

Channel Pages TLV.

OT_NETWORK_DIAGNOSTIC_TLV_TYPE_LIST

Type List TLV.

OT_NETWORK_DIAGNOSTIC_TLV_MAX_CHILD_TIMEOUT

Max Child Timeout TLV.

◆ otDeviceRole

Represents a Thread device role.

Enumerator
OT_DEVICE_ROLE_DISABLED

The Thread stack is disabled.

OT_DEVICE_ROLE_DETACHED

Not currently participating in a Thread network/partition.

OT_DEVICE_ROLE_CHILD

The Thread Child role.

OT_DEVICE_ROLE_ROUTER

The Thread Router role.

OT_DEVICE_ROLE_LEADER

The Thread Leader role.

◆ otNetDataPublisherEvent

This enumeration represents the events reported from the Publisher callbacks.

Enumerator
OT_NETDATA_PUBLISHER_EVENT_ENTRY_ADDED

Published entry is added to the Thread Network Data.

OT_NETDATA_PUBLISHER_EVENT_ENTRY_REMOVED

Published entry is removed from the Thread Network Data.

◆ otRoutePreference

Defines valid values for mPreference in otExternalRouteConfig and otBorderRouterConfig .

Enumerator
OT_ROUTE_PREFERENCE_LOW

Low route preference.

OT_ROUTE_PREFERENCE_MED

Medium route preference.

OT_ROUTE_PREFERENCE_HIGH

High route preference.

Function Documentation

◆ otNetDataGet()

otError otNetDataGet ( otInstance * aInstance,
bool aStable,
uint8_t * aData,
uint8_t * aDataLength
)

This method provides a full or stable copy of the Partition's Thread Network Data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aStable TRUE when copying the stable version, FALSE when copying the full version.
[out] aData A pointer to the data buffer.
[in,out] aDataLength On entry, size of the data buffer pointed to by aData . On exit, number of copied bytes.

◆ otNetDataGetNextOnMeshPrefix()

otError otNetDataGetNextOnMeshPrefix ( otInstance * aInstance,
otNetworkDataIterator * aIterator,
otBorderRouterConfig * aConfig
)

This function gets the next On Mesh Prefix in the partition's Network Data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in,out] aIterator A pointer to the Network Data iterator context. To get the first on-mesh entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT.
[out] aConfig A pointer to where the On Mesh Prefix information will be placed.
Return values
OT_ERROR_NONE Successfully found the next On Mesh prefix.
OT_ERROR_NOT_FOUND No subsequent On Mesh prefix exists in the Thread Network Data.

◆ otNetDataGetNextRoute()

otError otNetDataGetNextRoute ( otInstance * aInstance,
otNetworkDataIterator * aIterator,
otExternalRouteConfig * aConfig
)

This function gets the next external route in the partition's Network Data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in,out] aIterator A pointer to the Network Data iterator context. To get the first external route entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT.
[out] aConfig A pointer to where the External Route information will be placed.
Return values
OT_ERROR_NONE Successfully found the next External Route.
OT_ERROR_NOT_FOUND No subsequent external route entry exists in the Thread Network Data.

◆ otNetDataGetNextService()

otError otNetDataGetNextService ( otInstance * aInstance,
otNetworkDataIterator * aIterator,
otServiceConfig * aConfig
)

This function gets the next service in the partition's Network Data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in,out] aIterator A pointer to the Network Data iterator context. To get the first service entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT.
[out] aConfig A pointer to where the service information will be placed.
Return values
OT_ERROR_NONE Successfully found the next service.
OT_ERROR_NOT_FOUND No subsequent service exists in the partition's Network Data.

◆ otNetDataGetStableVersion()

uint8_t otNetDataGetStableVersion ( otInstance * aInstance )

Get the Stable Network Data Version.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Stable Network Data Version.

◆ otNetDataGetVersion()

uint8_t otNetDataGetVersion ( otInstance * aInstance )

Get the Network Data Version.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Network Data Version.

◆ otNetDataIsDnsSrpServiceAdded()

bool otNetDataIsDnsSrpServiceAdded ( otInstance * aInstance )

This function indicates whether or not currently the "DNS/SRP Service" entry is added to the Thread Network Data.

This function requires the feature OPENTHREAD_CONFIG_TMF_NETDATA_SERVICE_ENABLE to be enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
TRUE The published DNS/SRP Service entry is added to the Thread Network Data.
FALSE The entry is not added to Thread Network Data or there is no entry to publish.

◆ otNetDataIsPrefixAdded()

bool otNetDataIsPrefixAdded ( otInstance * aInstance,
const otIp6Prefix * aPrefix
)

This function indicates whether or not currently a published prefix entry (on-mesh or external route) is added to the Thread Network Data.

This function requires the feature OPENTHREAD_CONFIG_BORDER_ROUTER_ENABLE to be enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPrefix A pointer to the prefix (MUST NOT be NULL).
Return values
TRUE The published prefix entry is added to the Thread Network Data.
FALSE The entry is not added to Thread Network Data or there is no entry to publish.

◆ otNetDataPublishDnsSrpServiceAnycast()

void otNetDataPublishDnsSrpServiceAnycast ( otInstance * aInstance,
uint8_t aSequenceNUmber
)

This function requests "DNS/SRP Service Anycast Address" to be published in the Thread Network Data.

This function requires the feature OPENTHREAD_CONFIG_TMF_NETDATA_SERVICE_ENABLE to be enabled.

A call to this function will remove and replace any previous "DNS/SRP Service" entry that was being published (from earlier call to any of otNetDataPublishDnsSrpService{Type}() functions).

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aSequenceNUmber The sequence number of DNS/SRP Anycast Service.

◆ otNetDataPublishDnsSrpServiceUnicast()

void otNetDataPublishDnsSrpServiceUnicast ( otInstance * aInstance,
const otIp6Address * aAddress,
uint16_t aPort
)

This function requests "DNS/SRP Service Unicast Address" to be published in the Thread Network Data.

This function requires the feature OPENTHREAD_CONFIG_TMF_NETDATA_SERVICE_ENABLE to be enabled.

A call to this function will remove and replace any previous "DNS/SRP Service" entry that was being published (from earlier call to any of otNetDataPublishDnsSrpService{Type}() functions).

This function publishes the "DNS/SRP Service Unicast Address" by including the address and port info in the Service TLV data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aAddress The DNS/SRP server address to publish (MUST NOT be NULL).
[in] aPort The SRP server port number to publish.

◆ otNetDataPublishDnsSrpServiceUnicastMeshLocalEid()

void otNetDataPublishDnsSrpServiceUnicastMeshLocalEid ( otInstance * aInstance,
uint16_t aPort
)

This function requests "DNS/SRP Service Unicast Address" to be published in the Thread Network Data.

This function requires the feature OPENTHREAD_CONFIG_TMF_NETDATA_SERVICE_ENABLE to be enabled.

A call to this function will remove and replace any previous "DNS/SRP Service" entry that was being published (from earlier call to any of otNetDataPublishDnsSrpService{Type}() functions).

Unlike otNetDataPublishDnsSrpServiceUnicast() which requires the published address to be given and includes the info in the Service TLV data, this function uses the device's mesh-local EID and includes the info in the Server TLV data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPort The SRP server port number to publish.

◆ otNetDataPublishExternalRoute()

otError otNetDataPublishExternalRoute ( otInstance * aInstance,
const otExternalRouteConfig * aConfig
)

This function requests an external route prefix to be published in the Thread Network Data.

This function requires the feature OPENTHREAD_CONFIG_BORDER_ROUTER_ENABLE to be enabled.

Only stable entries can be published (i.e., aConfig.mStable MUST be TRUE).

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aConfig The external route config to publish (MUST NOT be NULL).
Return values
OT_ERROR_NONE The external route is published successfully.
OT_ERROR_INVALID_ARGS The aConfig is not valid (bad prefix, invalid flag combinations, or not stable).
OT_ERROR_ALREADY An entry with the same prefix is already in the published list.
OT_ERROR_NO_BUFS Could not allocate an entry for the new request. Publisher supports a limited number of entries (shared between on-mesh prefix and external route) determined by config OPENTHREAD_CONFIG_NETDATA_PUBLISHER_MAX_PREFIX_ENTRIES .

◆ otNetDataPublishOnMeshPrefix()

otError otNetDataPublishOnMeshPrefix ( otInstance * aInstance,
const otBorderRouterConfig * aConfig
)

This function requests an on-mesh prefix to be published in the Thread Network Data.

This function requires the feature OPENTHREAD_CONFIG_BORDER_ROUTER_ENABLE to be enabled.

Only stable entries can be published (i.e., aConfig.mStable MUST be TRUE).

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aConfig The on-mesh prefix config to publish (MUST NOT be NULL).
Return values
OT_ERROR_NONE The on-mesh prefix is published successfully.
OT_ERROR_INVALID_ARGS The aConfig is not valid (bad prefix, invalid flag combinations, or not stable).
OT_ERROR_ALREADY An entry with the same prefix is already in the published list.
OT_ERROR_NO_BUFS Could not allocate an entry for the new request. Publisher supports a limited number of entries (shared between on-mesh prefix and external route) determined by config OPENTHREAD_CONFIG_NETDATA_PUBLISHER_MAX_PREFIX_ENTRIES .

◆ otNetDataSetDnsSrpServicePublisherCallback()

void otNetDataSetDnsSrpServicePublisherCallback ( otInstance * aInstance,
otNetDataDnsSrpServicePublisherCallback aCallback,
void * aContext
)

This function sets a callback for notifying when a published "DNS/SRP Service" is actually added to or removed from the Thread Network Data.

A subsequent call to this function replaces any previously set callback function.

This function requires the feature OPENTHREAD_CONFIG_TMF_NETDATA_SERVICE_ENABLE to be enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aCallback The callback function pointer (can be NULL if not needed).
[in] aContext A pointer to application-specific context (used when aCallback is invoked).

◆ otNetDataSetPrefixPublisherCallback()

void otNetDataSetPrefixPublisherCallback ( otInstance * aInstance,
otNetDataPrefixPublisherCallback aCallback,
void * aContext
)

This function sets a callback for notifying when a published prefix entry is actually added to or removed from the Thread Network Data.

A subsequent call to this function replaces any previously set callback function.

This function requires the feature OPENTHREAD_CONFIG_BORDER_ROUTER_ENABLE to be enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aCallback The callback function pointer (can be NULL if not needed).
[in] aContext A pointer to application-specific context (used when aCallback is invoked).

◆ otNetDataSteeringDataCheckJoiner()

otError otNetDataSteeringDataCheckJoiner ( otInstance * aInstance,
const otExtAddress * aEui64
)

Check if the steering data includes a Joiner.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aEui64 A pointer to the Joiner's IEEE EUI-64.
Return values
OT_ERROR_NONE aEui64 is included in the steering data.
OT_ERROR_INVALID_STATE No steering data present.
OT_ERROR_NOT_FOUND aEui64 is not included in the steering data.

◆ otNetDataSteeringDataCheckJoinerWithDiscerner()

otError otNetDataSteeringDataCheckJoinerWithDiscerner ( otInstance * aInstance,
const struct otJoinerDiscerner * aDiscerner
)

Check if the steering data includes a Joiner with a given discerner value.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDiscerner A pointer to the Joiner Discerner.
Return values
OT_ERROR_NONE aDiscerner is included in the steering data.
OT_ERROR_INVALID_STATE No steering data present.
OT_ERROR_NOT_FOUND aDiscerner is not included in the steering data.

◆ otNetDataUnpublishDnsSrpService()

void otNetDataUnpublishDnsSrpService ( otInstance * aInstance )

This function unpublishes any previously added "DNS/SRP (Anycast or Unicast) Service" entry from the Thread Network Data.

This function requires the feature OPENTHREAD_CONFIG_TMF_NETDATA_SERVICE_ENABLE to be enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otNetDataUnpublishPrefix()

otError otNetDataUnpublishPrefix ( otInstance * aInstance,
const otIp6Prefix * aPrefix
)

This function unpublishes a previously published prefix (on-mesh or external route).

This function requires the feature OPENTHREAD_CONFIG_BORDER_ROUTER_ENABLE to be enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aPrefix The prefix to unpublish (MUST NOT be NULL).
Return values
OT_ERROR_NONE The prefix was unpublished successfully.
OT_ERROR_NOT_FOUND Could not find the prefix in the published list.

◆ otThreadBecomeChild()

otError otThreadBecomeChild ( otInstance * aInstance )

Attempt to reattach as a child.

Note
This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NONE Successfully begin attempt to become a child.
OT_ERROR_INVALID_STATE Thread is disabled.

◆ otThreadBecomeDetached()

otError otThreadBecomeDetached ( otInstance * aInstance )

Detach from the Thread network.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NONE Successfully detached from the Thread network.
OT_ERROR_INVALID_STATE Thread is disabled.

◆ otThreadDeviceRoleToString()

const char* otThreadDeviceRoleToString ( otDeviceRole aRole )

Convert the device role to human-readable string.

Parameters
[in] aRole The device role to convert.
Returns
A string representing aRole .

◆ otThreadDiscover()

otError otThreadDiscover ( otInstance * aInstance,
uint32_t aScanChannels,
uint16_t aPanId,
bool aJoiner,
bool aEnableEui64Filtering,
otHandleActiveScanResult aCallback,
void * aCallbackContext
)

This function starts a Thread Discovery scan.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aScanChannels A bit vector indicating which channels to scan (e.g. OT_CHANNEL_11_MASK).
[in] aPanId The PAN ID filter (set to Broadcast PAN to disable filter).
[in] aJoiner Value of the Joiner Flag in the Discovery Request TLV.
[in] aEnableEui64Filtering TRUE to filter responses on EUI-64, FALSE otherwise.
[in] aCallback A pointer to a function called on receiving an MLE Discovery Response or scan completes.
[in] aCallbackContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Successfully started a Thread Discovery Scan.
OT_ERROR_INVALID_STATE The IPv6 interface is not enabled (netif is not up).
OT_ERROR_NO_BUFS Could not allocate message for Discovery Request.
OT_ERROR_BUSY Thread Discovery Scan is already in progress.

◆ otThreadGetChildTimeout()

uint32_t otThreadGetChildTimeout ( otInstance * aInstance )

Get the Thread Child Timeout used when operating in the Child role.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Thread Child Timeout value in seconds.
See also
otThreadSetChildTimeout

◆ otThreadGetDeviceRole()

otDeviceRole otThreadGetDeviceRole ( otInstance * aInstance )

Get the device role.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_DEVICE_ROLE_DISABLED The Thread stack is disabled.
OT_DEVICE_ROLE_DETACHED The device is not currently participating in a Thread network/partition.
OT_DEVICE_ROLE_CHILD The device is currently operating as a Thread Child.
OT_DEVICE_ROLE_ROUTER The device is currently operating as a Thread Router.
OT_DEVICE_ROLE_LEADER The device is currently operating as a Thread Leader.

◆ otThreadGetDomainName()

const char* otThreadGetDomainName ( otInstance * aInstance )

Get the Thread Domain Name.

This function is only available since Thread 1.2.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the Thread Domain Name.
See also
otThreadSetDomainName

◆ otThreadGetExtendedPanId()

const otExtendedPanId * otThreadGetExtendedPanId ( otInstance * aInstance )

Get the IEEE 802.15.4 Extended PAN ID.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the IEEE 802.15.4 Extended PAN ID.
See also
otThreadSetExtendedPanId

◆ otThreadGetFixedDuaInterfaceIdentifier()

const otIp6InterfaceIdentifier * otThreadGetFixedDuaInterfaceIdentifier ( otInstance * aInstance )

Get the Interface Identifier manually specified for the Thread Domain Unicast Address.

This function is only available since Thread 1.2 when OPENTHREAD_CONFIG_DUA_ENABLE is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the Interface Identifier which was set manually, or NULL if none was set.
See also
otThreadSetFixedDuaInterfaceIdentifier

◆ otThreadGetIp6Counters()

const otIpCounters * otThreadGetIp6Counters ( otInstance * aInstance )

Get the IPv6 counters.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the IPv6 counters.

◆ otThreadGetKeySequenceCounter()

uint32_t otThreadGetKeySequenceCounter ( otInstance * aInstance )

Get the thrKeySequenceCounter.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The thrKeySequenceCounter value.
See also
otThreadSetKeySequenceCounter

◆ otThreadGetKeySwitchGuardTime()

uint32_t otThreadGetKeySwitchGuardTime ( otInstance * aInstance )

Get the thrKeySwitchGuardTime.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The thrKeySwitchGuardTime value (in hours).
See also
otThreadSetKeySwitchGuardTime

◆ otThreadGetLeaderData()

otError otThreadGetLeaderData ( otInstance * aInstance,
otLeaderData * aLeaderData
)

This function get the Thread Leader Data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aLeaderData A pointer to where the leader data is placed.
Return values
OT_ERROR_NONE Successfully retrieved the leader data.
OT_ERROR_DETACHED Not currently attached.

◆ otThreadGetLeaderRloc()

otError otThreadGetLeaderRloc ( otInstance * aInstance,
otIp6Address * aLeaderRloc
)

This function returns a pointer to the Leader's RLOC.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aLeaderRloc A pointer to the Leader's RLOC.
Return values
OT_ERROR_NONE The Leader's RLOC was successfully written to aLeaderRloc .
OT_ERROR_INVALID_ARGS aLeaderRloc was NULL.
OT_ERROR_DETACHED Not currently attached to a Thread Partition.

◆ otThreadGetLeaderRouterId()

uint8_t otThreadGetLeaderRouterId ( otInstance * aInstance )

Get the Leader's Router ID.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Leader's Router ID.

◆ otThreadGetLeaderWeight()

uint8_t otThreadGetLeaderWeight ( otInstance * aInstance )

Get the Leader's Weight.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Leader's Weight.

◆ otThreadGetLinkLocalAllThreadNodesMulticastAddress()

const otIp6Address * otThreadGetLinkLocalAllThreadNodesMulticastAddress ( otInstance * aInstance )

This function returns the Thread Link-Local All Thread Nodes multicast address.

The address is a link-local Unicast Prefix-Based Multcast Address [RFC 3306], with:

  • flgs set to 3 (P = 1 and T = 1)
  • scop set to 2
  • plen set to 64
  • network prefix set to the Mesh Local Prefix
  • group ID set to 1
Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to Thread Link-Local All Thread Nodes multicast address.

◆ otThreadGetLinkLocalIp6Address()

const otIp6Address * otThreadGetLinkLocalIp6Address ( otInstance * aInstance )

This function returns the Thread link-local IPv6 address.

The Thread link local address is derived using IEEE802.15.4 Extended Address as Interface Identifier.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to Thread link-local IPv6 address.

◆ otThreadGetLinkMode()

otLinkModeConfig otThreadGetLinkMode ( otInstance * aInstance )

Get the MLE Link Mode configuration.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The MLE Link Mode configuration.
See also
otThreadSetLinkMode

◆ otThreadGetMeshLocalEid()

const otIp6Address * otThreadGetMeshLocalEid ( otInstance * aInstance )

This function returns a pointer to the Mesh Local EID address.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the Mesh Local EID address.

◆ otThreadGetMeshLocalPrefix()

const otMeshLocalPrefix * otThreadGetMeshLocalPrefix ( otInstance * aInstance )

This function returns a pointer to the Mesh Local Prefix.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the Mesh Local Prefix.

◆ otThreadGetMleCounters()

const otMleCounters * otThreadGetMleCounters ( otInstance * aInstance )

Get the Thread MLE counters.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the Thread MLE counters.

◆ otThreadGetNetworkKey()

void otThreadGetNetworkKey ( otInstance * aInstance,
otNetworkKey * aNetworkKey
)

Get the Thread Network Key.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aNetworkKey A pointer to an otNetworkkey to return the Thread Network Key.
See also
otThreadSetNetworkKey

◆ otThreadGetNetworkKeyRef()

otNetworkKeyRef otThreadGetNetworkKeyRef ( otInstance * aInstance )

Get the otNetworkKeyRef for Thread Network Key.

This function requires the build-time feature OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE to be enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
Reference to the Thread Network Key stored in memory.
See also
otThreadSetNetworkKeyRef

◆ otThreadGetNetworkName()

const char* otThreadGetNetworkName ( otInstance * aInstance )

Get the Thread Network Name.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the Thread Network Name.
See also
otThreadSetNetworkName

◆ otThreadGetNextDiagnosticTlv()

otError otThreadGetNextDiagnosticTlv ( const otMessage * aMessage,
otNetworkDiagIterator * aIterator,
otNetworkDiagTlv * aNetworkDiagTlv
)

This function gets the next Network Diagnostic TLV in the message.

Parameters
[in] aMessage A pointer to a message.
[in,out] aIterator A pointer to the Network Diagnostic iterator context. To get the first Network Diagnostic TLV it should be set to OT_NETWORK_DIAGNOSTIC_ITERATOR_INIT.
[out] aNetworkDiagTlv A pointer to where the Network Diagnostic TLV information will be placed.
Return values
OT_ERROR_NONE Successfully found the next Network Diagnostic TLV.
OT_ERROR_NOT_FOUND No subsequent Network Diagnostic TLV exists in the message.
OT_ERROR_PARSE Parsing the next Network Diagnostic failed.

A subsequent call to this function is allowed only when current return value is OT_ERROR_NONE.

◆ otThreadGetNextNeighborInfo()

otError otThreadGetNextNeighborInfo ( otInstance * aInstance,
otNeighborInfoIterator * aIterator,
otNeighborInfo * aInfo
)

This function gets the next neighbor information.

It is used to go through the entries of the neighbor table.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in,out] aIterator A pointer to the iterator context. To get the first neighbor entry it should be set to OT_NEIGHBOR_INFO_ITERATOR_INIT.
[out] aInfo A pointer to the neighbor information.
Return values
OT_ERROR_NONE Successfully found the next neighbor entry in table.
OT_ERROR_NOT_FOUND No subsequent neighbor entry exists in the table.
OT_ERROR_INVALID_ARGS aIterator or aInfo was NULL.

◆ otThreadGetParentAverageRssi()

otError otThreadGetParentAverageRssi ( otInstance * aInstance,
int8_t * aParentRssi
)

The function retrieves the average RSSI for the Thread Parent.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aParentRssi A pointer to where the parent RSSI should be placed.

◆ otThreadGetParentInfo()

otError otThreadGetParentInfo ( otInstance * aInstance,
otRouterInfo * aParentInfo
)

The function retrieves diagnostic information for a Thread Router as parent.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aParentInfo A pointer to where the parent router information is placed.

◆ otThreadGetParentLastRssi()

otError otThreadGetParentLastRssi ( otInstance * aInstance,
int8_t * aLastRssi
)

The function retrieves the RSSI of the last packet from the Thread Parent.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aLastRssi A pointer to where the last RSSI should be placed.
Return values
OT_ERROR_NONE Successfully retrieved the RSSI data.
OT_ERROR_FAILED Unable to get RSSI data.
OT_ERROR_INVALID_ARGS aLastRssi is NULL.

◆ otThreadGetPartitionId()

uint32_t otThreadGetPartitionId ( otInstance * aInstance )

Get the Partition ID.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The Partition ID.

◆ otThreadGetRealmLocalAllThreadNodesMulticastAddress()

const otIp6Address * otThreadGetRealmLocalAllThreadNodesMulticastAddress ( otInstance * aInstance )

This function returns the Thread Realm-Local All Thread Nodes multicast address.

The address is a realm-local Unicast Prefix-Based Multcast Address [RFC 3306], with:

  • flgs set to 3 (P = 1 and T = 1)
  • scop set to 3
  • plen set to 64
  • network prefix set to the Mesh Local Prefix
  • group ID set to 1
Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to Thread Realm-Local All Thread Nodes multicast address.

◆ otThreadGetRloc()

const otIp6Address * otThreadGetRloc ( otInstance * aInstance )

This function returns a pointer to the Thread Routing Locator (RLOC) address.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the Thread Routing Locator (RLOC) address.

◆ otThreadGetRloc16()

uint16_t otThreadGetRloc16 ( otInstance * aInstance )

Get the RLOC16.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The RLOC16.

◆ otThreadGetServiceAloc()

otError otThreadGetServiceAloc ( otInstance * aInstance,
uint8_t aServiceId,
otIp6Address * aServiceAloc
)

This function retrieves the Service ALOC for given Service ID.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aServiceId Service ID to get ALOC for.
[out] aServiceAloc A pointer to output the Service ALOC. MUST NOT BE NULL.
Return values
OT_ERROR_NONE Successfully retrieved the Service ALOC.
OT_ERROR_DETACHED The Thread interface is not currently attached to a Thread Partition.

◆ otThreadGetVersion()

uint16_t otThreadGetVersion ( void )

This function gets the Thread protocol version.

Returns
the Thread protocol version.

◆ otThreadIsAnycastLocateInProgress()

bool otThreadIsAnycastLocateInProgress ( otInstance * aInstance )

This function indicates whether an anycast locate request is currently in progress.

This function is only available when OPENTHREAD_CONFIG_TMF_ANYCAST_LOCATOR_ENABLE is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
TRUE if an anycast locate request is currently in progress, FALSE otherwise.

◆ otThreadIsDiscoverInProgress()

bool otThreadIsDiscoverInProgress ( otInstance * aInstance )

This function determines if an MLE Thread Discovery is currently in progress.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otThreadIsSingleton()

bool otThreadIsSingleton ( otInstance * aInstance )

This function indicates whether a node is the only router on the network.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
TRUE It is the only router in the network.
FALSE It is a child or is not a single router in the network.

◆ otThreadLocateAnycastDestination()

otError otThreadLocateAnycastDestination ( otInstance * aInstance,
const otIp6Address * aAnycastAddress,
otThreadAnycastLocatorCallback aCallback,
void * aContext
)

This function requests the closest destination of a given anycast address to be located.

This function is only available when OPENTHREAD_CONFIG_TMF_ANYCAST_LOCATOR_ENABLE is enabled.

If a previous request is ongoing, a subsequent call to this function will cancel and replace the earlier request.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aAnycastAddress The anycast address to locate. MUST NOT be NULL.
[in] aCallback The callback function to report the result.
[in] aContext An arbitrary context used with aCallback .
Return values
OT_ERROR_NONE The request started successfully. aCallback will be invoked to report the result.
OT_ERROR_INVALID_ARGS The aAnycastAddress is not a valid anycast address or aCallback is NULL.
OT_ERROR_NO_BUFS Out of buffer to prepare and send the request message.

◆ otThreadRegisterParentResponseCallback()

void otThreadRegisterParentResponseCallback ( otInstance * aInstance,
otThreadParentResponseCallback aCallback,
void * aContext
)

This function registers a callback to receive MLE Parent Response data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aCallback A pointer to a function that is called upon receiving an MLE Parent Response message.
[in] aContext A pointer to callback client-specific context.

◆ otThreadResetIp6Counters()

void otThreadResetIp6Counters ( otInstance * aInstance )

Reset the IPv6 counters.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otThreadResetMleCounters()

void otThreadResetMleCounters ( otInstance * aInstance )

Reset the Thread MLE counters.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otThreadSendAddressNotification()

void otThreadSendAddressNotification ( otInstance * aInstance,
otIp6Address * aDestination,
otIp6Address * aTarget,
otIp6InterfaceIdentifier * aMlIid
)

This function sends a Proactive Address Notification (ADDR_NTF.ntf) message.

This function is only available when OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDestination The destination to send the ADDR_NTF.ntf message.
[in] aTarget The target address of the ADDR_NTF.ntf message.
[in] aMlIid The ML-IID of the ADDR_NTF.ntf message.

◆ otThreadSendDiagnosticGet()

otError otThreadSendDiagnosticGet ( otInstance * aInstance,
const otIp6Address * aDestination,
const uint8_t aTlvTypes[],
uint8_t aCount,
otReceiveDiagnosticGetCallback aCallback,
void * aCallbackContext
)

Send a Network Diagnostic Get request.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDestination A pointer to destination address.
[in] aTlvTypes An array of Network Diagnostic TLV types.
[in] aCount Number of types in aTlvTypes.
[in] aCallback A pointer to a function that is called when Network Diagnostic Get response is received or NULL to disable the callback.
[in] aCallbackContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Successfully queued the DIAG_GET.req.
OT_ERROR_NO_BUFS Insufficient message buffers available to send DIAG_GET.req.

◆ otThreadSendDiagnosticReset()

otError otThreadSendDiagnosticReset ( otInstance * aInstance,
const otIp6Address * aDestination,
const uint8_t aTlvTypes[],
uint8_t aCount
)

Send a Network Diagnostic Reset request.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDestination A pointer to destination address.
[in] aTlvTypes An array of Network Diagnostic TLV types. Currently only Type 9 is allowed.
[in] aCount Number of types in aTlvTypes
Return values
OT_ERROR_NONE Successfully queued the DIAG_RST.ntf.
OT_ERROR_NO_BUFS Insufficient message buffers available to send DIAG_RST.ntf.

◆ otThreadSendProactiveBackboneNotification()

otError otThreadSendProactiveBackboneNotification ( otInstance * aInstance,
otIp6Address * aTarget,
otIp6InterfaceIdentifier * aMlIid,
uint32_t aTimeSinceLastTransaction
)

This function sends a Proactive Backbone Notification (PRO_BB.ntf) message on the Backbone link.

This function is only available when OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aTarget The target address of the PRO_BB.ntf message.
[in] aMlIid The ML-IID of the PRO_BB.ntf message.
[in] aTimeSinceLastTransaction Time since last transaction (in seconds).
Return values
OT_ERROR_NONE Successfully sent PRO_BB.ntf on backbone link.
OT_ERROR_NO_BUFS If insufficient message buffers available.

◆ otThreadSetChildTimeout()

void otThreadSetChildTimeout ( otInstance * aInstance,
uint32_t aTimeout
)

Set the Thread Child Timeout used when operating in the Child role.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aTimeout The timeout value in seconds.
See also
otThreadGetChildTimeout

◆ otThreadSetDiscoveryRequestCallback()

void otThreadSetDiscoveryRequestCallback ( otInstance * aInstance,
otThreadDiscoveryRequestCallback aCallback,
void * aContext
)

This function sets a callback to receive MLE Discovery Request data.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aCallback A pointer to a function that is called upon receiving an MLE Discovery Request message.
[in] aContext A pointer to callback application-specific context.

◆ otThreadSetDomainName()

otError otThreadSetDomainName ( otInstance * aInstance,
const char * aDomainName
)

Set the Thread Domain Name.

This function is only available since Thread 1.2. This function succeeds only when Thread protocols are disabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDomainName A pointer to the Thread Domain Name.
Return values
OT_ERROR_NONE Successfully set the Thread Domain Name.
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otThreadGetDomainName

◆ otThreadSetEnabled()

otError otThreadSetEnabled ( otInstance * aInstance,
bool aEnabled
)

This function starts Thread protocol operation.

The interface must be up when calling this function.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aEnabled TRUE if Thread is enabled, FALSE otherwise.
Return values
OT_ERROR_NONE Successfully started Thread protocol operation.
OT_ERROR_INVALID_STATE The network interface was not not up.

◆ otThreadSetExtendedPanId()

otError otThreadSetExtendedPanId ( otInstance * aInstance,
const otExtendedPanId * aExtendedPanId
)

Set the IEEE 802.15.4 Extended PAN ID.

This function can only be called while Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aExtendedPanId A pointer to the IEEE 802.15.4 Extended PAN ID.
Return values
OT_ERROR_NONE Successfully set the Extended PAN ID.
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otThreadGetExtendedPanId

◆ otThreadSetFixedDuaInterfaceIdentifier()

otError otThreadSetFixedDuaInterfaceIdentifier ( otInstance * aInstance,
const otIp6InterfaceIdentifier * aIid
)

Set/Clear the Interface Identifier manually specified for the Thread Domain Unicast Address.

This function is only available since Thread 1.2 when OPENTHREAD_CONFIG_DUA_ENABLE is enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aIid A pointer to the Interface Identifier to set or NULL to clear.
Return values
OT_ERROR_NONE Successfully set/cleared the Interface Identifier.
OT_ERROR_INVALID_ARGS The specified Interface Identifier is reserved.
See also
otThreadGetFixedDuaInterfaceIdentifier

◆ otThreadSetJoinerAdvertisement()

otError otThreadSetJoinerAdvertisement ( otInstance * aInstance,
uint32_t aOui,
const uint8_t * aAdvData,
uint8_t aAdvDataLength
)

This method sets the Thread Joiner Advertisement when discovering Thread network.

Thread Joiner Advertisement is used to allow a Joiner to advertise its own application-specific information (such as Vendor ID, Product ID, Discriminator, etc.) via a newly-proposed Joiner Advertisement TLV, and to make this information available to Commissioners or Commissioner Candidates without human interaction.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aOui The Vendor IEEE OUI value that will be included in the Joiner Advertisement. Only the least significant 3 bytes will be used, and the most significant byte will be ignored.
[in] aAdvData A pointer to the AdvData that will be included in the Joiner Advertisement.
[in] aAdvDataLength The length of AdvData in bytes.
Return values
OT_ERROR_NONE Successfully set Joiner Advertisement.
OT_ERROR_INVALID_ARGS Invalid AdvData.

◆ otThreadSetKeySequenceCounter()

void otThreadSetKeySequenceCounter ( otInstance * aInstance,
uint32_t aKeySequenceCounter
)

Set the thrKeySequenceCounter.

Note
This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aKeySequenceCounter The thrKeySequenceCounter value.
See also
otThreadGetKeySequenceCounter

◆ otThreadSetKeySwitchGuardTime()

void otThreadSetKeySwitchGuardTime ( otInstance * aInstance,
uint32_t aKeySwitchGuardTime
)

Set the thrKeySwitchGuardTime.

Note
This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aKeySwitchGuardTime The thrKeySwitchGuardTime value (in hours).
See also
otThreadGetKeySwitchGuardTime

◆ otThreadSetLinkMode()

otError otThreadSetLinkMode ( otInstance * aInstance,
otLinkModeConfig aConfig
)

Set the MLE Link Mode configuration.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aConfig A pointer to the Link Mode configuration.
Return values
OT_ERROR_NONE Successfully set the MLE Link Mode configuration.
See also
otThreadGetLinkMode

◆ otThreadSetMeshLocalPrefix()

otError otThreadSetMeshLocalPrefix ( otInstance * aInstance,
const otMeshLocalPrefix * aMeshLocalPrefix
)

This function sets the Mesh Local Prefix.

This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aMeshLocalPrefix A pointer to the Mesh Local Prefix.
Return values
OT_ERROR_NONE Successfully set the Mesh Local Prefix.
OT_ERROR_INVALID_STATE Thread protocols are enabled.

◆ otThreadSetNetworkKey()

otError otThreadSetNetworkKey ( otInstance * aInstance,
const otNetworkKey * aKey
)

Set the Thread Network Key.

This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aKey A pointer to a buffer containing the Thread Network Key.
Return values
OT_ERROR_NONE Successfully set the Thread Network Key.
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otThreadGetNetworkKey

◆ otThreadSetNetworkKeyRef()

otError otThreadSetNetworkKeyRef ( otInstance * aInstance,
otNetworkKeyRef aKeyRef
)

Set the Thread Network Key as a otNetworkKeyRef .

This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.

This function requires the build-time feature OPENTHREAD_CONFIG_PLATFORM_KEY_REFERENCES_ENABLE to be enabled.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aKeyRef Reference to the Thread Network Key.
Return values
OT_ERROR_NONE Successfully set the Thread Network Key.
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otThreadGetNetworkKeyRef

◆ otThreadSetNetworkName()

otError otThreadSetNetworkName ( otInstance * aInstance,
const char * aNetworkName
)

Set the Thread Network Name.

This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aNetworkName A pointer to the Thread Network Name.
Return values
OT_ERROR_NONE Successfully set the Thread Network Name.
OT_ERROR_INVALID_STATE Thread protocols are enabled.
See also
otThreadGetNetworkName