otRadioIeInfo Struct Reference

This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame.

#include < include/openthread/platform/radio.h >

Public Attributes

int64_t mNetworkTimeOffset
The time offset to the Thread network time.
uint8_t mTimeIeOffset
The Time IE offset from the start of PSDU.
uint8_t mTimeSyncSeq
The Time sync sequence.

This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame.


The documentation for this struct was generated from the following file:
  • include/openthread/platform/ radio.h