otSecurityPolicy Struct Reference
This structure represent Security Policy.
#include <
include/openthread/dataset.h
>
Public Attributes |
|
uint16_t | mRotationTime |
The value for thrKeyRotation in units of hours.
|
|
bool | mObtainNetworkKeyEnabled : 1 |
Obtaining the Network Key for out-of-band commissioning is enabled.
|
|
bool | mNativeCommissioningEnabled : 1 |
Native Commissioning using PSKc is allowed.
|
|
bool | mRoutersEnabled : 1 |
Thread 1.0/1.1.x Routers are enabled.
|
|
bool | mExternalCommissioningEnabled : 1 |
External Commissioner authentication is allowed.
|
|
bool | mBeaconsEnabled : 1 |
Thread 1.0/1.1.x Beacons are enabled.
|
|
bool | mCommercialCommissioningEnabled : 1 |
Commercial Commissioning is enabled.
|
|
bool | mAutonomousEnrollmentEnabled : 1 |
Autonomous Enrollment is enabled.
|
|
bool | mNetworkKeyProvisioningEnabled : 1 |
Network Key Provisioning is enabled.
|
|
bool | mTobleLinkEnabled : 1 |
ToBLE link is enabled.
|
|
bool | mNonCcmRoutersEnabled : 1 |
Non-CCM Routers enabled.
|
|
uint8_t | mVersionThresholdForRouting : 3 |
Version-threshold for Routing.
|
This structure represent Security Policy.
The documentation for this struct was generated from the following file:
-
include/openthread/
dataset.h