This module includes functions for signal jamming detection feature.
Typedefs | |
typedef void(* | otJamDetectionCallback) (bool aJamState, void *aContext) |
This function pointer is called if signal jam detection is enabled and a jam is detected. |
Functions | |
otError | otJamDetectionSetRssiThreshold (otInstance *aInstance, int8_t aRssiThreshold) |
Set the Jam Detection RSSI Threshold (in dBm). | |
int8_t | otJamDetectionGetRssiThreshold (otInstance *aInstance) |
Get the Jam Detection RSSI Threshold (in dBm). | |
otError | otJamDetectionSetWindow (otInstance *aInstance, uint8_t aWindow) |
Set the Jam Detection Detection Window (in seconds). | |
uint8_t | otJamDetectionGetWindow (otInstance *aInstance) |
Get the Jam Detection Detection Window (in seconds). | |
otError | otJamDetectionSetBusyPeriod (otInstance *aInstance, uint8_t aBusyPeriod) |
Set the Jam Detection Busy Period (in seconds). | |
uint8_t | otJamDetectionGetBusyPeriod (otInstance *aInstance) |
Get the Jam Detection Busy Period (in seconds) | |
otError | otJamDetectionStart (otInstance *aInstance, otJamDetectionCallback aCallback, void *aContext) |
Start the jamming detection. | |
otError | otJamDetectionStop (otInstance *aInstance) |
Stop the jamming detection. | |
bool | otJamDetectionIsEnabled (otInstance *aInstance) |
Get the Jam Detection Status (enabled/disabled) | |
bool | otJamDetectionGetState (otInstance *aInstance) |
Get the Jam Detection State. | |
uint64_t | otJamDetectionGetHistoryBitmap (otInstance *aInstance) |
Get the current history bitmap. |
Detailed Description
This module includes functions for signal jamming detection feature.
The functions in this module are available when jam-detection feature (OPENTHREAD_CONFIG_JAM_DETECTION_ENABLE
) is enabled.
Typedef Documentation
◆ otJamDetectionCallback
typedef void(* otJamDetectionCallback) (bool aJamState, void *aContext) |
This function pointer is called if signal jam detection is enabled and a jam is detected.
- Parameters
-
[in] aJamState
Current jam state ( true
if jam is detected,false
otherwise).[in] aContext
A pointer to application-specific context.
Function Documentation
◆ otJamDetectionGetBusyPeriod()
uint8_t otJamDetectionGetBusyPeriod | ( | otInstance * | aInstance | ) |
Get the Jam Detection Busy Period (in seconds)
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Jam Detection Busy Period.
◆ otJamDetectionGetHistoryBitmap()
uint64_t otJamDetectionGetHistoryBitmap | ( | otInstance * | aInstance | ) |
Get the current history bitmap.
This value provides information about current state of jamming detection module for monitoring/debugging purpose. It returns a 64-bit value where each bit corresponds to one second interval starting with bit 0 for the most recent interval and bit 63 for the oldest intervals (63 sec earlier). The bit is set to 1 if the jamming detection module observed/detected high signal level during the corresponding one second interval.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The current history bitmap.
◆ otJamDetectionGetRssiThreshold()
int8_t otJamDetectionGetRssiThreshold | ( | otInstance * | aInstance | ) |
Get the Jam Detection RSSI Threshold (in dBm).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Jam Detection RSSI Threshold.
◆ otJamDetectionGetState()
bool otJamDetectionGetState | ( | otInstance * | aInstance | ) |
Get the Jam Detection State.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Jam Detection state (
true
jam is detected, `false' otherwise).
◆ otJamDetectionGetWindow()
uint8_t otJamDetectionGetWindow | ( | otInstance * | aInstance | ) |
Get the Jam Detection Detection Window (in seconds).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Jam Detection Window.
◆ otJamDetectionIsEnabled()
bool otJamDetectionIsEnabled | ( | otInstance * | aInstance | ) |
Get the Jam Detection Status (enabled/disabled)
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Returns
- The Jam Detection status (true if enabled, false otherwise).
◆ otJamDetectionSetBusyPeriod()
otError otJamDetectionSetBusyPeriod | ( | otInstance * | aInstance, |
uint8_t | aBusyPeriod |
||
) |
Set the Jam Detection Busy Period (in seconds).
The number of aggregate seconds within the detection window where the RSSI must be above threshold to trigger detection.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aBusyPeriod
The Jam Detection busy period (should be non-zero and less than or equal to Jam Detection Window)
- Return values
-
OT_ERROR_NONE
Successfully set the window. OT_ERROR_INVALID_ARGS
The given input is not within the valid range.
◆ otJamDetectionSetRssiThreshold()
otError otJamDetectionSetRssiThreshold | ( | otInstance * | aInstance, |
int8_t | aRssiThreshold |
||
) |
Set the Jam Detection RSSI Threshold (in dBm).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aRssiThreshold
The RSSI threshold.
- Return values
-
OT_ERROR_NONE
Successfully set the threshold.
◆ otJamDetectionSetWindow()
otError otJamDetectionSetWindow | ( | otInstance * | aInstance, |
uint8_t | aWindow |
||
) |
Set the Jam Detection Detection Window (in seconds).
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aWindow
The Jam Detection window (valid range is 1 to 63)
- Return values
-
OT_ERROR_NONE
Successfully set the window. OT_ERROR_INVALID_ARGS
The given input parameter not within valid range (1-63)
◆ otJamDetectionStart()
otError otJamDetectionStart | ( | otInstance * | aInstance, |
otJamDetectionCallback | aCallback, |
||
void * | aContext |
||
) |
Start the jamming detection.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aCallback
A pointer to a function called to notify of jamming state change. [in] aContext
A pointer to application-specific context.
- Return values
-
OT_ERROR_NONE
Successfully started the jamming detection. OT_ERROR_ALREADY
Jam detection has been started before.
◆ otJamDetectionStop()
otError otJamDetectionStop | ( | otInstance * | aInstance | ) |
Stop the jamming detection.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance.
- Return values
-
OT_ERROR_NONE
Successfully stopped the jamming detection. OT_ERROR_ALREADY
Jam detection is already stopped.