otNetworkName Struct Reference
This structure represents a Network Name.
#include <
include/openthread/dataset.h
>
Public Attributes | |
char | m8 [OT_NETWORK_NAME_MAX_SIZE+1] |
Byte values. The + 1 is for null char. |
This structure represents a Network Name.
The otNetworkName
is a null terminated C string (i.e., m8
char array MUST end with null char \0
).
The documentation for this struct was generated from the following file:
- include/openthread/
dataset.h