This structure represents a Network Diagnostic Connectivity value.
#include <
include/openthread/netdiag.h
>
Public Attributes | |
int8_t | mParentPriority |
The priority of the sender as a parent. | |
uint8_t | mLinkQuality3 |
The number of neighboring devices with which the sender shares a link of quality 3. | |
uint8_t | mLinkQuality2 |
The number of neighboring devices with which the sender shares a link of quality 2. | |
uint8_t | mLinkQuality1 |
The number of neighboring devices with which the sender shares a link of quality 1. | |
uint8_t | mLeaderCost |
The sender's routing cost to the Leader. | |
uint8_t | mIdSequence |
The most recent ID sequence number received by the sender. | |
uint8_t | mActiveRouters |
The number of active Routers in the sender's Thread Network Partition. | |
uint16_t | mSedBufferSize |
The guaranteed buffer capacity in octets for all IPv6 datagrams destined to a given SED. | |
uint8_t | mSedDatagramCount |
The guaranteed queue capacity in number of IPv6 datagrams destined to a given SED. |
This structure represents a Network Diagnostic Connectivity value.
Member Data Documentation
◆ mSedBufferSize
uint16_t otNetworkDiagConnectivity::mSedBufferSize |
The guaranteed buffer capacity in octets for all IPv6 datagrams destined to a given SED.
Optional.
◆ mSedDatagramCount
uint8_t otNetworkDiagConnectivity::mSedDatagramCount |
The guaranteed queue capacity in number of IPv6 datagrams destined to a given SED.
Optional.
The documentation for this struct was generated from the following file:
- include/openthread/
netdiag.h