Types
This module includes the platform abstraction for a radio frame.
Classes | |
struct | otExtAddress |
This structure represents the IEEE 802.15.4 Extended Address. | |
struct | otMacKey |
This structure represents a MAC Key. | |
struct | otMacKeyMaterial |
This structure represents a MAC Key. | |
struct | otRadioIeInfo |
This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame. | |
struct | otRadioFrame |
This structure represents an IEEE 802.15.4 radio frame. | |
struct | otRadioCoexMetrics |
The following are valid radio state transitions: | |
struct | otLinkMetrics |
This structure represents what metrics are specified to query. |
Macros | |
#define | OT_PANID_BROADCAST 0xffff |
IEEE 802.15.4 Broadcast PAN ID. | |
#define | OT_EXT_ADDRESS_SIZE 8 |
Size of an IEEE 802.15.4 Extended Address (bytes) | |
#define | CSL_IE_HEADER_BYTES_LO 0x04 |
Fixed CSL IE header first byte. | |
#define | CSL_IE_HEADER_BYTES_HI 0x0d |
Fixed CSL IE header second byte. | |
#define | OT_MAC_KEY_SIZE 16 |
Size of the MAC Key in bytes. | |
#define | OT_TOOL_PACKED_END |
Compiler-specific indication at the end of a byte packed class or struct. |
Typedefs | |
typedef uint8_t | otRadioCaps |
This type represents radio capabilities. | |
typedef uint16_t | otPanId |
This type represents the IEEE 802.15.4 PAN ID. | |
typedef uint16_t | otShortAddress |
This type represents the IEEE 802.15.4 Short Address. | |
typedef struct otExtAddress | otExtAddress |
This structure represents the IEEE 802.15.4 Extended Address. | |
typedef struct otMacKey | otMacKey |
This structure represents a MAC Key. | |
typedef otCryptoKeyRef | otMacKeyRef |
This type represents a MAC Key Ref used by PSA. | |
typedef struct otMacKeyMaterial | otMacKeyMaterial |
typedef struct otRadioIeInfo | otRadioIeInfo |
This structure represents the IEEE 802.15.4 Header IE (Information Element) related information of a radio frame. | |
typedef struct otRadioFrame | otRadioFrame |
This structure represents an IEEE 802.15.4 radio frame. | |
typedef enum otRadioState | otRadioState |
This structure represents the state of a radio. | |
typedef struct otRadioCoexMetrics | otRadioCoexMetrics |
The following are valid radio state transitions: | |
typedef struct otLinkMetrics | otLinkMetrics |
This structure represents what metrics are specified to query. |
Enumerations | |
enum | { OT_RADIO_FRAME_MAX_SIZE = 127, OT_RADIO_FRAME_MIN_SIZE = 3, OT_RADIO_SYMBOLS_PER_OCTET = 2, OT_RADIO_BIT_RATE = 250000, OT_RADIO_BITS_PER_OCTET = 8, OT_RADIO_SYMBOL_TIME = ((OT_RADIO_BITS_PER_OCTET / OT_RADIO_SYMBOLS_PER_OCTET) * 1000000) / OT_RADIO_BIT_RATE, OT_RADIO_LQI_NONE = 0, OT_RADIO_RSSI_INVALID = 127, OT_RADIO_POWER_INVALID = 127 } |
enum | { OT_RADIO_CHANNEL_PAGE_0 = 0, OT_RADIO_CHANNEL_PAGE_0_MASK = (1U << OT_RADIO_CHANNEL_PAGE_0), OT_RADIO_CHANNEL_PAGE_2 = 2, OT_RADIO_CHANNEL_PAGE_2_MASK = (1U << OT_RADIO_CHANNEL_PAGE_2) } |
This enumeration defines the channel page. | |
enum | { OT_RADIO_915MHZ_OQPSK_CHANNEL_MIN = 1, OT_RADIO_915MHZ_OQPSK_CHANNEL_MAX = 10, OT_RADIO_915MHZ_OQPSK_CHANNEL_MASK = 0x3ff << OT_RADIO_915MHZ_OQPSK_CHANNEL_MIN, OT_RADIO_2P4GHZ_OQPSK_CHANNEL_MIN = 11, OT_RADIO_2P4GHZ_OQPSK_CHANNEL_MAX = 26, OT_RADIO_2P4GHZ_OQPSK_CHANNEL_MASK = 0xffff << OT_RADIO_2P4GHZ_OQPSK_CHANNEL_MIN } |
This enumeration defines the frequency band channel range. | |
enum | { OT_RADIO_CAPS_NONE = 0, OT_RADIO_CAPS_ACK_TIMEOUT = 1 << 0, OT_RADIO_CAPS_ENERGY_SCAN = 1 << 1, OT_RADIO_CAPS_TRANSMIT_RETRIES = 1 << 2, OT_RADIO_CAPS_CSMA_BACKOFF = 1 << 3, OT_RADIO_CAPS_SLEEP_TO_TX = 1 << 4, OT_RADIO_CAPS_TRANSMIT_SEC = 1 << 5, OT_RADIO_CAPS_TRANSMIT_TIMING = 1 << 6, OT_RADIO_CAPS_RECEIVE_TIMING = 1 << 7 } |
This enumeration defines constants that are used to indicate different radio capabilities. | |
enum | { OT_IE_HEADER_SIZE = 2, OT_CSL_IE_SIZE = 4, OT_ACK_IE_MAX_SIZE = 16, OT_ENH_PROBING_IE_DATA_MAX_SIZE = 2 } |
This enumeration defines constants about size of header IE in ACK. | |
enum | otRadioKeyType { OT_KEY_TYPE_LITERAL_KEY = 0, OT_KEY_TYPE_KEY_REF = 1 } |
This enumeration defines constants about key types. | |
enum | otRadioState { OT_RADIO_STATE_DISABLED = 0, OT_RADIO_STATE_SLEEP = 1, OT_RADIO_STATE_RECEIVE = 2, OT_RADIO_STATE_TRANSMIT = 3, OT_RADIO_STATE_INVALID = 255 } |
This structure represents the state of a radio. |
Variables | |
OT_TOOL_PACKED_BEGIN struct otExtAddress | OT_TOOL_PACKED_END |
Detailed Description
This module includes the platform abstraction for a radio frame.
Typedef Documentation
◆ otRadioCaps
typedef uint8_t otRadioCaps |
This type represents radio capabilities.
The value is a bit-field indicating the capabilities supported by the radio. See OT_RADIO_CAPS_*
definitions.
◆ otRadioCoexMetrics
typedef struct otRadioCoexMetrics otRadioCoexMetrics |
The following are valid radio state transitions:
(Radio ON) +----——+ Enable() +-——+ Receive() +---——+ Transmit() +----——+ | |-----——>| |-----——>| |--------——>| | | Disabled | | Sleep | | Receive | | Transmit | | |<-----——| |<-----——| |<--------——| | +----——+ Disable() +-——+ Sleep() +---——+ Receive() +----——+ (Radio OFF) or signal TransmitDone
During the IEEE 802.15.4 data request command the transition Sleep->Receive->Transmit can be shortened to direct transition from Sleep to Transmit if the platform supports the OT_RADIO_CAPS_SLEEP_TO_TX capability. This structure represents radio coexistence metrics.
◆ otRadioState
typedef enum otRadioState otRadioState |
This structure represents the state of a radio.
Initially, a radio is in the Disabled state.
Enumeration Type Documentation
◆ anonymous enum
anonymous enum |
◆ anonymous enum
anonymous enum |
◆ anonymous enum
anonymous enum |
This enumeration defines the frequency band channel range.
◆ anonymous enum
anonymous enum |
This enumeration defines constants that are used to indicate different radio capabilities.
See otRadioCaps
.
◆ anonymous enum
anonymous enum |
This enumeration defines constants about size of header IE in ACK.
◆ otRadioKeyType
enum otRadioKeyType |
◆ otRadioState
enum otRadioState |
This structure represents the state of a radio.
Initially, a radio is in the Disabled state.