This structure represents the message buffer information.
#include <
include/openthread/message.h
>
Public Attributes | |
uint16_t | mTotalBuffers |
The number of buffers in the pool. | |
uint16_t | mFreeBuffers |
The number of free message buffers. | |
uint16_t | m6loSendMessages |
The number of messages in the 6lo send queue. | |
uint16_t | m6loSendBuffers |
The number of buffers in the 6lo send queue. | |
uint16_t | m6loReassemblyMessages |
The number of messages in the 6LoWPAN reassembly queue. | |
uint16_t | m6loReassemblyBuffers |
The number of buffers in the 6LoWPAN reassembly queue. | |
uint16_t | mIp6Messages |
The number of messages in the IPv6 send queue. | |
uint16_t | mIp6Buffers |
The number of buffers in the IPv6 send queue. | |
uint16_t | mMplMessages |
The number of messages in the MPL send queue. | |
uint16_t | mMplBuffers |
The number of buffers in the MPL send queue. | |
uint16_t | mMleMessages |
The number of messages in the MLE send queue. | |
uint16_t | mMleBuffers |
The number of buffers in the MLE send queue. | |
uint16_t | mArpMessages |
The number of messages in the ARP send queue. | |
uint16_t | mArpBuffers |
The number of buffers in the ARP send queue. | |
uint16_t | mCoapMessages |
The number of messages in the CoAP send queue. | |
uint16_t | mCoapBuffers |
The number of buffers in the CoAP send queue. | |
uint16_t | mCoapSecureMessages |
The number of messages in the CoAP secure send queue. | |
uint16_t | mCoapSecureBuffers |
The number of buffers in the CoAP secure send queue. | |
uint16_t | mApplicationCoapMessages |
The number of messages in the application CoAP send queue. | |
uint16_t | mApplicationCoapBuffers |
The number of buffers in the application CoAP send queue. |
This structure represents the message buffer information.
The documentation for this struct was generated from the following file:
- include/openthread/
message.h