Operational Dataset

This module includes functions for Dataset Updater.

Classes

struct otNetworkKey
This structure represents a Thread Network Key.
struct otNetworkName
This structure represents a Network Name.
struct otExtendedPanId
This structure represents an Extended PAN ID.
struct otPskc
This structure represents PSKc.
struct otSecurityPolicy
This structure represent Security Policy.
struct otOperationalDatasetComponents
This structure represents presence of different components in Active or Pending Operational Dataset.
struct otOperationalDataset
This structure represents an Active or Pending Operational Dataset.
struct otOperationalDatasetTlvs
This structure represents an Active or Pending Operational Dataset.

Macros

#define OT_NETWORK_KEY_SIZE 16
Size of the Thread Network Key (bytes)
#define OT_NETWORK_NAME_MAX_SIZE 16
Maximum size of the Thread Network Name field (bytes)
#define OT_EXT_PAN_ID_SIZE 8
Size of a Thread PAN ID (bytes)
#define OT_MESH_LOCAL_PREFIX_SIZE OT_IP6_PREFIX_SIZE
Size of the Mesh Local Prefix (bytes)
#define OT_PSKC_MAX_SIZE 16
Maximum size of the PSKc (bytes)
#define OT_CHANNEL_1_MASK (1 << 1)
Channel 1.
#define OT_CHANNEL_2_MASK (1 << 2)
Channel 2.
#define OT_CHANNEL_3_MASK (1 << 3)
Channel 3.
#define OT_CHANNEL_4_MASK (1 << 4)
Channel 4.
#define OT_CHANNEL_5_MASK (1 << 5)
Channel 5.
#define OT_CHANNEL_6_MASK (1 << 6)
Channel 6.
#define OT_CHANNEL_7_MASK (1 << 7)
Channel 7.
#define OT_CHANNEL_8_MASK (1 << 8)
Channel 8.
#define OT_CHANNEL_9_MASK (1 << 9)
Channel 9.
#define OT_CHANNEL_10_MASK (1 << 10)
Channel 10.
#define OT_CHANNEL_11_MASK (1 << 11)
Channel 11.
#define OT_CHANNEL_12_MASK (1 << 12)
Channel 12.
#define OT_CHANNEL_13_MASK (1 << 13)
Channel 13.
#define OT_CHANNEL_14_MASK (1 << 14)
Channel 14.
#define OT_CHANNEL_15_MASK (1 << 15)
Channel 15.
#define OT_CHANNEL_16_MASK (1 << 16)
Channel 16.
#define OT_CHANNEL_17_MASK (1 << 17)
Channel 17.
#define OT_CHANNEL_18_MASK (1 << 18)
Channel 18.
#define OT_CHANNEL_19_MASK (1 << 19)
Channel 19.
#define OT_CHANNEL_20_MASK (1 << 20)
Channel 20.
#define OT_CHANNEL_21_MASK (1 << 21)
Channel 21.
#define OT_CHANNEL_22_MASK (1 << 22)
Channel 22.
#define OT_CHANNEL_23_MASK (1 << 23)
Channel 23.
#define OT_CHANNEL_24_MASK (1 << 24)
Channel 24.
#define OT_CHANNEL_25_MASK (1 << 25)
Channel 25.
#define OT_CHANNEL_26_MASK (1 << 26)
Channel 26.
#define OT_OPERATIONAL_DATASET_MAX_LENGTH 254
Maximum length of Operational Dataset in bytes.

Typedefs

typedef struct otNetworkKey otNetworkKey
This structure represents a Thread Network Key.
typedef otCryptoKeyRef otNetworkKeyRef
This datatype represents KeyRef to NetworkKey.
typedef struct otNetworkName otNetworkName
This structure represents a Network Name.
typedef struct otExtendedPanId otExtendedPanId
This structure represents an Extended PAN ID.
typedef otIp6NetworkPrefix otMeshLocalPrefix
This structure represents a Mesh Local Prefix.
typedef struct otPskc otPskc
This structure represents a PSKc.
typedef otCryptoKeyRef otPskcRef
This datatype represents KeyRef to PSKc.
typedef struct otSecurityPolicy otSecurityPolicy
This structure represent Security Policy.
typedef uint32_t otChannelMask
This type represents Channel Mask.
typedef struct otOperationalDatasetComponents otOperationalDatasetComponents
This structure represents presence of different components in Active or Pending Operational Dataset.
typedef struct otOperationalDataset otOperationalDataset
This structure represents an Active or Pending Operational Dataset.
typedef struct otOperationalDatasetTlvs otOperationalDatasetTlvs
This structure represents an Active or Pending Operational Dataset.
typedef enum otMeshcopTlvType otMeshcopTlvType
This enumeration represents meshcop TLV types.
typedef void(* otDatasetMgmtSetCallback ) ( otError aResult, void *aContext)
This function pointer is called when a response to a MGMT_SET request is received or times out.
typedef void(* otDatasetUpdaterCallback ) ( otError aError, void *aContext)
This callback function pointer is called when a Dataset update request finishes, reporting success or failure status of the Dataset update request.

Enumerations

enum otMeshcopTlvType {
OT_MESHCOP_TLV_CHANNEL = 0,
OT_MESHCOP_TLV_PANID = 1,
OT_MESHCOP_TLV_EXTPANID = 2,
OT_MESHCOP_TLV_NETWORKNAME = 3,
OT_MESHCOP_TLV_PSKC = 4,
OT_MESHCOP_TLV_NETWORKKEY = 5,
OT_MESHCOP_TLV_NETWORK_KEY_SEQUENCE = 6,
OT_MESHCOP_TLV_MESHLOCALPREFIX = 7,
OT_MESHCOP_TLV_STEERING_DATA = 8,
OT_MESHCOP_TLV_BORDER_AGENT_RLOC = 9,
OT_MESHCOP_TLV_COMMISSIONER_ID = 10,
OT_MESHCOP_TLV_COMM_SESSION_ID = 11,
OT_MESHCOP_TLV_SECURITYPOLICY = 12,
OT_MESHCOP_TLV_GET = 13,
OT_MESHCOP_TLV_ACTIVETIMESTAMP = 14,
OT_MESHCOP_TLV_COMMISSIONER_UDP_PORT = 15,
OT_MESHCOP_TLV_STATE = 16,
OT_MESHCOP_TLV_JOINER_DTLS = 17,
OT_MESHCOP_TLV_JOINER_UDP_PORT = 18,
OT_MESHCOP_TLV_JOINER_IID = 19,
OT_MESHCOP_TLV_JOINER_RLOC = 20,
OT_MESHCOP_TLV_JOINER_ROUTER_KEK = 21,
OT_MESHCOP_TLV_PROVISIONING_URL = 32,
OT_MESHCOP_TLV_VENDOR_NAME_TLV = 33,
OT_MESHCOP_TLV_VENDOR_MODEL_TLV = 34,
OT_MESHCOP_TLV_VENDOR_SW_VERSION_TLV = 35,
OT_MESHCOP_TLV_VENDOR_DATA_TLV = 36,
OT_MESHCOP_TLV_VENDOR_STACK_VERSION_TLV = 37,
OT_MESHCOP_TLV_UDP_ENCAPSULATION_TLV = 48,
OT_MESHCOP_TLV_IPV6_ADDRESS_TLV = 49,
OT_MESHCOP_TLV_PENDINGTIMESTAMP = 51,
OT_MESHCOP_TLV_DELAYTIMER = 52,
OT_MESHCOP_TLV_CHANNELMASK = 53,
OT_MESHCOP_TLV_COUNT = 54,
OT_MESHCOP_TLV_PERIOD = 55,
OT_MESHCOP_TLV_SCAN_DURATION = 56,
OT_MESHCOP_TLV_ENERGY_LIST = 57,
OT_MESHCOP_TLV_DISCOVERYREQUEST = 128,
OT_MESHCOP_TLV_DISCOVERYRESPONSE = 129,
OT_MESHCOP_TLV_JOINERADVERTISEMENT = 241
}
This enumeration represents meshcop TLV types.

Functions

bool otDatasetIsCommissioned ( otInstance *aInstance)
This function indicates whether a valid network is present in the Active Operational Dataset or not.
otError otDatasetGetActive ( otInstance *aInstance, otOperationalDataset *aDataset)
This function gets the Active Operational Dataset.
otError otDatasetGetActiveTlvs ( otInstance *aInstance, otOperationalDatasetTlvs *aDataset)
This function gets the Active Operational Dataset.
otError otDatasetSetActive ( otInstance *aInstance, const otOperationalDataset *aDataset)
This function sets the Active Operational Dataset.
otError otDatasetSetActiveTlvs ( otInstance *aInstance, const otOperationalDatasetTlvs *aDataset)
This function sets the Active Operational Dataset.
otError otDatasetGetPending ( otInstance *aInstance, otOperationalDataset *aDataset)
This function gets the Pending Operational Dataset.
otError otDatasetGetPendingTlvs ( otInstance *aInstance, otOperationalDatasetTlvs *aDataset)
This function gets the Pending Operational Dataset.
otError otDatasetSetPending ( otInstance *aInstance, const otOperationalDataset *aDataset)
This function sets the Pending Operational Dataset.
otError otDatasetSetPendingTlvs ( otInstance *aInstance, const otOperationalDatasetTlvs *aDataset)
This function sets the Pending Operational Dataset.
otError otDatasetSendMgmtActiveGet ( otInstance *aInstance, const otOperationalDatasetComponents *aDatasetComponents, const uint8_t *aTlvTypes, uint8_t aLength, const otIp6Address *aAddress)
This function sends MGMT_ACTIVE_GET.
otError otDatasetSendMgmtActiveSet ( otInstance *aInstance, const otOperationalDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength, otDatasetMgmtSetCallback aCallback, void *aContext)
This function sends MGMT_ACTIVE_SET.
otError otDatasetSendMgmtPendingGet ( otInstance *aInstance, const otOperationalDatasetComponents *aDatasetComponents, const uint8_t *aTlvTypes, uint8_t aLength, const otIp6Address *aAddress)
This function sends MGMT_PENDING_GET.
otError otDatasetSendMgmtPendingSet ( otInstance *aInstance, const otOperationalDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength, otDatasetMgmtSetCallback aCallback, void *aContext)
This function sends MGMT_PENDING_SET.
otError otDatasetGeneratePskc (const char *aPassPhrase, const otNetworkName *aNetworkName, const otExtendedPanId *aExtPanId, otPskc *aPskc)
This function generates PSKc from a given pass-phrase, network name, and extended PAN ID.
otError otNetworkNameFromString ( otNetworkName *aNetworkName, const char *aNameString)
This function sets an otNetworkName instance from a given null terminated C string.
otError otDatasetParseTlvs (const otOperationalDatasetTlvs *aDatasetTlvs, otOperationalDataset *aDataset)
This function parses an Operational Dataset from a otOperationalDatasetTlvs .
otError otDatasetCreateNewNetwork ( otInstance *aInstance, otOperationalDataset *aDataset)
This method creates a new Operational Dataset to use when forming a new network.
uint32_t otDatasetGetDelayTimerMinimal ( otInstance *aInstance)
Get minimal delay timer.
otError otDatasetSetDelayTimerMinimal ( otInstance *aInstance, uint32_t aDelayTimerMinimal)
Set minimal delay timer.
otError otDatasetUpdaterRequestUpdate ( otInstance *aInstance, const otOperationalDataset *aDataset, otDatasetUpdaterCallback aCallback, void *aContext)
This function requests an update to Operational Dataset.
void otDatasetUpdaterCancelUpdate ( otInstance *aInstance)
This function cancels an ongoing (if any) Operational Dataset update request.
bool otDatasetUpdaterIsUpdateOngoing ( otInstance *aInstance)
This function indicates whether there is an ongoing Operation Dataset update request.

Variables

OT_TOOL_PACKED_BEGIN struct otNetworkKey OT_TOOL_PACKED_END

Detailed Description

This module includes functions for Dataset Updater.

The functions in this module are available when Dataset Updater feature is enabled (i.e. OPENTHREAD_CONFIG_DATASET_UPDATER_ENABLE is set to 1). Further this feature is available only on an FTD build.

Typedef Documentation

◆ otDatasetMgmtSetCallback

typedef void(* otDatasetMgmtSetCallback) ( otError aResult, void *aContext)

This function pointer is called when a response to a MGMT_SET request is received or times out.

Parameters
[in] aResult A result of the operation.
[in] aContext A pointer to application-specific context.
Return values
OT_ERROR_NONE The request was accepted by the leader.
OT_ERROR_REJECTED The request was rejected by the leader.
OT_ERROR_PARSE An error occurred during parsing the response.
OT_ERROR_ABORT The request was reset by peer.
OT_ERROR_RESPONSE_TIMEOUT No response or acknowledgment received during timeout period.

◆ otDatasetUpdaterCallback

typedef void(* otDatasetUpdaterCallback) ( otError aError, void *aContext)

This callback function pointer is called when a Dataset update request finishes, reporting success or failure status of the Dataset update request.

Parameters
[in] aError The error status. OT_ERROR_NONE indicates successful Dataset update. OT_ERROR_INVALID_STATE indicates failure due invalid state (MLE being disabled). OT_ERROR_ALREADY indicates failure due to another device within network requesting a conflicting Dataset update.
[in] aContext A pointer to the arbitrary context (provided by user in otDatasetUpdaterRequestUpdate() ).

◆ otNetworkKeyRef

This datatype represents KeyRef to NetworkKey.

Reference to Key

◆ otNetworkName

This structure represents a Network Name.

The otNetworkName is a null terminated C string (i.e., m8 char array MUST end with null char \0 ).

◆ otOperationalDataset

This structure represents an Active or Pending Operational Dataset.

Components in Dataset are optional. mComponets structure specifies which components are present in the Dataset.

◆ otOperationalDatasetTlvs

This structure represents an Active or Pending Operational Dataset.

The Operational Dataset is TLV encoded as specified by Thread.

◆ otPskcRef

This datatype represents KeyRef to PSKc.

Reference to Key

Enumeration Type Documentation

◆ otMeshcopTlvType

This enumeration represents meshcop TLV types.

Enumerator
OT_MESHCOP_TLV_CHANNEL

meshcop Channel TLV

OT_MESHCOP_TLV_PANID

meshcop Pan Id TLV

OT_MESHCOP_TLV_EXTPANID

meshcop Extended Pan Id TLV

OT_MESHCOP_TLV_NETWORKNAME

meshcop Network Name TLV

OT_MESHCOP_TLV_PSKC

meshcop PSKc TLV

OT_MESHCOP_TLV_NETWORKKEY

meshcop Network Key TLV

OT_MESHCOP_TLV_NETWORK_KEY_SEQUENCE

meshcop Network Key Sequence TLV

OT_MESHCOP_TLV_MESHLOCALPREFIX

meshcop Mesh Local Prefix TLV

OT_MESHCOP_TLV_STEERING_DATA

meshcop Steering Data TLV

OT_MESHCOP_TLV_BORDER_AGENT_RLOC

meshcop Border Agent Locator TLV

OT_MESHCOP_TLV_COMMISSIONER_ID

meshcop Commissioner ID TLV

OT_MESHCOP_TLV_COMM_SESSION_ID

meshcop Commissioner Session ID TLV

OT_MESHCOP_TLV_SECURITYPOLICY

meshcop Security Policy TLV

OT_MESHCOP_TLV_GET

meshcop Get TLV

OT_MESHCOP_TLV_ACTIVETIMESTAMP

meshcop Active Timestamp TLV

OT_MESHCOP_TLV_COMMISSIONER_UDP_PORT

meshcop Commissioner UDP Port TLV

OT_MESHCOP_TLV_STATE

meshcop State TLV

OT_MESHCOP_TLV_JOINER_DTLS

meshcop Joiner DTLS Encapsulation TLV

OT_MESHCOP_TLV_JOINER_UDP_PORT

meshcop Joiner UDP Port TLV

OT_MESHCOP_TLV_JOINER_IID

meshcop Joiner IID TLV

OT_MESHCOP_TLV_JOINER_RLOC

meshcop Joiner Router Locator TLV

OT_MESHCOP_TLV_JOINER_ROUTER_KEK

meshcop Joiner Router KEK TLV

OT_MESHCOP_TLV_PROVISIONING_URL

meshcop Provisioning URL TLV

OT_MESHCOP_TLV_VENDOR_NAME_TLV

meshcop Vendor Name TLV

OT_MESHCOP_TLV_VENDOR_MODEL_TLV

meshcop Vendor Model TLV

OT_MESHCOP_TLV_VENDOR_SW_VERSION_TLV

meshcop Vendor SW Version TLV

OT_MESHCOP_TLV_VENDOR_DATA_TLV

meshcop Vendor Data TLV

OT_MESHCOP_TLV_VENDOR_STACK_VERSION_TLV

meshcop Vendor Stack Version TLV

OT_MESHCOP_TLV_UDP_ENCAPSULATION_TLV

meshcop UDP encapsulation TLV

OT_MESHCOP_TLV_IPV6_ADDRESS_TLV

meshcop IPv6 address TLV

OT_MESHCOP_TLV_PENDINGTIMESTAMP

meshcop Pending Timestamp TLV

OT_MESHCOP_TLV_DELAYTIMER

meshcop Delay Timer TLV

OT_MESHCOP_TLV_CHANNELMASK

meshcop Channel Mask TLV

OT_MESHCOP_TLV_COUNT

meshcop Count TLV

OT_MESHCOP_TLV_PERIOD

meshcop Period TLV

OT_MESHCOP_TLV_SCAN_DURATION

meshcop Scan Duration TLV

OT_MESHCOP_TLV_ENERGY_LIST

meshcop Energy List TLV

OT_MESHCOP_TLV_DISCOVERYREQUEST

meshcop Discovery Request TLV

OT_MESHCOP_TLV_DISCOVERYRESPONSE

meshcop Discovery Response TLV

OT_MESHCOP_TLV_JOINERADVERTISEMENT

meshcop Joiner Advertisement TLV

Function Documentation

◆ otDatasetCreateNewNetwork()

otError otDatasetCreateNewNetwork ( otInstance * aInstance,
otOperationalDataset * aDataset
)

This method creates a new Operational Dataset to use when forming a new network.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aDataset The Operational Dataset.
Return values
OT_ERROR_NONE Successfully created a new Operational Dataset.
OT_ERROR_FAILED Failed to generate random values for new parameters.

◆ otDatasetGeneratePskc()

otError otDatasetGeneratePskc ( const char * aPassPhrase,
const otNetworkName * aNetworkName,
const otExtendedPanId * aExtPanId,
otPskc * aPskc
)

This function generates PSKc from a given pass-phrase, network name, and extended PAN ID.

PSKc is used to establish the Commissioner Session.

Parameters
[in] aPassPhrase The commissioning pass-phrase.
[in] aNetworkName The network name for PSKc computation.
[in] aExtPanId The extended PAN ID for PSKc computation.
[out] aPskc A pointer to variable to output the generated PSKc.
Return values
OT_ERROR_NONE Successfully generate PSKc.
OT_ERROR_INVALID_ARGS If any of the input arguments is invalid.

◆ otDatasetGetActive()

otError otDatasetGetActive ( otInstance * aInstance,
otOperationalDataset * aDataset
)

This function gets the Active Operational Dataset.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aDataset A pointer to where the Active Operational Dataset will be placed.
Return values
OT_ERROR_NONE Successfully retrieved the Active Operational Dataset.
OT_ERROR_NOT_FOUND No corresponding value in the setting store.

◆ otDatasetGetActiveTlvs()

otError otDatasetGetActiveTlvs ( otInstance * aInstance,
otOperationalDatasetTlvs * aDataset
)

This function gets the Active Operational Dataset.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aDataset A pointer to where the Active Operational Dataset will be placed.
Return values
OT_ERROR_NONE Successfully retrieved the Active Operational Dataset.
OT_ERROR_NOT_FOUND No corresponding value in the setting store.

◆ otDatasetGetDelayTimerMinimal()

uint32_t otDatasetGetDelayTimerMinimal ( otInstance * aInstance )

Get minimal delay timer.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
the value of minimal delay timer (in ms).

◆ otDatasetGetPending()

otError otDatasetGetPending ( otInstance * aInstance,
otOperationalDataset * aDataset
)

This function gets the Pending Operational Dataset.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aDataset A pointer to where the Pending Operational Dataset will be placed.
Return values
OT_ERROR_NONE Successfully retrieved the Pending Operational Dataset.
OT_ERROR_NOT_FOUND No corresponding value in the setting store.

◆ otDatasetGetPendingTlvs()

otError otDatasetGetPendingTlvs ( otInstance * aInstance,
otOperationalDatasetTlvs * aDataset
)

This function gets the Pending Operational Dataset.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aDataset A pointer to where the Pending Operational Dataset will be placed.
Return values
OT_ERROR_NONE Successfully retrieved the Pending Operational Dataset.
OT_ERROR_NOT_FOUND No corresponding value in the setting store.

◆ otDatasetIsCommissioned()

bool otDatasetIsCommissioned ( otInstance * aInstance )

This function indicates whether a valid network is present in the Active Operational Dataset or not.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
TRUE if a valid network is present in the Active Operational Dataset, FALSE otherwise.

◆ otDatasetParseTlvs()

otError otDatasetParseTlvs ( const otOperationalDatasetTlvs * aDatasetTlvs,
otOperationalDataset * aDataset
)

This function parses an Operational Dataset from a otOperationalDatasetTlvs .

Parameters
[in] aDatasetTlvs A pointer to dataset TLVs.
[out] aDataset A pointer to where the dataset will be placed.
Return values
OT_ERROR_NONE Successfully set aDataset from aDatasetTlvs .
OT_ERROR_INVALID_ARGS aDatasetTlvs is invalid.

◆ otDatasetSendMgmtActiveGet()

otError otDatasetSendMgmtActiveGet ( otInstance * aInstance,
const otOperationalDatasetComponents * aDatasetComponents,
const uint8_t * aTlvTypes,
uint8_t aLength,
const otIp6Address * aAddress
)

This function sends MGMT_ACTIVE_GET.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDatasetComponents A pointer to a Dataset Components structure specifying which components to request.
[in] aTlvTypes A pointer to array containing additional raw TLV types to be requested.
[in] aLength The length of aTlvTypes .
[in] aAddress A pointer to the IPv6 destination, if it is NULL, will use Leader ALOC as default.
Return values
OT_ERROR_NONE Successfully send the meshcop dataset command.
OT_ERROR_NO_BUFS Insufficient buffer space to send.

◆ otDatasetSendMgmtActiveSet()

otError otDatasetSendMgmtActiveSet ( otInstance * aInstance,
const otOperationalDataset * aDataset,
const uint8_t * aTlvs,
uint8_t aLength,
otDatasetMgmtSetCallback aCallback,
void * aContext
)

This function sends MGMT_ACTIVE_SET.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDataset A pointer to operational dataset.
[in] aTlvs A pointer to TLVs.
[in] aLength The length of TLVs.
[in] aCallback A pointer to a function that is called on response reception or timeout.
[in] aContext A pointer to application-specific context for aCallback .
Return values
OT_ERROR_NONE Successfully send the meshcop dataset command.
OT_ERROR_NO_BUFS Insufficient buffer space to send.
OT_ERROR_BUSY A previous request is ongoing.

◆ otDatasetSendMgmtPendingGet()

otError otDatasetSendMgmtPendingGet ( otInstance * aInstance,
const otOperationalDatasetComponents * aDatasetComponents,
const uint8_t * aTlvTypes,
uint8_t aLength,
const otIp6Address * aAddress
)

This function sends MGMT_PENDING_GET.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDatasetComponents A pointer to a Dataset Components structure specifying which components to request.
[in] aTlvTypes A pointer to array containing additional raw TLV types to be requested.
[in] aLength The length of aTlvTypes .
[in] aAddress A pointer to the IPv6 destination, if it is NULL, will use Leader ALOC as default.
Return values
OT_ERROR_NONE Successfully send the meshcop dataset command.
OT_ERROR_NO_BUFS Insufficient buffer space to send.

◆ otDatasetSendMgmtPendingSet()

otError otDatasetSendMgmtPendingSet ( otInstance * aInstance,
const otOperationalDataset * aDataset,
const uint8_t * aTlvs,
uint8_t aLength,
otDatasetMgmtSetCallback aCallback,
void * aContext
)

This function sends MGMT_PENDING_SET.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDataset A pointer to operational dataset.
[in] aTlvs A pointer to TLVs.
[in] aLength The length of TLVs.
[in] aCallback A pointer to a function that is called on response reception or timeout.
[in] aContext A pointer to application-specific context for aCallback .
Return values
OT_ERROR_NONE Successfully send the meshcop dataset command.
OT_ERROR_NO_BUFS Insufficient buffer space to send.
OT_ERROR_BUSY A previous request is ongoing.

◆ otDatasetSetActive()

otError otDatasetSetActive ( otInstance * aInstance,
const otOperationalDataset * aDataset
)

This function sets the Active Operational Dataset.

If the dataset does not include an Active Timestamp, the dataset is only partially complete.

If Thread is enabled on a device that has a partially complete Active Dataset, the device will attempt to attach to an existing Thread network using any existing information in the dataset. Only the Thread Network Key is needed to attach to a network.

If channel is not included in the dataset, the device will send MLE Announce messages across different channels to find neighbors on other channels.

If the device successfully attaches to a Thread network, the device will then retrieve the full Active Dataset from its Parent. Note that a router-capable device will not transition to the Router or Leader roles until it has a complete Active Dataset.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDataset A pointer to the Active Operational Dataset.
Return values
OT_ERROR_NONE Successfully set the Active Operational Dataset.
OT_ERROR_NO_BUFS Insufficient buffer space to set the Active Operational Dataset.
OT_ERROR_NOT_IMPLEMENTED The platform does not implement settings functionality.

◆ otDatasetSetActiveTlvs()

otError otDatasetSetActiveTlvs ( otInstance * aInstance,
const otOperationalDatasetTlvs * aDataset
)

This function sets the Active Operational Dataset.

If the dataset does not include an Active Timestamp, the dataset is only partially complete.

If Thread is enabled on a device that has a partially complete Active Dataset, the device will attempt to attach to an existing Thread network using any existing information in the dataset. Only the Thread Network Key is needed to attach to a network.

If channel is not included in the dataset, the device will send MLE Announce messages across different channels to find neighbors on other channels.

If the device successfully attaches to a Thread network, the device will then retrieve the full Active Dataset from its Parent. Note that a router-capable device will not transition to the Router or Leader roles until it has a complete Active Dataset.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDataset A pointer to the Active Operational Dataset.
Return values
OT_ERROR_NONE Successfully set the Active Operational Dataset.
OT_ERROR_NO_BUFS Insufficient buffer space to set the Active Operational Dataset.
OT_ERROR_NOT_IMPLEMENTED The platform does not implement settings functionality.

◆ otDatasetSetDelayTimerMinimal()

otError otDatasetSetDelayTimerMinimal ( otInstance * aInstance,
uint32_t aDelayTimerMinimal
)

Set minimal delay timer.

Note
This API is reserved for testing and demo purposes only. Changing settings with this API will render a production application non-compliant with the Thread Specification.
Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDelayTimerMinimal The value of minimal delay timer (in ms).
Return values
OT_ERROR_NONE Successfully set minimal delay timer.
OT_ERROR_INVALID_ARGS If aDelayTimerMinimal is not valid.

◆ otDatasetSetPending()

otError otDatasetSetPending ( otInstance * aInstance,
const otOperationalDataset * aDataset
)

This function sets the Pending Operational Dataset.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDataset A pointer to the Pending Operational Dataset.
Return values
OT_ERROR_NONE Successfully set the Pending Operational Dataset.
OT_ERROR_NO_BUFS Insufficient buffer space to set the Pending Operational Dataset.
OT_ERROR_NOT_IMPLEMENTED The platform does not implement settings functionality.

◆ otDatasetSetPendingTlvs()

otError otDatasetSetPendingTlvs ( otInstance * aInstance,
const otOperationalDatasetTlvs * aDataset
)

This function sets the Pending Operational Dataset.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDataset A pointer to the Pending Operational Dataset.
Return values
OT_ERROR_NONE Successfully set the Pending Operational Dataset.
OT_ERROR_NO_BUFS Insufficient buffer space to set the Pending Operational Dataset.
OT_ERROR_NOT_IMPLEMENTED The platform does not implement settings functionality.

◆ otDatasetUpdaterCancelUpdate()

void otDatasetUpdaterCancelUpdate ( otInstance * aInstance )

This function cancels an ongoing (if any) Operational Dataset update request.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otDatasetUpdaterIsUpdateOngoing()

bool otDatasetUpdaterIsUpdateOngoing ( otInstance * aInstance )

This function indicates whether there is an ongoing Operation Dataset update request.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
TRUE There is an ongoing update.
FALSE There is no ongoing update.

◆ otDatasetUpdaterRequestUpdate()

otError otDatasetUpdaterRequestUpdate ( otInstance * aInstance,
const otOperationalDataset * aDataset,
otDatasetUpdaterCallback aCallback,
void * aContext
)

This function requests an update to Operational Dataset.

aDataset should contain the fields to be updated and their new value. It must not contain Active or Pending Timestamp fields. The Delay field is optional, if not provided a default value (1000 ms) would be used.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aDataset A pointer to the Dataset containing the fields to change.
[in] aCallback A callback to indicate when Dataset update request finishes.
[in] aContext An arbitrary context passed to callback.
Return values
OT_ERROR_NONE Dataset update started successfully ( aCallback will be invoked on completion).
OT_ERROR_INVALID_STATE Device is disabled (MLE is disabled).
OT_ERROR_INVALID_ARGS The aDataset is not valid (contains Active or Pending Timestamp).
OT_ERROR_BUSY Cannot start update, a previous one is ongoing.
OT_ERROR_NO_BUFS Could not allocated buffer to save Dataset.

◆ otNetworkNameFromString()

otError otNetworkNameFromString ( otNetworkName * aNetworkName,
const char * aNameString
)

This function sets an otNetworkName instance from a given null terminated C string.

This function also validates that the given aNameString follows UTF-8 encoding and its length is not longer than OT_NETWORK_NAME_MAX_SIZE .

Parameters
[out] aNetworkName A pointer to the otNetworkName to set.
[in] aNameString A name C string.
Return values
OT_ERROR_NONE Successfully set aNetworkName from aNameString .
OT_ERROR_INVALID_ARGS aNameStrng is invalid (too long or does not follow UTF-8 encoding).