otTcpEndpoint Struct Reference
This structure represents a TCP endpoint.
#include <
include/openthread/tcp.h
>
Public Attributes |
|
| struct otTcpEndpoint * | mNext |
|
A pointer to the next TCP endpoint (internal use only)
|
|
| otInstance * | mInstance |
|
A pointer to the OpenThread instance associated with this TCP endpoint.
|
|
| void * | mContext |
|
A pointer to application-specific context.
|
|
| otTcpEstablished | mEstablishedCallback |
|
"Established" callback function
|
|
| otTcpSendDone | mSendDoneCallback |
|
"Send done" callback function
|
|
| otTcpSendReady | mSendReadyCallback |
|
"Send ready" callback function
|
|
| otTcpReceiveAvailable | mReceiveAvailableCallback |
|
"Receive available" callback function
|
|
| otTcpDisconnected | mDisconnectedCallback |
|
"Disconnected" callback function
|
|
| uint32_t | mTimers [4] |
This structure represents a TCP endpoint.
An TCP endpoint acts an endpoint of TCP connection. It can be used to initiate TCP connections, and, once a TCP connection is established, send data to and receive data from the connection peer.
The application should not inspect the fields of this structure directly; it should only interact with it via the TCP API functions whose signatures are provided in this file.
The documentation for this struct was generated from the following file:
-
include/openthread/
tcp.h