otNetworkDiagMacCounters Struct Reference

This structure represents a Network Diagnostic Mac Counters value.

#include <include/openthread/netdiag.h>

Public Attributes

uint32_t mIfInUnknownProtos
 
uint32_t mIfInErrors
 
uint32_t mIfOutErrors
 
uint32_t mIfInUcastPkts
 
uint32_t mIfInBroadcastPkts
 
uint32_t mIfInDiscards
 
uint32_t mIfOutUcastPkts
 
uint32_t mIfOutBroadcastPkts
 
uint32_t mIfOutDiscards

This structure represents a Network Diagnostic Mac Counters value.

See RFC 2863 for definitions of member fields.


The documentation for this struct was generated from the following file:
  • include/openthread/netdiag.h