This structure represents the IP level counters.
#include <
include/openthread/thread.h
>
Public Attributes | |
uint32_t | mTxSuccess |
The number of IPv6 packets successfully transmitted. | |
uint32_t | mRxSuccess |
The number of IPv6 packets successfully received. | |
uint32_t | mTxFailure |
The number of IPv6 packets failed to transmit. | |
uint32_t | mRxFailure |
The number of IPv6 packets failed to receive. |
This structure represents the IP level counters.
The documentation for this struct was generated from the following file:
- include/openthread/
thread.h