RNG Non-cryptographic
This module includes functions that generates non cryptographic random numbers.
Functions | |
uint32_t | otRandomNonCryptoGetUint32 (void) |
This function generates and returns a random uint32_t value. | |
uint8_t | otRandomNonCryptoGetUint8 (void) |
This function generates and returns a random byte. | |
uint16_t | otRandomNonCryptoGetUint16 (void) |
This function generates and returns a random uint16_t value. | |
uint8_t | otRandomNonCryptoGetUint8InRange (uint8_t aMin, uint8_t aMax) |
This function generates and returns a random uint8_t value within a given range [aMin, aMax) . | |
uint16_t | otRandomNonCryptoGetUint16InRange (uint16_t aMin, uint16_t aMax) |
This function generates and returns a random uint16_t value within a given range [aMin, aMax) . | |
uint32_t | otRandomNonCryptoGetUint32InRange (uint32_t aMin, uint32_t aMax) |
This function generates and returns a random uint32_t value within a given range [aMin, aMax) . | |
void | otRandomNonCryptoFillBuffer (uint8_t *aBuffer, uint16_t aSize) |
This function fills a given buffer with random bytes. | |
uint32_t | otRandomNonCryptoAddJitter (uint32_t aValue, uint16_t aJitter) |
This function adds a random jitter within a given range to a given value. |
Detailed Description
This module includes functions that generates non cryptographic random numbers.
Function Documentation
◆ otRandomNonCryptoAddJitter()
uint32_t otRandomNonCryptoAddJitter | ( | uint32_t | aValue, |
uint16_t | aJitter |
||
) |
This function adds a random jitter within a given range to a given value.
- Parameters
-
[in] aValue
A value to which the random jitter is added. [in] aJitter
Maximum jitter. Random jitter is selected from the range [-aJitter, aJitter]
.
- Returns
- The given value with an added random jitter.
◆ otRandomNonCryptoFillBuffer()
void otRandomNonCryptoFillBuffer | ( | uint8_t * | aBuffer, |
uint16_t | aSize |
||
) |
This function fills a given buffer with random bytes.
- Parameters
-
[out] aBuffer
A pointer to a buffer to fill with the random bytes. [in] aSize
Size of buffer (number of bytes to fill).
◆ otRandomNonCryptoGetUint16()
uint16_t otRandomNonCryptoGetUint16 | ( | void |
| ) |
This function generates and returns a random uint16_t
value.
- Returns
- A random
uint16_t
value.
◆ otRandomNonCryptoGetUint16InRange()
uint16_t otRandomNonCryptoGetUint16InRange | ( | uint16_t | aMin, |
uint16_t | aMax |
||
) |
This function generates and returns a random uint16_t
value within a given range [aMin, aMax)
.
- Note
- The returned random value can include the
aMin
value but excludes theaMax
.
- Parameters
-
[in] aMin
A minimum value (this value can be included in returned random result). [in] aMax
A maximum value (this value is excluded from returned random result).
- Returns
- A random
uint16_t
value in the given range (i.e., aMin <= random value < aMax).
◆ otRandomNonCryptoGetUint32()
uint32_t otRandomNonCryptoGetUint32 | ( | void |
| ) |
This function generates and returns a random uint32_t
value.
- Returns
- A random
uint32_t
value.
◆ otRandomNonCryptoGetUint32InRange()
uint32_t otRandomNonCryptoGetUint32InRange | ( | uint32_t | aMin, |
uint32_t | aMax |
||
) |
This function generates and returns a random uint32_t
value within a given range [aMin, aMax)
.
- Note
- The returned random value can include the
aMin
value but excludes theaMax
.
- Parameters
-
[in] aMin
A minimum value (this value can be included in returned random result). [in] aMax
A maximum value (this value is excluded from returned random result).
- Returns
- A random
uint32_t
value in the given range (i.e., aMin <= random value < aMax).
◆ otRandomNonCryptoGetUint8()
uint8_t otRandomNonCryptoGetUint8 | ( | void |
| ) |
This function generates and returns a random byte.
- Returns
- A random
uint8_t
value.
◆ otRandomNonCryptoGetUint8InRange()
uint8_t otRandomNonCryptoGetUint8InRange | ( | uint8_t | aMin, |
uint8_t | aMax |
||
) |
This function generates and returns a random uint8_t
value within a given range [aMin, aMax)
.
- Parameters
-
[in] aMin
A minimum value (this value can be included in returned random result). [in] aMax
A maximum value (this value is excluded from returned random result).
- Returns
- A random
uint8_t
value in the given range (i.e., aMin <= random value < aMax).