otOperationalDatasetTlvs Struct Reference
This structure represents an Active or Pending Operational Dataset.
#include <
include/openthread/dataset.h
>
Public Attributes | |
uint8_t | mTlvs [OT_OPERATIONAL_DATASET_MAX_LENGTH] |
Operational Dataset TLVs. | |
uint8_t | mLength |
Size of Operational Dataset in bytes. |
This structure represents an Active or Pending Operational Dataset.
The Operational Dataset is TLV encoded as specified by Thread.
The documentation for this struct was generated from the following file:
- include/openthread/
dataset.h