otLinkMetricsValues Struct Reference
This structure represents the result (value) for a Link Metrics query.
#include <
include/openthread/link_metrics.h
>
Public Attributes | |
otLinkMetrics | mMetrics |
Specifies which metrics values are present/included. | |
uint32_t | mPduCountValue |
The value of Pdu Count. | |
uint8_t | mLqiValue |
The value LQI. | |
uint8_t | mLinkMarginValue |
The value of Link Margin. | |
int8_t | mRssiValue |
The value of Rssi. |
This structure represents the result (value) for a Link Metrics query.
The documentation for this struct was generated from the following file:
- include/openthread/
link_metrics.h