This module includes functions that control the OpenThread Instance.

Macros

#define OT_UPTIME_STRING_SIZE 24
Recommended size for string representation of uptime.

Typedefs

typedef struct otInstance otInstance
This structure represents the OpenThread instance structure.
typedef uint32_t otChangedFlags
This type represents a bit-field indicating specific state/configuration that has changed.
typedef void(* otStateChangedCallback ) ( otChangedFlags aFlags, void *aContext)
This function pointer is called to notify certain configuration or state changes within OpenThread.

Enumerations

enum {
OT_CHANGED_IP6_ADDRESS_ADDED = 1 << 0,
OT_CHANGED_IP6_ADDRESS_REMOVED = 1 << 1,
OT_CHANGED_THREAD_ROLE = 1 << 2,
OT_CHANGED_THREAD_LL_ADDR = 1 << 3,
OT_CHANGED_THREAD_ML_ADDR = 1 << 4,
OT_CHANGED_THREAD_RLOC_ADDED = 1 << 5,
OT_CHANGED_THREAD_RLOC_REMOVED = 1 << 6,
OT_CHANGED_THREAD_PARTITION_ID = 1 << 7,
OT_CHANGED_THREAD_KEY_SEQUENCE_COUNTER = 1 << 8,
OT_CHANGED_THREAD_NETDATA = 1 << 9,
OT_CHANGED_THREAD_CHILD_ADDED = 1 << 10,
OT_CHANGED_THREAD_CHILD_REMOVED = 1 << 11,
OT_CHANGED_IP6_MULTICAST_SUBSCRIBED = 1 << 12,
OT_CHANGED_IP6_MULTICAST_UNSUBSCRIBED = 1 << 13,
OT_CHANGED_THREAD_CHANNEL = 1 << 14,
OT_CHANGED_THREAD_PANID = 1 << 15,
OT_CHANGED_THREAD_NETWORK_NAME = 1 << 16,
OT_CHANGED_THREAD_EXT_PANID = 1 << 17,
OT_CHANGED_NETWORK_KEY = 1 << 18,
OT_CHANGED_PSKC = 1 << 19,
OT_CHANGED_SECURITY_POLICY = 1 << 20,
OT_CHANGED_CHANNEL_MANAGER_NEW_CHANNEL = 1 << 21,
OT_CHANGED_SUPPORTED_CHANNEL_MASK = 1 << 22,
OT_CHANGED_COMMISSIONER_STATE = 1 << 23,
OT_CHANGED_THREAD_NETIF_STATE = 1 << 24,
OT_CHANGED_THREAD_BACKBONE_ROUTER_STATE = 1 << 25,
OT_CHANGED_THREAD_BACKBONE_ROUTER_LOCAL = 1 << 26,
OT_CHANGED_JOINER_STATE = 1 << 27,
OT_CHANGED_ACTIVE_DATASET = 1 << 28,
OT_CHANGED_PENDING_DATASET = 1 << 29
}
This enumeration defines flags that are passed as part of otStateChangedCallback .

Functions

otInstance * otInstanceInit (void *aInstanceBuffer, size_t *aInstanceBufferSize)
This function initializes the OpenThread library.
otInstance * otInstanceInitSingle (void)
This function initializes the static single instance of the OpenThread library.
bool otInstanceIsInitialized ( otInstance *aInstance)
This function indicates whether or not the instance is valid/initialized.
void otInstanceFinalize ( otInstance *aInstance)
This function disables the OpenThread library.
uint64_t otInstanceGetUptime ( otInstance *aInstance)
This function returns the current instance uptime (in msec).
void otInstanceGetUptimeAsString ( otInstance *aInstance, char *aBuffer, uint16_t aSize)
This function returns the current instance uptime as a human-readable string.
otError otSetStateChangedCallback ( otInstance *aInstance, otStateChangedCallback aCallback, void *aContext)
This function registers a callback to indicate when certain configuration or state changes within OpenThread.
void otRemoveStateChangeCallback ( otInstance *aInstance, otStateChangedCallback aCallback, void *aContext)
This function removes a callback to indicate when certain configuration or state changes within OpenThread.
void otInstanceReset ( otInstance *aInstance)
This method triggers a platform reset.
void otInstanceFactoryReset ( otInstance *aInstance)
This method deletes all the settings stored on non-volatile memory, and then triggers platform reset.
void otInstanceResetRadioStack ( otInstance *aInstance)
This method resets the internal states of the OpenThread radio stack.
otError otInstanceErasePersistentInfo ( otInstance *aInstance)
This function erases all the OpenThread persistent info (network settings) stored on non-volatile memory.
const char * otGetVersionString (void)
This function gets the OpenThread version string.
const char * otGetRadioVersionString ( otInstance *aInstance)
This function gets the OpenThread radio version string.

Detailed Description

This module includes functions that control the OpenThread Instance.

Typedef Documentation

◆ otChangedFlags

typedef uint32_t otChangedFlags

This type represents a bit-field indicating specific state/configuration that has changed.

See OT_CHANGED_* definitions.

◆ otStateChangedCallback

typedef void(* otStateChangedCallback) ( otChangedFlags aFlags, void *aContext)

This function pointer is called to notify certain configuration or state changes within OpenThread.

Parameters
[in] aFlags A bit-field indicating specific state that has changed. See OT_CHANGED_* definitions.
[in] aContext A pointer to application-specific context.

Enumeration Type Documentation

◆ anonymous enum

anonymous enum

This enumeration defines flags that are passed as part of otStateChangedCallback .

Enumerator
OT_CHANGED_IP6_ADDRESS_ADDED

IPv6 address was added.

OT_CHANGED_IP6_ADDRESS_REMOVED

IPv6 address was removed.

OT_CHANGED_THREAD_ROLE

Role (disabled, detached, child, router, leader) changed.

OT_CHANGED_THREAD_LL_ADDR

The link-local address changed.

OT_CHANGED_THREAD_ML_ADDR

The mesh-local address changed.

OT_CHANGED_THREAD_RLOC_ADDED

RLOC was added.

OT_CHANGED_THREAD_RLOC_REMOVED

RLOC was removed.

OT_CHANGED_THREAD_PARTITION_ID

Partition ID changed.

OT_CHANGED_THREAD_KEY_SEQUENCE_COUNTER

Thread Key Sequence changed.

OT_CHANGED_THREAD_NETDATA

Thread Network Data changed.

OT_CHANGED_THREAD_CHILD_ADDED

Child was added.

OT_CHANGED_THREAD_CHILD_REMOVED

Child was removed.

OT_CHANGED_IP6_MULTICAST_SUBSCRIBED

Subscribed to a IPv6 multicast address.

OT_CHANGED_IP6_MULTICAST_UNSUBSCRIBED

Unsubscribed from a IPv6 multicast address.

OT_CHANGED_THREAD_CHANNEL

Thread network channel changed.

OT_CHANGED_THREAD_PANID

Thread network PAN Id changed.

OT_CHANGED_THREAD_NETWORK_NAME

Thread network name changed.

OT_CHANGED_THREAD_EXT_PANID

Thread network extended PAN ID changed.

OT_CHANGED_NETWORK_KEY

Network key changed.

OT_CHANGED_PSKC

PSKc changed.

OT_CHANGED_SECURITY_POLICY

Security Policy changed.

OT_CHANGED_CHANNEL_MANAGER_NEW_CHANNEL

Channel Manager new pending Thread channel changed.

OT_CHANGED_SUPPORTED_CHANNEL_MASK

Supported channel mask changed.

OT_CHANGED_COMMISSIONER_STATE

Commissioner state changed.

OT_CHANGED_THREAD_NETIF_STATE

Thread network interface state changed.

OT_CHANGED_THREAD_BACKBONE_ROUTER_STATE

Backbone Router state changed.

OT_CHANGED_THREAD_BACKBONE_ROUTER_LOCAL

Local Backbone Router configuration changed.

OT_CHANGED_JOINER_STATE

Joiner state changed.

OT_CHANGED_ACTIVE_DATASET

Active Operational Dataset changed.

OT_CHANGED_PENDING_DATASET

Pending Operational Dataset changed.

Function Documentation

◆ otGetRadioVersionString()

const char* otGetRadioVersionString ( otInstance * aInstance )

This function gets the OpenThread radio version string.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
A pointer to the OpenThread radio version.

◆ otGetVersionString()

const char* otGetVersionString ( void )

This function gets the OpenThread version string.

Returns
A pointer to the OpenThread version.

◆ otInstanceErasePersistentInfo()

otError otInstanceErasePersistentInfo ( otInstance * aInstance )

This function erases all the OpenThread persistent info (network settings) stored on non-volatile memory.

Erase is successful only if the device is in disabled state/role.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Return values
OT_ERROR_NONE All persistent info/state was erased successfully.
OT_ERROR_INVALID_STATE Device is not in disabled state/role.

◆ otInstanceFactoryReset()

void otInstanceFactoryReset ( otInstance * aInstance )

This method deletes all the settings stored on non-volatile memory, and then triggers platform reset.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otInstanceFinalize()

void otInstanceFinalize ( otInstance * aInstance )

This function disables the OpenThread library.

Call this function when OpenThread is no longer in use.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otInstanceGetUptime()

uint64_t otInstanceGetUptime ( otInstance * aInstance )

This function returns the current instance uptime (in msec).

This function requires OPENTHREAD_CONFIG_UPTIME_ENABLE to be enabled.

The uptime is given as number of milliseconds since OpenThread instance was initialized.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
The uptime (number of milliseconds).

◆ otInstanceGetUptimeAsString()

void otInstanceGetUptimeAsString ( otInstance * aInstance,
char * aBuffer,
uint16_t aSize
)

This function returns the current instance uptime as a human-readable string.

This function requires OPENTHREAD_CONFIG_UPTIME_ENABLE to be enabled.

The string follows the format "<hh>:<mm>:<ss>.<mmmm>" for hours, minutes, seconds and millisecond (if uptime is shorter than one day) or "<dd>d.<hh>:<mm>:<ss>.<mmmm>" (if longer than a day).

If the resulting string does not fit in aBuffer (within its aSize characters), the string will be truncated but the outputted string is always null-terminated.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[out] aBuffer A pointer to a char array to output the string.
[in] aSize The size of aBuffer (in bytes). Recommended to use OT_UPTIME_STRING_SIZE .

◆ otInstanceInit()

otInstance * otInstanceInit ( void * aInstanceBuffer,
size_t * aInstanceBufferSize
)

This function initializes the OpenThread library.

This function initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread.

This function is available and can only be used when support for multiple OpenThread instances is enabled.

Parameters
[in] aInstanceBuffer The buffer for OpenThread to use for allocating the otInstance structure.
[in,out] aInstanceBufferSize On input, the size of aInstanceBuffer. On output, if not enough space for otInstance, the number of bytes required for otInstance.
Returns
A pointer to the new OpenThread instance.
See also
otInstanceFinalize

◆ otInstanceInitSingle()

otInstance * otInstanceInitSingle ( void )

This function initializes the static single instance of the OpenThread library.

This function initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread.

This function is available and can only be used when support for multiple OpenThread instances is disabled.

Returns
A pointer to the single OpenThread instance.

◆ otInstanceIsInitialized()

bool otInstanceIsInitialized ( otInstance * aInstance )

This function indicates whether or not the instance is valid/initialized.

The instance is considered valid if it is acquired and initialized using either otInstanceInitSingle() (in single instance case) or otInstanceInit() (in multi instance case). A subsequent call to otInstanceFinalize() causes the instance to be considered as uninitialized.

Parameters
[in] aInstance A pointer to an OpenThread instance.
Returns
TRUE if the given instance is valid/initialized, FALSE otherwise.

◆ otInstanceReset()

void otInstanceReset ( otInstance * aInstance )

This method triggers a platform reset.

The reset process ensures that all the OpenThread state/info (stored in volatile memory) is erased. Note that the otPlatformReset does not erase any persistent state/info saved in non-volatile memory.

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otInstanceResetRadioStack()

void otInstanceResetRadioStack ( otInstance * aInstance )

This method resets the internal states of the OpenThread radio stack.

Callbacks and configurations are preserved.

This API is only available under radio builds ( OPENTHREAD_RADIO = 1 ).

Parameters
[in] aInstance A pointer to an OpenThread instance.

◆ otRemoveStateChangeCallback()

void otRemoveStateChangeCallback ( otInstance * aInstance,
otStateChangedCallback aCallback,
void * aContext
)

This function removes a callback to indicate when certain configuration or state changes within OpenThread.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aCallback A pointer to a function that is called with certain configuration or state changes.
[in] aContext A pointer to application-specific context.

◆ otSetStateChangedCallback()

otError otSetStateChangedCallback ( otInstance * aInstance,
otStateChangedCallback aCallback,
void * aContext
)

This function registers a callback to indicate when certain configuration or state changes within OpenThread.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aCallback A pointer to a function that is called with certain configuration or state changes.
[in] aContext A pointer to application-specific context.
Return values
OT_ERROR_NONE Added the callback to the list of callbacks.
OT_ERROR_ALREADY The callback was already registered.
OT_ERROR_NO_BUFS Could not add the callback due to resource constraints.