otUdpSocket Struct Reference
This structure represents a UDP socket.
#include <
include/openthread/udp.h
>
Public Attributes | |
otSockAddr | mSockName |
The local IPv6 socket address. | |
otSockAddr | mPeerName |
The peer IPv6 socket address. | |
otUdpReceive | mHandler |
A function pointer to the application callback. | |
void * | mContext |
A pointer to application-specific context. | |
void * | mHandle |
A handle to platform's UDP. | |
struct otUdpSocket * | mNext |
A pointer to the next UDP socket (internal use only). |
This structure represents a UDP socket.
The documentation for this struct was generated from the following file:
- include/openthread/
udp.h