This file includes the OpenThread API for the ping sender module.

Classes

struct otPingSenderReply
This structure represents a ping reply.
struct otPingSenderStatistics
This structure represents statistics of a ping request.
struct otPingSenderConfig
This structure represents a ping request configuration.

Typedefs

typedef struct otPingSenderReply otPingSenderReply
This structure represents a ping reply.
typedef struct otPingSenderStatistics otPingSenderStatistics
This structure represents statistics of a ping request.
typedef void(* otPingSenderReplyCallback ) (const otPingSenderReply *aReply, void *aContext)
This function pointer type specifies the callback to notify receipt of a ping reply.
typedef void(* otPingSenderStatisticsCallback ) (const otPingSenderStatistics *aStatistics, void *aContext)
This function pointer type specifies the callback to report the ping statistics.
typedef struct otPingSenderConfig otPingSenderConfig
This structure represents a ping request configuration.

Functions

otError otPingSenderPing ( otInstance *aInstance, const otPingSenderConfig *aConfig)
This function starts a ping.
void otPingSenderStop ( otInstance *aInstance)
This function stops an ongoing ping.

Detailed Description

This file includes the OpenThread API for the ping sender module.

Typedef Documentation

◆ otPingSenderReplyCallback

typedef void(* otPingSenderReplyCallback) (const otPingSenderReply *aReply, void *aContext)

This function pointer type specifies the callback to notify receipt of a ping reply.

Parameters
[in] aReply A pointer to a otPingSenderReply containing info about the received ping reply.
[in] aContext A pointer to application-specific context.

◆ otPingSenderStatisticsCallback

typedef void(* otPingSenderStatisticsCallback) (const otPingSenderStatistics *aStatistics, void *aContext)

This function pointer type specifies the callback to report the ping statistics.

Parameters
[in] aStatistics A pointer to a otPingSenderStatistics containing info about the received ping statistics.
[in] aContext A pointer to application-specific context.

Function Documentation

◆ otPingSenderPing()

otError otPingSenderPing ( otInstance * aInstance,
const otPingSenderConfig * aConfig
)

This function starts a ping.

Parameters
[in] aInstance A pointer to an OpenThread instance.
[in] aConfig The ping config to use.
Return values
OT_ERROR_NONE The ping started successfully.
OT_ERROR_BUSY Could not start since busy with a previous ongoing ping request.
OT_ERROR_INVALID_ARGS The aConfig contains invalid parameters (e.g., ping interval is too long).

◆ otPingSenderStop()

void otPingSenderStop ( otInstance * aInstance )

This function stops an ongoing ping.

Parameters
[in] aInstance A pointer to an OpenThread instance.