This structure represents an External Route configuration.
#include <
include/openthread/netdata.h
>
Public Attributes | |
otIp6Prefix | mPrefix |
The IPv6 prefix. | |
uint16_t | mRloc16 |
The border router's RLOC16 (value ignored on config add). | |
signed int | mPreference: 2 |
A 2-bit signed int preference (OT_ROUTE_PREFERENCE_* values). | |
bool | mNat64: 1 |
Whether this is a NAT64 prefix. | |
bool | mStable: 1 |
Whether this configuration is considered Stable Network Data. | |
bool | mNextHopIsThisDevice: 1 |
Whether the next hop is this device (value ignored on config add). |
This structure represents an External Route configuration.
The documentation for this struct was generated from the following file:
- include/openthread/
netdata.h