Building and Sending Messages
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_BSEND |
|
bsend [srcEndpoint:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_GROUP |
|
interpan group [groupId:2] [destPan:2] [destprofileID:2]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_LONG |
|
interpan long [longId:8] [destPAN:2] [destProfileID:2] [options:2]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_SHORT |
|
interpan short [shortId:2] [destPan:2] [destprofileID:2]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_RAW |
|
raw [clusterId:2] [data:-1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND |
|
send [id:2] [src-endpoint:1] [dst-endpoint:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND_USING_MULTICAST_BINDING |
|
send-using-multicast-binding [useMulticastBinding:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND_MULTICAST |
|
send_multicast [groupId:2] [src-endpoint:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_TIMESYNC |
|
timesync [id:2] [srcEndpoint:1] [destEndpoint:1]
|
|
Detailed Description
Commands for building and sending messages out onto the network.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_BSEND |
bsend [srcEndpoint:1]
-
Send using a binding based on the clusterId in the globalApsFrame and the srcEndpoint specified (if the src endpoint is zero it only sends based on the clusterId)
- srcEndpoint - INT8U - Source endpoint to send a binding based message from
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_GROUP |
interpan group [groupId:2] [destPan:2] [destprofileID:2]
-
send an interpan message to a group id.
- groupId - INT16U - group id to send to
- destPan - INT16U - destination pan id
- destprofileID - INT16U - destination profile ID
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_LONG |
interpan long [longId:8] [destPAN:2] [destProfileID:2] [options:2]
-
Send an interpan message to a long address (8 byte eui64)
- longId - IEEE_ADDRESS - long ieee address to send the interpan message to
- destPAN - INT16U - two byte destination PA ID
- destProfileID - INT16U - two byte destination profile ID
- options - INT16U - two byte options
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_SHORT |
interpan short [shortId:2] [destPan:2] [destprofileID:2]
-
Send an interpan message to a short id.
- shortId - INT16U - group id to send to
- destPan - INT16U - destination pan id
- destprofileID - INT16U - destination profile ID
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_RAW |
raw [clusterId:2] [data:-1]
-
Creates a message by specifying the raw bytes. Use "send" to send the message once it has been created. Ex: raw 0x000F {00 0A 00 11 22 33 44 55} sends a message to cluster 15 (0x000F) of length 8 which includes the ZCL header.
- clusterId - INT16U - two byte cluster id
- data - OCTET_STRING - ZCL message, including ZCL header and payload
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND |
send [id:2] [src-endpoint:1] [dst-endpoint:1]
-
Send a pre-buffered message from a given endpoint to an endpoint on a device with a given short address.
- id - INT16U - short id of the device to send the message to
- src-endpoint - INT8U - The endpoint to send the message from
- dst-endpoint - INT8U - The endpoint to send the message to
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND_MULTICAST |
send_multicast [groupId:2] [src-endpoint:1]
-
Send a pre-buffered multicast message to a given group id from a given endpoint.
- groupId - INT16U - group id of the multicast group to send the message to
- src-endpoint - INT8U - The endpoint to send the message from
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND_USING_MULTICAST_BINDING |
send-using-multicast-binding [useMulticastBinding:1]
-
When sending using a binding, specify whether a multicast binding should be used.
- useMulticastBinding - BOOLEAN - Whether to send via a multicast binding
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_TIMESYNC |
timesync [id:2] [srcEndpoint:1] [destEndpoint:1]
-
This sends a read attr for the time of the device specified. It sets a flag so when it gets the response it writes the time to its own time attr
- id - INT16U - two byte short id of the time server
- srcEndpoint - INT8U - source endpoint to send time sync from
- destEndpoint - INT8U - destination endpoint to expect response on