Plugin Commands: Mac address filtering
Detailed Description
Commands to manipulate the MAC address filtering tables.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_CLEAR_STATS |
plugin mac-address-filtering clear-stats
- Clears all packet counts for all modes. Leaves config and lists intact.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_ADD |
plugin mac-address-filtering long-address-list add [eui64:8]
-
Adds a long address to the long address filter.
- eui64 - IEEE_ADDRESS - The long address to add.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_CLEAR |
plugin mac-address-filtering long-address-list clear
- Clears the long address list filter.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_DELETE |
plugin mac-address-filtering long-address-list delete [index:1]
-
Deletes an entry in the long address list filter.
- index - INT8U - The entry in the long address list to delete.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_SET_BLACKLIST |
plugin mac-address-filtering long-address-list set-blacklist
- Sets the long address list filter to a blacklist.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_LONG_ADDRESS_LIST_SET_WHITELIST |
plugin mac-address-filtering long-address-list set-whitelist
- Sets the long address list filter to a whitelist.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_ADD |
plugin mac-address-filtering pan-id-list add [pan-id:2]
-
Adds a PAN ID to the filter.
- pan-id - INT16U - The PAN ID to add to the list.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_CLEAR |
plugin mac-address-filtering pan-id-list clear
- Clears the PAN ID list filter.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_DELETE |
plugin mac-address-filtering pan-id-list delete [index:1]
-
Deletes an entry in the PAN ID list filter.
- index - INT8U - The index of the entry to delete.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_SET_BLACKLIST |
plugin mac-address-filtering pan-id-list set-blacklist
- Sets the PAN_ID list filter to a blacklist.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PAN_ID_LIST_SET_WHITELIST |
plugin mac-address-filtering pan-id-list set-whitelist
- Sets the PAN-ID list filter to a whitelist.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_PRINT_CONFIG |
plugin mac-address-filtering print-config
- Prints the current filtering config and statistics.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_RESET |
plugin mac-address-filtering reset
- Resets the state of the plugin to the default of no filtering.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SET_CONFIG_NO_ADDRESS_FILTER |
plugin mac-address-filtering set-config no-address-filter [enable:1]
-
Enable/disable filtering of no-address messages.
- enable - BOOLEAN - True means drop no-address messages, false means allow.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_ADD |
plugin mac-address-filtering short-address-list add [node-id:2]
-
Adds an address to the short address list.
- node-id - INT16U - The node-id to add to the short list.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_CLEAR |
plugin mac-address-filtering short-address-list clear
- Clears the short address list filter.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_DELETE |
plugin mac-address-filtering short-address-list delete [index:1]
-
Deletes an entry in the short address list filter.
- index - INT8U - The index of the entry to delete.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_SET_BLACKLIST |
plugin mac-address-filtering short-address-list set-blacklist
- Sets the short address list filter to a blacklist.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MAC_ADDRESS_FILTERING_PLUGIN_MAC_ADDRESS_FILTERING_SHORT_ADDRESS_LIST_SET_WHITELIST |
plugin mac-address-filtering short-address-list set-whitelist
- Sets the short address list filter to a whitelist.