Plugin Commands: Network Steering
Detailed Description
The Network Steering plugin commands are currently being used for the Profile Interop event.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_ADD |
plugin network-steering mask add [whichMask:1] [channel:1]
-
Adds a channel to either the primary or secondary channel mask of the network-steering plugin.
- whichMask - INT8U - The channel mask to add a channel to.
- channel - INT8U - The channel to add to the mask.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SET |
plugin network-steering mask set [whichMask:1] [mask:4]
-
Set either the primary or secondary channel mask.
- whichMask - INT8U - The channel mask to subtract the channel from.
- mask - INT32U - The value to set the channel mask to.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_MASK_SUBTRACT |
plugin network-steering mask subtract [whichMask:1] [channel:1]
-
Subtracts a channel from either the primary or secondary channel mask of the network-steering plugin.
- whichMask - INT8U - The channel mask to subtract the channel from.
- channel - INT8U - The channel to subtract the mask from.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_PRE_CONFIGURED_KEY_SET |
plugin network-steering pre-configured-key-set [preconfiguredkey:-1]
-
Set the pre-configured key
- preconfiguredkey - OCTET_STRING - Set the preconfigured key so that the joining device can enter the network.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_START |
plugin network-steering start [options:1]
-
Starts the network steering process.
- options - INT8U - A mask of options for indicating specific behavior within the network-steering process.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STATUS |
plugin network-steering status
- Displays the current status of the network steering process.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_NETWORK_STEERING_PLUGIN_NETWORK_STEERING_STOP |
plugin network-steering stop
- Stops the network steering process.