EmberSignatureData Struct Reference
This data structure contains a DSA signature. It is the bit concatenation of the 'r' and 's' components of the signature.
#include <
ember-types.h
>
Data Fields |
|
uint8_t | contents [ EMBER_SIGNATURE_SIZE ] |
This data structure contains a DSA signature. It is the bit concatenation of the 'r' and 's' components of the signature.
Field Documentation
uint8_t EmberSignatureData::contents[ EMBER_SIGNATURE_SIZE ] |
The documentation for this struct was generated from the following file:
-
ember-types.h