Plugin Commands: Events Server
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_ADD |
|
plugin events-server add [endpoint:1] [logId:1] [eventId:2] [eventTime:4] [eventData:-1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_CLEAR |
|
plugin events-server clear [endpoint:1] [logId:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_EPRINT |
|
plugin events-server eprint [endpoint:1] [logId:1] [index:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_PRINT |
|
plugin events-server print [endpoint:1] [logId:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_PUBLISH |
|
plugin events-server publish [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [logId:1] [index:1] [eventControl:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_SET |
|
plugin events-server set [endpoint:1] [logId:1] [index:1] [eventId:2] [eventTime:4] [eventData:-1]
|
|
Detailed Description
The events-server plugin contributes several commands to the application framework's CLI. These commands are be used for adding, clearing, and printing events.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_ADD |
plugin events-server add [endpoint:1] [logId:1] [eventId:2] [eventTime:4] [eventData:-1]
-
Append the event to the event log for the provided endpoint. Once the event log is full, new events will start overwriting old events at the beginning of the table.
- endpoint - INT8U - the relevant endpoint
- logId - INT8U - the relevant log
- eventId - INT16U - the event id
- eventTime - INT32U - the event time
- eventData - OCTET_STRING - additional event data
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_CLEAR |
plugin events-server clear [endpoint:1] [logId:1]
-
Clear out the specified event log for the provided endpoint.
- endpoint - INT8U - the relevant endpoint
- logId - INT8U - the log to be cleared
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_EPRINT |
plugin events-server eprint [endpoint:1] [logId:1] [index:1]
-
Print the event at the given index in the specified event log for the provided endpoint.
- endpoint - INT8U - the relevant endpoint
- logId - INT8U - the relevant log
- index - INT8U - the index within the event log to print
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_PRINT |
plugin events-server print [endpoint:1] [logId:1]
-
Print the specified event log for the provided endpoint.
- endpoint - INT8U - the relevant endpoint
- logId - INT8U - the log to be printed
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_PUBLISH |
plugin events-server publish [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [logId:1] [index:1] [eventControl:1]
-
Publish an event.
- nodeId - INT16U - the destination node id
- srcEndpoint - INT8U - the source endpoint
- dstEndpoint - INT8U - the destination endpoint
- logId - INT8U - the relevant log
- index - INT8U - the index within the event log to set
- eventControl - INT8U - the event control
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EVENTS_SERVER_PLUGIN_EVENTS_SERVER_SET |
plugin events-server set [endpoint:1] [logId:1] [index:1] [eventId:2] [eventTime:4] [eventData:-1]
-
Set the event at the specified index in the event log for the provided endpoint.
- endpoint - INT8U - the relevant endpoint
- logId - INT8U - the relevant log
- index - INT8U - the index within the event log to set
- eventId - INT16U - the event id
- eventTime - INT32U - the event time
- eventData - OCTET_STRING - additional event data