EmberAfDefinedEndpoint Struct Reference
Struct that maps actual endpoint type, onto a specific endpoint.
#include <
af-types.h
>
Data Fields |
|
| uint8_t | endpoint |
| EmberAfProfileId | profileId |
| uint16_t | deviceId |
| uint8_t | deviceVersion |
| EmberAfEndpointType * | endpointType |
| uint8_t | networkIndex |
| EmberAfEndpointBitmask | bitmask |
Struct that maps actual endpoint type, onto a specific endpoint.
Field Documentation
| EmberAfEndpointBitmask EmberAfDefinedEndpoint::bitmask |
Meta-data about the endpoint
| uint16_t EmberAfDefinedEndpoint::deviceId |
Device ID of the device on this endpoint.
| uint8_t EmberAfDefinedEndpoint::deviceVersion |
Version of the device.
| uint8_t EmberAfDefinedEndpoint::endpoint |
Actual zigbee endpoint number.
| EmberAfEndpointType * EmberAfDefinedEndpoint::endpointType |
Endpoint type for this endpoint.
| uint8_t EmberAfDefinedEndpoint::networkIndex |
Network index for this endpoint.
| EmberAfProfileId EmberAfDefinedEndpoint::profileId |
Profile ID of the device on this endpoint.
The documentation for this struct was generated from the following file:
-
af-types.h