EmberBindingTableEntry Struct Reference
Defines an entry in the binding table.
#include <
ember-types.h
>
Data Fields |
|
| EmberBindingType | type |
| uint8_t | local |
| uint16_t | clusterId |
| uint8_t | remote |
| EmberEUI64 | identifier |
| uint8_t | networkIndex |
Defines an entry in the binding table.
A binding entry specifies a local endpoint, a remote endpoint, a cluster ID and either the destination EUI64 (for unicast bindings) or the 64-bit group address (for multicast bindings).
Field Documentation
| uint16_t EmberBindingTableEntry::clusterId |
A cluster ID that matches one from the local endpoint's simple descriptor. This cluster ID is set by the provisioning application to indicate which part an endpoint's functionality is bound to this particular remote node and is used to distinguish between unicast and multicast bindings. Note that a binding can be used to to send messages with any cluster ID, not just that listed in the binding.
Referenced by
emAfCliBsendCommand()
,
optionBindingTablePrintCommand()
, and
optionBindingTableSetCommand()
.
| EmberEUI64 EmberBindingTableEntry::identifier |
A 64-bit identifier. This is either:
- The destination EUI64, for unicasts.
- A 16-bit multicast group address, for multicasts.
Referenced by
optionBindingTablePrintCommand()
, and
optionBindingTableSetCommand()
.
| uint8_t EmberBindingTableEntry::local |
The endpoint on the local node.
Referenced by
emAfCliBsendCommand()
,
optionBindingTablePrintCommand()
, and
optionBindingTableSetCommand()
.
| uint8_t EmberBindingTableEntry::networkIndex |
The index of the network the binding belongs to.
Referenced by
optionBindingTablePrintCommand()
, and
optionBindingTableSetCommand()
.
| uint8_t EmberBindingTableEntry::remote |
The endpoint on the remote node (specified by
identifier
).
Referenced by
optionBindingTablePrintCommand()
, and
optionBindingTableSetCommand()
.
| EmberBindingType EmberBindingTableEntry::type |
The type of binding.
Referenced by
emAfCliBsendCommand()
,
optionBindingTablePrintCommand()
, and
optionBindingTableSetCommand()
.
The documentation for this struct was generated from the following file:
-
ember-types.h