Plugin Commands: Reporting
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_ADD |
|
plugin reporting add [endpoint:1] [clusterId:2] [attributeId:2] [mask:1] [minInterval:2] [maxInterval:2] [reportableChange:4]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR |
|
plugin reporting clear
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR_LAST_REPORT_TIME |
|
plugin reporting clear-last-report-time
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_PRINT |
|
plugin reporting print
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_REMOVE |
|
plugin reporting remove [index:1]
|
|
Detailed Description
The reporting plugin contributes several CLI commands to the application framework to be used in creating and managing reporting table entries directly on the device.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_ADD |
plugin reporting add [endpoint:1] [clusterId:2] [attributeId:2] [mask:1] [minInterval:2] [maxInterval:2] [reportableChange:4]
-
Add a new entry to the report table.
- endpoint - INT8U - The local endpoint from which the attribute is reported.
- clusterId - INT16U - The cluster where the attribute is located.
- attributeId - INT16U - The id of the attribute being reported.
- mask - INT8U - 0 for client-side attributes or 1 for server-side attributes.
- minInterval - INT16U - The minimum reporting interval, measured in seconds.
- maxInterval - INT16U - The maximum reporting interval, measured in seconds.
- reportableChange - INT32U - The minimum change to the attribute that will result in a report being sent.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR |
plugin reporting clear
- Clear all entries from the report table.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_CLEAR_LAST_REPORT_TIME |
plugin reporting clear-last-report-time
- Clear last report time of attributes.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_PRINT |
plugin reporting print
- Print the report table.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_REPORTING_PLUGIN_REPORTING_REMOVE |
plugin reporting remove [index:1]
-
Remove an entry from the report table.
- index - INT8U - The index of the report to be removed.