EmberAfDeviceManagementTenancy Struct Reference
#include <
af-types.h
>
Data Fields |
|
| uint32_t | providerId |
| uint32_t | issuerEventId |
| uint8_t | tariffType |
| uint32_t | implementationDateTime |
| uint32_t | tenancy |
Field Documentation
| uint32_t EmberAfDeviceManagementTenancy::implementationDateTime |
| uint32_t EmberAfDeviceManagementTenancy::issuerEventId |
| uint32_t EmberAfDeviceManagementTenancy::providerId |
| uint8_t EmberAfDeviceManagementTenancy::tariffType |
| uint32_t EmberAfDeviceManagementTenancy::tenancy |
The documentation for this struct was generated from the following file:
-
af-types.h