EmberAfAllowedInterPanMessage Struct Reference
This structure is used define an interpan message that will be accepted by the interpan filters.
#include <
af-types.h
>
Data Fields |
|
| EmberAfProfileId | profileId |
| EmberAfClusterId | clusterId |
| uint8_t | commandId |
| EmberAfAllowedInterpanOptions | options |
This structure is used define an interpan message that will be accepted by the interpan filters.
Field Documentation
| EmberAfClusterId EmberAfAllowedInterPanMessage::clusterId |
| uint8_t EmberAfAllowedInterPanMessage::commandId |
| EmberAfAllowedInterpanOptions EmberAfAllowedInterPanMessage::options |
| EmberAfProfileId EmberAfAllowedInterPanMessage::profileId |
The documentation for this struct was generated from the following file:
-
af-types.h