Plugin Commands: Command Relay
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_ADD |
|
plugin command-relay add [inDeviceEui:8] [inDeviceEndpoint:1] [inClusterId:2] [outDeviceEui:8] [outDeviceEndpoint:1] [outClusterId:2]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_CLEAR |
|
plugin command-relay clear
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_LOAD |
|
plugin command-relay load
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_PRINT |
|
plugin command-relay print
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_REMOVE |
|
plugin command-relay remove [inDeviceEui:8] [inDeviceEndpoint:1] [inClusterId:2] [outDeviceEui:8] [outDeviceEndpoint:1] [outClusterId:2]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_SAVE |
|
plugin command-relay save
|
|
Detailed Description
The command relay plugin allows the forwarding of commands from one device to another.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_ADD |
plugin command-relay add [inDeviceEui:8] [inDeviceEndpoint:1] [inClusterId:2] [outDeviceEui:8] [outDeviceEndpoint:1] [outClusterId:2]
-
Retransmit commands from inDevice to outDevice.
- inDeviceEui - IEEE_ADDRESS - Incoming device EUI64.
- inDeviceEndpoint - INT8U - Incoming device endpoint.
- inClusterId - INT16U - Incoming cluster ID.
- outDeviceEui - IEEE_ADDRESS - Outgoing device EUI64.
- outDeviceEndpoint - INT8U - Outgoing device endpoint.
- outClusterId - INT16U - Outgoing cluster ID.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_CLEAR |
plugin command-relay clear
- Clear all relays.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_LOAD |
plugin command-relay load
- Load from disk.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_PRINT |
plugin command-relay print
- Print relays.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_REMOVE |
plugin command-relay remove [inDeviceEui:8] [inDeviceEndpoint:1] [inClusterId:2] [outDeviceEui:8] [outDeviceEndpoint:1] [outClusterId:2]
-
Deletes a relay between devices.
- inDeviceEui - IEEE_ADDRESS - Incoming device EUI64.
- inDeviceEndpoint - INT8U - Incoming device endpoint.
- inClusterId - INT16U - Incoming cluster ID.
- outDeviceEui - IEEE_ADDRESS - Outgoing device EUI64.
- outDeviceEndpoint - INT8U - Outgoing device endpoint.
- outClusterId - INT16U - Outgoing cluster ID.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMAND_RELAY_PLUGIN_COMMAND_RELAY_SAVE |
plugin command-relay save
- Save to disk.