EmberRouteTableEntry Struct Reference
Defines an entry in the route table.
#include <
ember-types.h
>
Data Fields |
|
| uint16_t | destination |
| uint16_t | nextHop |
| uint8_t | status |
| uint8_t | age |
| uint8_t | concentratorType |
| uint8_t | routeRecordState |
Defines an entry in the route table.
A route table entry stores information about the next hop along the route to the destination.
Field Documentation
| uint8_t EmberRouteTableEntry::age |
The number of seconds since this route entry was last used to send a packet.
Referenced by
optionBindingTableSetCommand()
.
| uint8_t EmberRouteTableEntry::concentratorType |
Indicates whether this destination is a High-RAM Concentrator (2), a Low-RAM Concentrator (1), or not a concentrator (0).
Referenced by
optionBindingTableSetCommand()
.
| uint16_t EmberRouteTableEntry::destination |
The short ID of the destination.
Referenced by
optionBindingTableSetCommand()
.
| uint16_t EmberRouteTableEntry::nextHop |
The short ID of the next hop to this destination.
Referenced by
optionBindingTableSetCommand()
.
| uint8_t EmberRouteTableEntry::routeRecordState |
For a High-RAM Concentrator, indicates whether a route record is needed (2), has been sent (1), or is no long needed (0) because a source routed message from the concentrator has been received.
Referenced by
optionBindingTableSetCommand()
.
| uint8_t EmberRouteTableEntry::status |
Indicates whether this entry is active (0), being discovered (1), or unused (3).
Referenced by
optionBindingTableSetCommand()
.
The documentation for this struct was generated from the following file:
-
ember-types.h