EmberAfDeviceManagementSupply Struct Reference
#include <
af-types.h
>
Data Fields |
|
| uint32_t | requestDateTime |
| uint32_t | implementationDateTime |
| uint8_t | supplyStatus |
| uint8_t | originatorIdSupplyControlBits |
Field Documentation
| uint32_t EmberAfDeviceManagementSupply::implementationDateTime |
| uint8_t EmberAfDeviceManagementSupply::originatorIdSupplyControlBits |
| uint32_t EmberAfDeviceManagementSupply::requestDateTime |
| uint8_t EmberAfDeviceManagementSupply::supplyStatus |
The documentation for this struct was generated from the following file:
-
af-types.h