Plugin Commands: Gas Proxy Function
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_LOG_CATCHUPS_IN_PROGRESS |
|
plugin gas-proxy-function print-log-catchups-in-progress
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_SUPPORTED_USE_CASES |
|
plugin gas-proxy-function print-supported-use-cases
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_FUTURE_DATED_MSG |
|
plugin gas-proxy-function simulate-future-dated-msg
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG |
|
plugin gas-proxy-function simulate-gbz-msg [useCase:2]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG_CREATION |
|
plugin gas-proxy-function simulate-gbz-msg-creation
|
|
Detailed Description
The reporting plugin contributes several CLI commands to the application framework to be used in creating and managing Gas Proxy Function functionality on the device.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_LOG_CATCHUPS_IN_PROGRESS |
plugin gas-proxy-function print-log-catchups-in-progress
- Print the number of logs that are currently catching up with missed entries.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_PRINT_SUPPORTED_USE_CASES |
plugin gas-proxy-function print-supported-use-cases
- Print the list of supported use cases. The message code printed should be used with the simulate-gbz-msg command.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_FUTURE_DATED_MSG |
plugin gas-proxy-function simulate-future-dated-msg
- Simulate transmission of a GBZ message to the Gas Proxy Function.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG |
plugin gas-proxy-function simulate-gbz-msg [useCase:2]
-
Simulate transmission of a GBZ message to the Gas Proxy Function.
- useCase - INT16U
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GAS_PROXY_FUNCTION_PLUGIN_GAS_PROXY_FUNCTION_SIMULATE_GBZ_MSG_CREATION |
plugin gas-proxy-function simulate-gbz-msg-creation
- Testing of GBZ message controller API.