Plugin Commands: Green Power Test Device
Detailed Description
The Green Power Test Device plugin contributes CLI commands to the application framework to be used for generating commands from a GPD
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_CHANNEL_REQUEST |
plugin green-power-test-device send-channel-request [channel:1]
-
Send a test GPD command
- channel - INT8U - Channel to set
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_COMM |
plugin green-power-test-device send-comm [type:1]
-
Send a test GPD command
- type - INT8U - 0 for tx only, 1 for bidir
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_IEEE_TEST |
plugin green-power-test-device send-ieee-test [gpdCommandId:1] [gpdCommandPayload:-1]
-
Send a test GPD command
- gpdCommandId - INT8U - gpd command ID
- gpdCommandPayload - OCTET_STRING - gpd command payload
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SEND_TEST |
plugin green-power-test-device send-test [gpdCommandId:1] [gpdCommandPayload:-1]
-
Send a test GPD command
- gpdCommandId - INT8U - gpd command ID
- gpdCommandPayload - OCTET_STRING - gpd command payload
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SET_PHY_CHANNEL |
plugin green-power-test-device set-phy-channel [channel:1]
-
set the phy channel
- channel - INT8U - Channel to set
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SETUP_GPD |
plugin green-power-test-device setup-gpd [srcId:4] [key:-1]
-
init a GPD
- srcId - INT32U - gpd src ID
- key - OCTET_STRING - the key
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_GREEN_POWER_TEST_DEVICE_PLUGIN_GREEN_POWER_TEST_DEVICE_SETUP_IEEE_GPD |
plugin green-power-test-device setup-ieee-gpd [eui:-1] [key:-1]
-
init a Ieee GPD
- eui - OCTET_STRING - gpd Ieee ID
- key - OCTET_STRING - the key