Plugin Commands: Simple Metering Client
Macros |
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_CLIENT_PLUGIN_SIMPLE_METERING_CLIENT_GET_SAMPLED_DATA |
|
plugin simple-metering-client get-sampled-data [server:2] [clientEndpoint:1] [serverEndpoint:1] [sampleId:2] [startTime:4] [sampleType:1] [numberOfSamples:2]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_CLIENT_PLUGIN_SIMPLE_METERING_CLIENT_LOCAL_CHANGE_SUPPLY |
|
plugin simple-metering-client local-change-supply [server:2] [clientEndpoint:1] [serverEndpoint:1] [proposedSupplyStatus:1]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_CLIENT_PLUGIN_SIMPLE_METERING_CLIENT_SCH_SNAPSHOT |
|
plugin simple-metering-client sch-snapshot [server:2] [clientEndpoint:1] [serverEndpoint:1] [issuerId:4] [commandIndex:1] [numberofCommands:1] [snapshotScheduleId:1] [snapshotStartDate:4] [snapshotSchedule:4] [snapshotType:1] [snapshotCause:4]
|
|
| #define | EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_CLIENT_PLUGIN_SIMPLE_METERING_CLIENT_START_SAMPLING |
|
plugin simple-metering-client start-sampling [server:2] [clientEndpoint:1] [serverEndpoint:1] [issuerId:4] [startTime:4] [sampleType:1] [SampleRequestInterval:2] [maxNumberOfSamples:2]
|
|
Detailed Description
The simple-metering-client plugin contributes CLI commands to the application framework to be used in conjunction with the Simple Metering cluster in a client context.
Macro Definition Documentation
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_CLIENT_PLUGIN_SIMPLE_METERING_CLIENT_GET_SAMPLED_DATA |
plugin simple-metering-client get-sampled-data [server:2] [clientEndpoint:1] [serverEndpoint:1] [sampleId:2] [startTime:4] [sampleType:1] [numberOfSamples:2]
-
Send a start sampling command to a metering server.
- server - INT16U - The network address of the server to which the request will be sent.
- clientEndpoint - INT8U - The local endpoint from which the request will be sent.
- serverEndpoint - INT8U - The remote endpoint to which the request will be sent.
- sampleId - INT16U - The sample id as received in a previous startSamplingResponse
- startTime - INT32U - The earliest start time sampling
- sampleType - INT8U - An 8 bit enumeration that identifies the required type of sampled data
- numberOfSamples - INT16U - The total number of samples.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_CLIENT_PLUGIN_SIMPLE_METERING_CLIENT_LOCAL_CHANGE_SUPPLY |
plugin simple-metering-client local-change-supply [server:2] [clientEndpoint:1] [serverEndpoint:1] [proposedSupplyStatus:1]
-
Send a start sampling command to a metering server.
- server - INT16U - The network address of the server to which the request will be sent.
- clientEndpoint - INT8U - The local endpoint from which the request will be sent.
- serverEndpoint - INT8U - The remote endpoint to which the request will be sent.
- proposedSupplyStatus - INT8U - The proposed supply status: either ON(2) or OFF/ARMED(1)
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_CLIENT_PLUGIN_SIMPLE_METERING_CLIENT_SCH_SNAPSHOT |
plugin simple-metering-client sch-snapshot [server:2] [clientEndpoint:1] [serverEndpoint:1] [issuerId:4] [commandIndex:1] [numberofCommands:1] [snapshotScheduleId:1] [snapshotStartDate:4] [snapshotSchedule:4] [snapshotType:1] [snapshotCause:4]
-
Schedule a snapshot.
- server - INT16U - The network address of the server to which the request will be sent.
- clientEndpoint - INT8U - The local endpoint from which the request will be sent.
- serverEndpoint - INT8U - The remote endpoint to which the request will be sent.
- issuerId - INT32U - The issuerId.
- commandIndex - INT8U - The commandIndex.
- numberofCommands - INT8U - The total number of commands
- snapshotScheduleId - INT8U - The snapshot schedule Id.
- snapshotStartDate - INT32U - The start time.
- snapshotSchedule - INT32U - The snapshot schedule. 3 bytes
- snapshotType - INT8U - The snapshot Type.
- snapshotCause - INT32U - The snapshot schedule cause.
| #define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SIMPLE_METERING_CLIENT_PLUGIN_SIMPLE_METERING_CLIENT_START_SAMPLING |
plugin simple-metering-client start-sampling [server:2] [clientEndpoint:1] [serverEndpoint:1] [issuerId:4] [startTime:4] [sampleType:1] [SampleRequestInterval:2] [maxNumberOfSamples:2]
-
Send a start sampling command to a metering server.
- server - INT16U - The network address of the server to which the request will be sent.
- clientEndpoint - INT8U - The local endpoint from which the request will be sent.
- serverEndpoint - INT8U - The remote endpoint to which the request will be sent.
- issuerId - INT32U - The issuerId.
- startTime - INT32U - The time to start sampling
- sampleType - INT8U - An 8 bit enumeration that identifies the type of data being sampled
- SampleRequestInterval - INT16U - An unsigned 16-bit field representing the interval or time in seconds between samples.
- maxNumberOfSamples - INT16U - A 16 bit unsigned integer that represents the number of samples to be taken.