EmberAfGpfMessage Struct Reference
#include <
af-types.h
>
Data Fields |
|
| uint8_t * | gbzCommands |
| uint16_t | gbzCommandsLength |
| uint8_t * | gbzCommandsResponse |
| uint16_t | gbzCommandsResponseLength |
| uint16_t | messageCode |
Field Documentation
| uint8_t* EmberAfGpfMessage::gbzCommands |
| uint16_t EmberAfGpfMessage::gbzCommandsLength |
| uint8_t* EmberAfGpfMessage::gbzCommandsResponse |
| uint16_t EmberAfGpfMessage::gbzCommandsResponseLength |
| uint16_t EmberAfGpfMessage::messageCode |
The documentation for this struct was generated from the following file:
-
af-types.h